Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Incorporating the LT 4320 Ideal Bridge in the Linear Bench Supply
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 3 Mar 2017 7:46 AM Date Created
  • Views 4037 views
  • Likes 8 likes
  • Comments 14 comments
  • bench top power supply
  • lt4320
Related
Recommended

Incorporating the LT 4320 Ideal Bridge in the Linear Bench Supply

jw0752
jw0752
3 Mar 2017

A while back I explored the Ideal Bridge available using the LT 4320 Controller and 4 N Channel MOSFETs.

 

https://www.element14.com/community/people/jw0752/blog/2017/02/01/exploring-the-lt4320-ideal-diode-bridge-controller

 

I also built a two channel linear bench supply using some Chinese Kits.

 

https://www.element14.com/community/people/jw0752/blog/2017/02/11/oh-no-not-another-power-supply

 

In this blog I will explore the results when I built another module with the Chinese Power Supply Kit but this time instead of using the 1N5408 Diodes supplied I substituted the LT 4320 Controller with 4 MOSFETs. Here are some pictures of the completed Module.

 

image

 

The small board in the upper left is the LT 4320 with the MOSFETs. The Yellow wires supply the AC voltage and the RED and Black are the rectified output back to the board. The small auxiliary board in the lower left is the fan controller which supplies about 11 volts to the 24 volt fan at room temperature and increases the voltage to the full 24 volts as the heat sink approaches 100 C.

 

image

 

The Red lead with the black coupler is the 12 volt supply to the meter circuitry.

 

image

 

The nice Radio Shack CPU heat sink that I used on the first two modules was not available any more so I had to use this less impressive but still adequate sink. The fan for this sink came at 24 volts instead of the previous 12 volts so the fan control had to be modified to make the adjustment. Since 24 volts was so close to the max raw voltage from the unregulated supply I used it directly instead of placing a regulator in the circuit.

 

image

 

Here is the final side view of the module. The next step was to remove one of the Diode Modules from the Linear Supply and install the LT4320 version.

 

image

 

The meter probes are looking at the voltage to the fan as the heat sink rises in temperature under a 36 Watt dissipation.

 

image

 

This is just the view from the back.

 

The goal of this experiment was to see what the difference would be between a channel using the LT4320 as opposed to the 1N5408 Diodes. Keep in mind the supply has identical Toroid Transformers and support controls for each channel. It turn out that the LT4320 side had a Max 27.6 Volts and the Diode side had 25.7 Volts. Besides this unloaded voltage difference at the top the load capability also showed the same differential. For example I turned both channels to their max output and then load each channel with a 2 amp load. The LT 4320 side dropped to 22 volts before it could support 2 amps. The Diode side dropped to 20.4 volts before it could support the 2 amp load. Even under a 3 amp load which is the max for this supply the MOSFETs ran very close to room temperature. While I like the LT4320 from a standpoint of improved efficiency and sophistication the improvement is probably not enough to justify its use in most cases.

 

image

 

Picture showing the no load difference between the two channels.

 

John

  • Sign in to reply

Top Comments

  • Gough Lui
    Gough Lui over 9 years ago in reply to mcb1 +5
    Hello guys (all the way from South Korea)! Interesting point in terms of mains "pollution" and it led me to scratch my head for a bit. Ideally, from my understanding anyhow, what you're probably most interested…
  • Jan Cumps
    Jan Cumps over 9 years ago +3
    Thanks God you had your clothes on. There's reflection in the last photo. Always dangerous...
  • jw0752
    jw0752 over 9 years ago in reply to Jan Cumps +2
    Ah yes Naked Electronics, Always an adventure.
  • jw0752
    jw0752 over 9 years ago in reply to shabaz

    Hi Shabaz

    It is really great that they include the schematic. It givse a good indication of how they are tapping in. Thanks for the link.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to jw0752

    Hi John,

     

    I just checked the device I've got, the schematic is on page 3 here:

    http://pdf.textfiles.com/manuals/STARINMANUALS/ETA/Archive/PowerProbe.pdf

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 9 years ago in reply to shabaz

    Hi Shabaz,

    I like your idea and I may experiment with it a little just to see what I can measure.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 9 years ago in reply to Gough Lui

    Yea!!  Gough is back.

    Thanks for your ideas and I hope all is going well on your world tour. It is good to know you are still looking over our shoulders.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to mcb1

    Another way is to use a 'LISN' device, or (even easier) just a transformer in series with resistor(s) i.e. like a potential divider, so the transformer only sees a small voltage across it, and then observe the other side of the transformer. You could at one time buy commercial products that were pretty much just that, and they allow you to check out on a 'scope what is going on (note there is a risk of damaging a scope here! So I wouldn't try it unless you're absolutely certain the transformer is behaving as expected). You can plug it into the same mains supply, and see the result before and after. Be prepared to see a lot of junk :  ) At home I see all sorts of noise overlaid, e.g. when the light dimmer is switched on. After seeing all the spikes and junk you'll want to buy a surge protected mains socket for the expensive equipment : )

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
>