Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Incorporating the LT 4320 Ideal Bridge in the Linear Bench Supply
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 3 Mar 2017 7:46 AM Date Created
  • Views 4037 views
  • Likes 8 likes
  • Comments 14 comments
  • bench top power supply
  • lt4320
Related
Recommended

Incorporating the LT 4320 Ideal Bridge in the Linear Bench Supply

jw0752
jw0752
3 Mar 2017

A while back I explored the Ideal Bridge available using the LT 4320 Controller and 4 N Channel MOSFETs.

 

https://www.element14.com/community/people/jw0752/blog/2017/02/01/exploring-the-lt4320-ideal-diode-bridge-controller

 

I also built a two channel linear bench supply using some Chinese Kits.

 

https://www.element14.com/community/people/jw0752/blog/2017/02/11/oh-no-not-another-power-supply

 

In this blog I will explore the results when I built another module with the Chinese Power Supply Kit but this time instead of using the 1N5408 Diodes supplied I substituted the LT 4320 Controller with 4 MOSFETs. Here are some pictures of the completed Module.

 

image

 

The small board in the upper left is the LT 4320 with the MOSFETs. The Yellow wires supply the AC voltage and the RED and Black are the rectified output back to the board. The small auxiliary board in the lower left is the fan controller which supplies about 11 volts to the 24 volt fan at room temperature and increases the voltage to the full 24 volts as the heat sink approaches 100 C.

 

image

 

The Red lead with the black coupler is the 12 volt supply to the meter circuitry.

 

image

 

The nice Radio Shack CPU heat sink that I used on the first two modules was not available any more so I had to use this less impressive but still adequate sink. The fan for this sink came at 24 volts instead of the previous 12 volts so the fan control had to be modified to make the adjustment. Since 24 volts was so close to the max raw voltage from the unregulated supply I used it directly instead of placing a regulator in the circuit.

 

image

 

Here is the final side view of the module. The next step was to remove one of the Diode Modules from the Linear Supply and install the LT4320 version.

 

image

 

The meter probes are looking at the voltage to the fan as the heat sink rises in temperature under a 36 Watt dissipation.

 

image

 

This is just the view from the back.

 

The goal of this experiment was to see what the difference would be between a channel using the LT4320 as opposed to the 1N5408 Diodes. Keep in mind the supply has identical Toroid Transformers and support controls for each channel. It turn out that the LT4320 side had a Max 27.6 Volts and the Diode side had 25.7 Volts. Besides this unloaded voltage difference at the top the load capability also showed the same differential. For example I turned both channels to their max output and then load each channel with a 2 amp load. The LT 4320 side dropped to 22 volts before it could support 2 amps. The Diode side dropped to 20.4 volts before it could support the 2 amp load. Even under a 3 amp load which is the max for this supply the MOSFETs ran very close to room temperature. While I like the LT4320 from a standpoint of improved efficiency and sophistication the improvement is probably not enough to justify its use in most cases.

 

image

 

Picture showing the no load difference between the two channels.

 

John

  • Sign in to reply

Top Comments

  • Gough Lui
    Gough Lui over 9 years ago in reply to mcb1 +5
    Hello guys (all the way from South Korea)! Interesting point in terms of mains "pollution" and it led me to scratch my head for a bit. Ideally, from my understanding anyhow, what you're probably most interested…
  • Jan Cumps
    Jan Cumps over 9 years ago +3
    Thanks God you had your clothes on. There's reflection in the last photo. Always dangerous...
  • jw0752
    jw0752 over 9 years ago in reply to Jan Cumps +2
    Ah yes Naked Electronics, Always an adventure.
  • jw0752
    jw0752 over 9 years ago in reply to mcb1

    Hi Mark,

    I will have to check these things out. I know how to look at ripple on a DC source but I am not sure how to do it on a mains feed>

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago

    Thanks God you had your clothes on. There's reflection in the last photo. Always dangerous...

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 9 years ago

    Great post John.

     

    I agree with Mark, you might want to look at the stability under loading.

     

    While the DC meters may look stable, you might have some interesting signals coming from your circuits.

     

    As for your fan, have you considered a large capacitor and a PWM circuit?

    Even at lower voltages, you should be able to drive the DC motor and control the speed with the PWM signal.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago

    the improvement is probably not enough to justify its use in most cases

    It might be interesting to see if there is a difference in the ripple and harmonics while using the Mosfets.

     

    One thing that we've always focused on is the Output, but I wonder what is going back to the mains supply with some of these devices.

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<