Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Inspired by Karen's Essentials The Learning Circuit
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 13 Dec 2018 5:27 AM Date Created
  • Views 5140 views
  • Likes 17 likes
  • Comments 41 comments
  • component_clamp
  • tech tips
Related
Recommended

Inspired by Karen's Essentials The Learning Circuit

jw0752
jw0752
13 Dec 2018

Today I watched Karen's makerkaren   Video about building a circuit from a schematic:

 

  https://www.element14.com/community/docs/DOC-91328/l/the-learning-circuit-34-making-a-circuit-from-a-schematic?sr=inbox&ru=360462

 

At first thought one might wonder what an old dog like me who has been playing with electronics for the last 62 years could learn from a beginners level 11 minute lesson on making a circuit from a schematic. As it turns out there is always a lot to learn from the members of this forum whether they are young or old, experienced or inexperienced and Karen's presentations are always a must watch for me.

 

Today I got two benefits from watching the show. The first benefit was watching how easily Karen flipped the board from one side to another for parts placement and soldering. While I had seen circuit board holders before, I had never seen one used and being a bit on the slow side I never realized, that with the amount of circuit board work I do, they could be a real benefit. So tonight I found one on line that would suit my needs and ordered it.

 

https://www.newark.com/aven/17010/circuit-board-holder-adjustable/dp/30Y9494?st=circuit%20board%20holder

 

The second thing that I received from watching Karen's video was an inspiration. I dawned on me how often I am frustrated or have to jury rig something to hold a component in place so it can be soldered. A lot of the components that I use for my builds are salvage components and as such they usually have short leads. When the components have long leads this isn't such a problem as the leads can be skewed to the board to hold the part in place. When I use a short lead component however,  I can place the component where I want it on the proto board but as soon as I turn the board over to solder the part, it falls or moves out of place. Many times it is just the case of not being tight to the board. While a part at a strange angle is functional, to me it is not acceptable.

 

The solution is this component clamp which I plan to use with my new circuit board.

 

   imageimage

The clamp was constructed from 12 AWG copper wire, 1/8" ID Brass Tubing, 1/8" OD Brass Rod, and an old twist spring. The copper wire was cut to the desired length and then formed using pliers. The 1/8" brass rod was cut slightly larger than the 1/8" brass tube so that the tube could fit over the rod and provide a bearing for the clamp finger to pivot on. The spring was the most difficult part as I soldered the clamp together before I figured out how to do the spring. Duh! Fortunately I was able to thread the spring onto the wire and then thread it again around the corner and onto the pivot. The two widely spaced fingers on the solder side of the board give ample room to get at the pads so that they can be soldered. If you look closely at the end of the finger that holds the component you will see that I have soldered a small brass pad to the wire. The purpose of the pad is to give me enough surface area so that I can use the clamp to hold headers and sharp topped components in place like this:

 

image

 

Here are a couple examples of how the clamp works to hold short lead components in place so the board can be turned over and the leads soldered.

 

  imageimage

Here we have a 555 timer. Traditionally I will bend a couple leads over to hold the IC and after soldering one lead I will apply pressure to the component, heat the pad again, and seat the component to the board. Now the new clamp will hold the chip in place and allow the soldering of all 8 legs and no seating required.

 

   imageimage

Here we have a 470 uF cap with short leads. As you can see it will be a breeze to solder in place thanks to the clamp.

 

A special Thanks to Karen, element 14, and the Producers of the Learning Circuit for tonight's fun in my shop.

 

John

  • Sign in to reply

Top Comments

  • makerkaren
    makerkaren over 7 years ago in reply to baldengineer +11
    The shape of these types is closer to John's design and is closer to what I had in mind. Though I think James "the bald engineer" Lewis was making a joke as to how if he were to try to use these clips…
  • Gough Lui
    Gough Lui over 7 years ago +8
    I find myself a little too lazy to bother. Honestly speaking, I do have some PCB holders and helping hands, as well as some "clip-on" heatsinks from my "beginner" days. But when I need something soldered…
  • jw0752
    jw0752 over 7 years ago in reply to jw0752 +8
    I have some additional comments on the Aven Circuit Board holder. First of all I found it to be a very good value and of sufficient quality so that I was very glad that I had purchased it. There was however…
Parents
  • luislabmo
    luislabmo over 7 years ago

    Hi John!,

     

    This is a very practical Idea! (I try something similar with my 3rd hand).

     

    My only complain with this kind of approach is when soldering male headers, as they get hot (mostly the ones that go to GND that usually require extra time to solder and therefore melt a little the plastic base that holds them in place) they may get pushed leaving the pins not uniform.

    image

    Luis

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to luislabmo

    Hi Luis,

     

    This is a legitimate concern. I use an extra hot setting so that I can minimize the time that the iron is on the connection. Another approach would be to hold the header with one or two pins and then solder the pins that aren't under pressure. Once the header is secured by one or two pins the clamp can be removed and the rest of the pins can be soldered.

     

    John

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • luislabmo
    luislabmo over 7 years ago in reply to jw0752

    Hi John,

     

    This is solid advice!. I'd like to try building one of my own, any tips on where to get the springs in the US?

     

    Luis

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 7 years ago in reply to luislabmo

    Hi Luis,

    I used a salvage spring but when I need springs I find that Ace Hardware or Hardware Hank usually have a pretty good selection in their specialty parts bins.

    John

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 7 years ago in reply to luislabmo

    Hi Luis,

    I used a salvage spring but when I need springs I find that Ace Hardware or Hardware Hank usually have a pretty good selection in their specialty parts bins.

    John

    • Cancel
    • Vote Up +5 Vote Down