Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog It's Not Just the ESD (Static)
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 18 May 2017 8:11 PM Date Created
  • Views 1271 views
  • Likes 6 likes
  • Comments 14 comments
  • emdr_machine
  • soldering_mosfets
Related
Recommended

It's Not Just the ESD (Static)

jw0752
jw0752
18 May 2017

I had a very challenging time last night. I have been working on producing a decent prototype of a machine I described in a previous blog.

 

https://www.element14.com/community/people/jw0752/blog/2017/04/17/prototyping-an-emdr-machine

 

The construction had been proceeding very well until last night as I neared completion and initial testing.

 

image

 

To power the LED Scanner I had decided to use the 2N7000 400mA  logic level MOSFETs. These, eleven in all,  had all been soldered into the board. and all the necessary connections had been made to the reverse side of the board. It was all neat and pretty except for one thing. It didn't work properly. It looked like most of the MOSFETs were showing a partial short from D to S.

 

image

 

image

 

A quick check with the meter showed that this was the case. 10 of the 11 MOSFET had from 10 to several K ohms of short between their drains and sources. My initial thought was that I had been careless with handling them and that static had gotten them. I hated what I had to do but I began to peal back the wiring from their contacts and with all the care and grounding straps I could find I replaced them one by one. At last reassembled I once again applied power and voila! Same problem, same appearance of partially shorted MOSFETS. So we dove back in for another go at it. This time I monitored the status of the MOSFETS as I went along. To my surprise they were being killed by me as they were being installed. At this point there was no way that static was to blame. Too many precautions and ground wires. It dawned on me at this point I was perhaps heat damaging them as I soldered them in. Because of space considerations the MOSFETs had been pulled down fairly tight to the board leaving about 3 mm of lead before entering the board. My solder iron does not have temperature control and runs at about 325 C. The data sheet for the 2N7000 says that it can tolerate 300 C on a 1/16 inch lead for 10 seconds. I think, from my experience, this is a bit optimistic. My usual technique is to minimize time on the contact but obviously something was damaging these parts. I got out the heat sink clips for leads and carefully began to replaced the remaining bad FETs. I continued to monitor them as I installed them. Since I was tacking wires and resistors to their solder pads It was necessary to make extra certain that time on the pad was minimized. I also sprayed coolant on the heat sink clips. Despite these precautions I still managed to kill a couple more. Finally after 6 hours and lots of frustration I had the machine up and running properly.

 

In all I killed 19 of the 2N7000 MOSFETS

 

image

 

Fortunately for the pocket book they are not expensive and while I did not have any left to spare after this debacle I did have exactly enough to complete the job.

Here is a picture of the completed project:

 

image

 

image

 

Here is a short video showing how the lights scan back and forth while hand held tactile devices buzz periodically in the patient's hands and a tone is emitted in the patient's ear as the light on the bar hits each end. I personally question the therapeutic value of this device but then what do I know, I am a technician who can't even seem to install eleven MOSFETs without Killing 19 of them.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

John

  • Sign in to reply

Top Comments

  • rachaelp
    rachaelp over 9 years ago +5
    After having to spend so long reworking your board to replace all the broken FET's are you thinking it might be time to invest in a temperature controlled soldering iron? With the amount of stuff you build…
  • shabaz
    shabaz over 9 years ago in reply to jw0752 +5
    Hi John, I found this photo on the internet of how some parts used to ship, because they were especially static-sensitive:
  • jw0752
    jw0752 over 9 years ago in reply to rachaelp +4
    Hi Rachael, Yes the thought crossed my mind. I am at this moment running some experiments to control the power to my present iron though this will only control the high temp and not really provide any…
  • jw0752
    jw0752 over 9 years ago in reply to mcb1

    Hi Mark,

    I have made a note to preform in the future. Typically I have formed by force but I can see that this is just one more place to create a failure. I love this forum as I always learn new things and I am continually improving my techniques.

    Thanks for your and dougw insights on preforming the leads.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to jw0752

    I'm not sure if they were new or recovered.

    I have 'broken' diodes by stressing the internal junction, so I'm with dougw on preforming leads now.

     

    Strange ...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 9 years ago

    Great post John.

     

    I sympathize with ESD issues.

     

    Back in the 1970's the initial EPROMS were very sensitive.  I could blow them up from about a meter.  This was at a time when they were about 100 USD each, so they made me stay out of the lab where they were stored.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 9 years ago in reply to shabaz

    image

     

    Here's some antistatic tube from the mid seventies. This is before the plastic type became common and they used extruded aluminium. Wonder if those CMOS parts still work?

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to jw0752

    There are quite a few good options for soldering stations, so if you do decide to upgrade I guess it depends on how much you'd want to spend.

     

    I personally swear by my Metcal kit, no adjustable knob to set the temp, but there are different cartridge types for leaded / lead free which run at different temps and then the way it works it ensures it ramps the power up only enough to heat the joint without overheating the component. It's got a funky power meter on the front that shows how much it's ramping up the power and for how long! If you want to read up about how they work there is an overview here: http://www.okinternational.com/metcal/english/globalnavigation/applications/hand-soldering/what-is-smartheat

     

    Hakko, Weller, Pace etc all do excellent kit too, but then you have an adjustable temp setting to deal with and your 50 years of old habits will become a factor image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>