Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Process Duration Timer  Blog 1 (The Timer)
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 24 Jul 2017 4:20 AM Date Created
  • Views 4687 views
  • Likes 12 likes
  • Comments 23 comments
  • diytestequipch
  • clock modification
  • process duration timer
Related
Recommended

Process Duration Timer  Blog 1 (The Timer)

jw0752
jw0752
24 Jul 2017

This is going to be an update and expansion of range for a test device I built and posted on the forum two years ago.

 

Battle of the Batteries - E*** vs D*** vs Bargain

 

The device that I built for that blog was designed to monitor a battery voltage that was under constant current load from a non-programmable electronic load and compare it to a target voltage that was selected by me. It was my purpose to time how long it took for the battery voltage to decay below the set target voltage. Since this process could take many hours I wanted an automated device that would let me walk away and return the next day to see the final results. For this first device I designed it using a comparator and support components which supplied power to an analog electric clock as long as the battery voltage was above the target voltage and then stopped the clock when the battery voltage finally dropped below the target. While this test adapter worked as planned it had several limitations and inconveniences.

 

I have been thinking for some time to revisit this project and to make the following improvements:

 

1. Use a digital clock timer that can be reset to 00:00:00 without having to manually move the clock hands.

 

2. Improve the accuracy of the timing to +/- 5 seconds.

 

3. Have an integral internal power supply to power the unit and produce the Target Voltage selection. ( The original required the use of an external bench supply to power the unit.)

 

4. Expand the range of Monitored (previously called Battery) Voltage that can be tested from 12 volts to 30 volts.

 

5. Expand the concept of the unit to include super capacitors and other processes where an initial energy source is consumed by a load over time.

 

This has been an idea knocking around in my head for some time but the recent posting of the DIY test equipment on the forum has made me put the idea back on the real bench.

 

This first blog will explain the progress I have made on finding an appropriate digital clock and some of the unusual modifications that I had to make to it. Please look with a critical eye at my solution as I am hoping those of you with more experience will warn me if I am making a mistake with this approach.

 

Here is my present best candidate for digital clock timer for the Process Duration Timer:

 

image

 

This is a $3.63 Chinese clock kit. The first thing that I liked about it was that it starts at 00:00:00 when power is first applied and then it begins to time immediately. As I built the kit I intentionally modified it with a mind to building it into the final enclosure. I left the LED display raised and made sure all the other components sat below the level of the faces of the digits. I left the memory battery off, as the fact that it will reset to 00:00:00 each time it is powered down if a asset for this application.

 

* First real problem is how to conserve the time on the clock when the transition of the monitored voltage from above to below the target voltage occurs. Keep in mind that the experiments that this unit will be timing may take many hours and I will not likely be there to look at the clock when the voltage transitions. It may be many more hours before I actually return and want to check the time. The clock system is built around an Atmel AT89C2051 Micro Processor and I have no access to its program nor do I have the skill to modify it if I did. My solution will have to be external and involve stopping the clock without loosing its current time register. I tried using the input switch on the unit to do this but all that it was programmed to do was reset the hours and minutes.

 

After some experimentation I discovered that if I disabled the oscillator clock to the AT89C2051 it stopped timing. I did this by pulling one side of the crystal to ground. (Question  - Is there any reason why this is not appropriate). When the microprocessor has its clock stopped a side effect of the stop is that I am also left with the current output to the LEDs which is usually a single bright digit on the display. I experimented with leaving the system in this state of suspended animation for 40 minutes and when I opened the grounded leg of the crystal the clock resumed at the exact time that it had when it was suspended.

 

The next step was to add a small 5 volt DPDT relay to the underside of the board. One of my concerns was that the additional capacitance of the relay structure that I was adding, to be able to pull the crystal lead to ground, might cause problems. I placed the relay close to the crystal and ground to minimize any capacitance. By now a good survey of the almost unreadable schematic supplied with the clock kit had given me a way to suppress the display of any digits while the clock is in suspended animation. There are six transistors on the unit that control whether a digit displays or not. These transistors all have a common emitter connect to the power supply. I used the second section of the DPDT relay to switch this power feed off to the transistors. In this way the energizing of the 5 volt relay puts the clock into suspended animation and blanks all the digits at the same time. I also used the other touch contact of this pole to light a red LED that I mounted in the place of the memory battery. After cutting some traces and adding a 470 ohm resistor for the LED the back of the circuit board looked like this.

 

image

 

You can see that I have also added a flyback diode to the relay to minimize a voltage spike when the relay is de-energized. The next step is to test the prototype of the timer to see if it does the things that I want it to do. First of all I want it to start off counting when power is applied at 00:00:00. Secondly I want to be able to put the timer into suspended animation for an indefinite period of time. The suspension will stop the clock pulse of the AT89C2051 and suppress the lighting of the digits in the display. To tell me that the clock is in suspended animation the red LED in the lower right corner should light. Here is a video of the proof of concept test.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I continue to be concerned about my use of the clock crystal for the AT89C2051 to produce the desired suspended animation. If anyone has any input or experience with this, your insights would be appreciated.

 

My next topics for this series of blogs leading up to building a working Process Duration Timer will concern themselves with a suitable power supply to drive the clock, the Arduino that will provide logic control of the unit, and a source for setting the target voltage. Also the integration of the Arduino and the programming thereof. I will also be including a scaling circuit so that the ADC of the Arduino is allowed to use its resolution to the best advantage regardless whether we are testing a device in the 30 volt area or the 1.5 volt area. We will also have to plan for instrumentation so that we can see the test voltage as well as the target voltage. I am sure that more ideas will come as I begin to build and test the individual components. This is probably the first project that I have decided to blog about as I design it rather than wait for a finished project. You just may get a chance to see me flounder and fail and have to be helped to the finish line.

 

John

 

https://www.element14.com/community/people/jw0752/blog/2017/07/28/process-duration-timer-part-2-power-supply

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 9 years ago +4
    Hi John, Clever idea, to freeze the clock as you have done : ) There are some other ways to do the freezing (e.g. use an external clock oscillator and gate it with (say) 'AND' logic, but that requires…
  • jw0752
    jw0752 over 9 years ago in reply to jc2048 +4
    Hi Jon, Thank you for your insights. I will make certain the I am using XTAL1 for the grounding. I did look at using the Arduino and a Real Time chip briefly before turning to modifying the existing clock…
  • shabaz
    shabaz over 9 years ago +3
    It is such a cool thing to have a process timer for the bench : ) For some recent testing (I think it was the Capacitance-to-Digital evaluation board from TI) I needed to do some timing, and in the end…
Parents
  • jc2048
    jc2048 over 9 years ago

    You're doing DIY Test Equipment too!

     

    The crystal oscillator is an amplifier (inside the processor) with the crystal as feedback. The crystal is very selective about the frequencies which it will pass (basically, the frequency at which it mechanically resonates and the odd harmonics of that frequency). So one pin (pin 5, XTAL1) is an input and the other (pin 4, XTAL2) is an output. I can't see which you've wired to. It's probably a bad idea to short the output to ground. CMOS can take a lot of abuse and you may get away with it but it won't necessarily be reliable over the long term.

     

    Crystal oscillators start up through random noise being amplified, the crystal selecting only those frequencies that fall in its very narrow passband, and the oscillation steadily building. That can take quite a long time - if you look at it on a scope you'll see what I mean. Processors have internal timers to hold off processing at start-up to ensure the clock is running and stable before they operate. In this case you are bypassing that and hoping that the processor will pick up and execute code properly. Evidently it is doing that, but you shouldn't depend on it getting it right.

     

    As Shabaz says, an external oscillator with a gating circuit would be cleaner as it allows for immediate execution from a standing start (in the old days, such circuits were used for single-stepping processors in order to watch code running slowly enough that you could see what the address and data buses were doing on LEDs). [The gating needs to be more than just an AND gate, though, so that you get full cycles and no danger of a short glitch at the start.]

     

    The relay will load the oscillator a little, but the contact capacitance when the contact is open should be small, so it probably won't pull the crystal frequency very much. [It's probably not very precise as a clock, anyhow, as there's no way to trim the load capacitance. As a clock, you could see an error of anything up to a minute or two a month unless you're very lucky.]

     

    If you are going to wire this up to an Arduino anyway, why not ditch the Atmel processor on this board and use the Atmel processor on the Arduino to do the clock timing and display? You seem to be jumping through hoops in order to avoid a little simple coding.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jc2048
    jc2048 over 9 years ago

    You're doing DIY Test Equipment too!

     

    The crystal oscillator is an amplifier (inside the processor) with the crystal as feedback. The crystal is very selective about the frequencies which it will pass (basically, the frequency at which it mechanically resonates and the odd harmonics of that frequency). So one pin (pin 5, XTAL1) is an input and the other (pin 4, XTAL2) is an output. I can't see which you've wired to. It's probably a bad idea to short the output to ground. CMOS can take a lot of abuse and you may get away with it but it won't necessarily be reliable over the long term.

     

    Crystal oscillators start up through random noise being amplified, the crystal selecting only those frequencies that fall in its very narrow passband, and the oscillation steadily building. That can take quite a long time - if you look at it on a scope you'll see what I mean. Processors have internal timers to hold off processing at start-up to ensure the clock is running and stable before they operate. In this case you are bypassing that and hoping that the processor will pick up and execute code properly. Evidently it is doing that, but you shouldn't depend on it getting it right.

     

    As Shabaz says, an external oscillator with a gating circuit would be cleaner as it allows for immediate execution from a standing start (in the old days, such circuits were used for single-stepping processors in order to watch code running slowly enough that you could see what the address and data buses were doing on LEDs). [The gating needs to be more than just an AND gate, though, so that you get full cycles and no danger of a short glitch at the start.]

     

    The relay will load the oscillator a little, but the contact capacitance when the contact is open should be small, so it probably won't pull the crystal frequency very much. [It's probably not very precise as a clock, anyhow, as there's no way to trim the load capacitance. As a clock, you could see an error of anything up to a minute or two a month unless you're very lucky.]

     

    If you are going to wire this up to an Arduino anyway, why not ditch the Atmel processor on this board and use the Atmel processor on the Arduino to do the clock timing and display? You seem to be jumping through hoops in order to avoid a little simple coding.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jw0752
    jw0752 over 9 years ago in reply to jc2048

    Hi Jon,

    Thank you for your insights. I will make certain the I am using XTAL1 for the grounding. I did look at using the Arduino and a Real Time chip briefly before turning to modifying the existing clock module. You are right that the whole unit including time measurement, voltage measurement and display can probably be handled by an Arduino and a good program. You are also correct that I prefer hoop jumping to programming. For me programming is like having to eat ones vegetables as a kid. I can do it but i will probably eat the pudding (hacking and putting together a Frankenstein piece of equipment) instead.

    John

    • Cancel
    • Vote Up +4 Vote Down