Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Repairing a Dental X-Ray Control
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 24 Dec 2015 7:55 AM Date Created
  • Views 5039 views
  • Likes 4 likes
  • Comments 6 comments
  • x-ray
  • dental_x-ray_unit
  • service
Related
Recommended

Repairing a Dental X-Ray Control

jw0752
jw0752
24 Dec 2015

Tonight I am going to perform a simple repair on a 70 KVp 7 mA Dental X-Ray control, Model 770 made by Gendex Corp in November 1997. This x-ray unit was one of the best designed of the all the units I have worked on over the years. The fact that after 18 years it is still working and relevant to current dental x-ray techniques attests to this.


image


In the course of this repair I am going to describe the technology of the 1997 era units. Bear in mind that many improvements have taken place since then. For one thing, a lot of the dental x-rays taken today are sensed on digital sensors and actual film is no longer a common medium. This has required a change in the design of the dental x-ray units to optimized the benefits of the digital medium. This x-ray was designed with enough flexibility that it still works well with the newer digital sensors.


This unit failed when a wall actuation button became shorted out. This caused the unit to experience a long duration voltage to a couple of key resistors. These resistors are sized to handle the voltage that was applied but only within a duty cycle of seconds. The shorted switch caused the seconds to turn into minutes and the resistors continued heating until one of them fused and the other one carbonized. I have seen this same problem several times in the past and there is never any collateral damage except the resistors themselves. Here is a picture of the block schematic for the unit and a couple pictures of the damaged parts.


image


image


This is a poor picture, the bad resistor is along side the small black relay. A better picture of the replacement resistor is further down in the blog.


image


The middle 30 Watt resistor in the stack has a black band of thermal damage.


I have always been impressed with the simplicity of the design of the Gendex 770. The Head ( the part that actually produces the x-rays) contains the x-ray tube, and a transformer that produces the high voltage 70,000 volts and the voltage to heat the filament of the tube. The transformer, the tube and its support structure are immersed in special oil that serves as an insulator and a coolant for the components. Here is a picture of a dental x-ray tube.


  image


The Anode is at the bottom and the two wires at the top go to the filament that serves as the Cathode.


When the proper voltage , about 108 volts AC, is applied to the two wires to the transformer of the x-ray head the filament heats up and the 70 KVp between the anode and the cathode accelerates electrons from the heated cathode to impact on the tungsten target of the anode. When electrons of the tungsten atoms fall back to normal energy levels they give off photons of x-ray energy. The purpose of the control we are repairing today is to provide a stable AC 108 volts to the head and to provide a way to time and control the duration of the applied voltage. Surprisingly there is no attempt to rectify the voltage to the x-ray tube. Since we are applying 108 volts AC the x-ray tube is actually being subjected to 70,000 volts AC between its anode and cathode.  At its basic level the x-ray tube is a diode. It will conduct when the cathode is negative with respect to the anode and block the current when the reverse polarity is present. The result is that this dental x-ray produces a stream of 1/120 second pulses rather than a continuous beam. The control also times out a warm up period for the x-ray head. This consists of 22 pulses  or 22/60 th of a second at which time a reduced voltage is applied to the head. This allows the filament to warm but doesn't produce signifcant x-rays. After the warm up period of 22 pulses the full power of the control is applied for the number of pulses selected on the control. At the end when I test the repaired unit I have made a video and you will be able to see this warm up and full power in action. Typically the duration of the full power x-rays will be from 1 pulse to 10 pulses ( 1/60 to 1/6 second ).


Here are pictures of the replaced resistors:


image


The 2 Watt 3.3 K resistor has been replaced


image


The middle resistor in this stack, a 30 W 15 Ohm, is the new replacement. This is the resistance that is put in series with the power to the x-ray head while it is in the warm up, 22 pulses, period. While the voltage applied produces more current than the resistor can handle continuous duty the 1/3 second of the warm up is too short to damage it.


Now having replaced the bad parts it is time to test the control to see if it is working properly. For my purposes I will not be testing it with an x-ray head. I will be testing it using a couple of 100 Watt light bulbs. I have connected the 100 Watt bulbs in parallel with the output that usually goes to the x-ray head. I have also jury-rigged a momentary push button to the trigger circuit of the control so I can trigger an exposure. This works well as I do not have to be concerned with ionizing radiation and I have only been asked to repair the control. Son Matt will hook up the head and test and perform calibration of the x-ray before he sells the machine. Here is what my test setup looks like:


image


Finally here is a short video of the actual test including my not so great moderator voice. If you have questions about dental x-ray units you can post them in the comments and I will try to answer them.


You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


John

.

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 10 years ago +2
    Hi John, Great demonstration video, and detailed explanation of how such machines work. I had no idea! : ) Very interesting how it is warmed up, and how the AC frequency is used for timing that and the…
  • DAB
    DAB over 10 years ago +1
    Nice post John. I wonder if anyone got over exposed due to the faulty switch. DAB
  • jw0752
    jw0752 over 10 years ago in reply to shabaz +1
    Hi Shabaz, I hope you are having a nice Holiday. This tube was salvaged from a tube head. This is a really messy operation as all the cooling/insulating oil in the head has to be dealt with. These heads…
Parents
  • mcb1
    mcb1 over 10 years ago

    Nice post.

    These repairs are made to look simple, but it takes yeas of experience to understand how it should work, in order to diagnose the cause.

     

    Cheers

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 10 years ago in reply to mcb1

    Hi Mark,

    I hope you and your family are having a great Christmas. You are correct that the first step in repairing anything is to understand what the device is suppose to do. Next one has to figure out how the specific circuit or mechanism goes about accomplishing this goal. Finally one looks for a break down in the process or the series of actions. The tough ones are in circuits that have a lot of feed back mechanisms or intermittents where the failure only happens occasionally and for no apparent reason. My favorites are where there is an apparent blast pattern to help locate the offending part.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 10 years ago in reply to mcb1

    Hi Mark,

    I hope you and your family are having a great Christmas. You are correct that the first step in repairing anything is to understand what the device is suppose to do. Next one has to figure out how the specific circuit or mechanism goes about accomplishing this goal. Finally one looks for a break down in the process or the series of actions. The tough ones are in circuits that have a lot of feed back mechanisms or intermittents where the failure only happens occasionally and for no apparent reason. My favorites are where there is an apparent blast pattern to help locate the offending part.

    John