Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Solder Iron for Ivan with a built in Timeout
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 14 Dec 2015 6:49 AM Date Created
  • Views 2835 views
  • Likes 6 likes
  • Comments 26 comments
  • auto_shut_off_solder_iron
Related
Recommended

Solder Iron for Ivan with a built in Timeout

jw0752
jw0752
14 Dec 2015

     Ever since I helped Grandson Ivan, age 9, with his school Science Project, See Grandson, Ivan, and the Volcano Science Project , I have continued to feed his curiosity and enthusiasm for electronics. So far, in addition to the Volcano Project, we have built a line following robot kit, a Ninja detector on a bread board, and several other small projects that he could take to school for show and tell. One day we took an old cassette deck apart. Ivan was immediately hooked on salvaging and his supportive Mom has been finding old pieces of equipment for him to tear apart. I only get to see Ivan on the weekends and sometimes it is only every other week but we really make the best of our time together. He must have some really good nerd genes as he can stay with me alert and focused on learning electronics for 5 hours straight. I think my previous record with some of his older cousins is about 45 minutes before they nod off.


     As Ivan's interest did not seem to wane I decided it was time to get him more involved in soldering. Even though he shows a lot of maturity in his ability to focus and learn I did not feel comfortable giving him a regular soldering iron to take home as I was afraid he would leave it on and forget it. (Grandpas worry about such things) So I got him involved in helping me design a modification to an old solder iron that would allow us the following functions:


Turn ON with a push button

Turn OFF with a different push button

LED to indicate when the iron is powered

Switch to choose between high and low wattage

Automatic turn off after 30 minutes.


     I told Ivan that we would make his solder iron and then we would use it to build our own small bench power supply for his own shop. We began by coming up with some plans that we could bread board and try out.


     imageimage


Here is one of our test circuits This first circuit used one section of an LM339 for a comparator of an RC timer circuit The final design will use a single  LM311MLM311M comparator The small sound module on the right side of the board is part of the discharge path of the capacitor This gives us a small beep every time the circuit shuts down The beep reminds us to turn the iron back on if we are still using it at the time One of the challenges of this project was how we were going to find a power supply for the timer small enough to fit into the case of the solder iron holder we planned to use The answer came when we decided to salvage a small 12 volt switching supply board from a wall wart power supply


      imageimage


I did not want to deprive Ivan of any part of the design process but I decided that there was plenty of time for him to learn the details and I did not want to get bogged down trying to solve the problems we all know constantly crop up during the build process. At least in these early stages of his learning I wanted things to flow smoothly, more like assembly of a well designed kit. Therefore in the days between Ivan's visits I busied myself planning and preparing the parts so that the assembly would go smoothly. A new control panel fascia was made for the solder iron and the holes were positioned and drilled for the switches and indicator LED. With Ivan's help the controls were installed and the unit began to take shape.


image


In the week leading up to Ivan coming today I continued to experiment with the circuit. I had originally hoped that the unit would have zero current draw in the off position but in the end the only way I could assure that we had the space for needed components was to leave the wall wart, 12 volt power supply, on and waiting for use. This would mean that the unit would draw 2 mA in the off mode just as most wall warts do when plugged in but not in use. While this doesn't sit perfectly well with my old fashioned idea that off should mean really off I guess that because so much of the appliances around me are really never truly off, I have gotten more used to the idea. When Ivan arrived today we got right down to business and began to assemble the the timer board which is the heart of the unit. Here is the schematic and circuit board layout that we used.


   imageimage


Ivan looked at the bread board with all its components and asked if all those parts were really going to fit on the small Adafruit  board we were going to use. I explained that this is why it is important to make a good plan before starting. We began to prepare for soldering by teaching and reminding Ivan about some techniques for handling the iron and cleaning the tip. In the process we managed to give him his first "Solder Iron Burn". We ran cold water on it and put a band aid on it and all he seemed concerned with was getting back to work. Little by little we assembled the board, all the while discussing the components that were being used and what they do. Here is the completed board.


     imageimage


The next step was to wire the assembled board, the power supply, and the switches together and fit them into the base of the solder iron.


     image


     With the unit finally assembled I explained to Ivan that we would probably be disappointed and we would likely have to take the unit apart again and find a mistake or two as this is my usual procedure.

He was eager to try it out so here he is pushing the START button for the first time.


     image image

 

The power light came on, I was pleased. The Stop button worked, as did the 16W / 35W switch. Now it was just a matter of turning it on and waiting approximately 35 minutes for it to turn itself off. Ivan and I busied ourselves with cleaning the bench and putting away the tools while we waited. As the time got close I became concerned as it was almost time for Ivan to go home and I didn't want him to leave with a failure hanging over us. Finally there was the small beep of the discharging capacitor and the power light went out.

 

Here is a short video of the soldering iron doing an auto shut down:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

With the soldering iron project under our belts Ivan and my next project will be a small safe power  supply for his bench so we can get him started building small circuits on his own, at home, between his visits to me. Hopefully we will have some extra time together over the Christmas Holidays.

 

John

  • Sign in to reply

Top Comments

  • D_Hersey
    D_Hersey over 10 years ago +2
    John, you outdo yourself! CD4060B | Counter/Arithmetic/Parity Function | Specialty Logic | Description & parametrics is another way to achieve your delay. Another idea is to use a capacitance multiplier…
  • CrazyFace
    CrazyFace over 10 years ago +2
    Absolutely love reading yours and Ivan's project blog's, Its so hard to get the kids today to show an interest, I lost my granddad at age 9 and luckily for me he had passed most of his knowledge onto my…
  • jw0752
    jw0752 over 10 years ago in reply to CrazyFace +2
    Hi Mark, Thank you for your encouragement. I have 12 grandkids that range in age from 23 to 9. Ivan, the youngest, is the first one to show a real interest and I am very happy about it. It seems that interest…
Parents
  • COMPACT
    COMPACT over 10 years ago

    Absolutely fantastic!!

    There's no time like your present!

    Your workshop is also the envy of many!

     

    1. Make sure he wears pH balanced Nitrile Gloves and avoids using PbSn solder.

    He doesn't need to unnecessarily ingest it like us older folk.

    Also be aware that many of the Pb free products contain carcinogenic chemicals.

    Also make sure that he washes his hands prior to going to the toot.

    Male electronics workers have been known to get testicular cancer!

     

    2. Get some ESD equipment and teach him about controlled Electrostatic Discharge!

    It only takes 20 volts of induced static to cause damage and contrary to the wives tales all components can be damaged with ESD.

    An the other wives tale is that once a component is in circuit it's ESD safe - It isn't!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 10 years ago in reply to COMPACT

    Hi Compact,

    Excellent suggestions. One of the best things about these blogs are the great suggestions that come from you guys. I will do my best to keep him safe.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 10 years ago in reply to COMPACT

    Hi Compact,

    Excellent suggestions. One of the best things about these blogs are the great suggestions that come from you guys. I will do my best to keep him safe.

    John