Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Using the Coarse + Fine Control circuit in my new Dual Bench Supply
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 24 Jan 2017 7:33 AM Date Created
  • Views 8894 views
  • Likes 10 likes
  • Comments 19 comments
  • bench_power_supply
  • power supply
  • coarse_fine_voltage_controls
Related
Recommended

Using the Coarse + Fine Control circuit in my new Dual Bench Supply

jw0752
jw0752
24 Jan 2017

A couple weeks ago I asked the forum for some ideas for a Coarse/Fine adjustment circuit for a basic bench power supply that I was going to build. While the power supply is nothing special and the build was rather routine I thought it might be fun to show you how the final product turned out and how I incorporated the Coarse and Fine circuit into the unit. Here is a picture of the inside of the completed power supply.

 

image

 

The unit has a nice project box that was originally a intra oral dental camera. Since I had two of these units I was able to salvage the nice toroid transformers from each unit so that I would have two isolated DC power channels on the outputs. The small green board in the back left corner was part of the original unit's circuit board that has been modified and retained as a line power entrance for the unit. Here is a close up of that board.

 

image

 

The board and the toroids are capable of switching from 120 VAC to 240 VAC input power though in my area, at least, only the 120 VAC option will be used. Along with the toroids from the original dental cameras I have also retained the bridge rectifiers and the filter caps. I will need 12 volts to power the LED meters that I have chosen for the front control panel and I will also need a voltage source for the power on LED and a small cooling fan. To do this I built a 7812 based linear regulator circuit for each channel. Besides the channel's meter this circuit will power the LED on one side and the fan on the other. Here is a better picture of the voltage regulator circuit:

 

image

 

Now is the point where I take a short cut and use a couple of Chinese DC to DC converters that I purchased for $4.00 each. Amazingly these came for that price including shipping. Every time I order some of these cheap items and get the shipping included I suspect that it may be the last time. It doesn't make sense how anyone can make a profit doing it this way. Here is a close up of the converter:

 

image

 

This little DC converter is based on an XL4016 chip and is capable of input up to 36 volts and output of 1.2 volts to 35 volts at 8 amps. Since my transformers will only produce unregulated 27 volts my upper range for this power supply will be limited by the voltage drop of the transformers under load. Experiments have shown me that I can expect 24 volts at 1 Amp and 20 volts at 5 amps final output from the unit. I was a little disappointed that I can not lower the output below 1.2 volts but this is more of an aesthetic complaint as opposed to a practical one. Most of my experiments are at 3.3 volts and above and should I need a lower voltage for some reason I could always use another means to get it. The DC/DC converters came with small multi-turn 10K trimmers which I have removed and installed wiring harnesses to attach to the control panel potentiometers. Here is a schematic of the circuit I finally settled on for my coarse / fine control. Since the converter only looks at a variable resistance between 0 and 10K to control the output voltage I have tried to stay close to that parameter in the control design.

 

image

 

Here is a picture of the inside of the control panel but unfortunately it doesn't do a very good job of showing the wiring to the controls. The Coarse Potentiometer will change the output voltage from 1.2 volts to 27 volts over it's 270 degree sweep while the Fine Potentiometer will change the voltage output by at the most plus or minus 1 volt over its 270 degree sweep. The fine control is more effective for voltage levels in the middle of the range and its effectiveness drops as the coarse control approaches its limits.

 

image

 

The meters come with very large shunt bars to be used to measure up to 100 amps but this would not be practical for this unit so it was necessary to make and calibrate some shunts more practical to this application. I used some 16 GA brass wire and soldered the leads from the ammeter to it. With a lab ammeter in series I was able to move and resolder the meter leads back and forth on the brass wire until I got the meter reading to match the Lab Meter. If you follow the large black and red wires from each meter you should be able to spot the brass shunt wires for each channel. Here is a picture of the unit completed and assembled:

 

image

 

I have also made a short video of me using the fine controls to zero in on a specific voltage on each channel. Besides my time which nowadays is practically worthless I have about $35 dollars invested in this unit thanks to my sons for the donation of the two scrap dental camera units and cheap Chinese electronic modules and meters.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I also want to thank my friends on E-14 for their excellent and inspiring suggestions for adding the fine voltage control.

 

John

  • Sign in to reply

Top Comments

  • rachaelp
    rachaelp over 9 years ago +3
    That's a nice tidy looking bench PSU! Have you tested it out with various loads and looked at how well the cheap regulators are working? Is there switching noise on the outputs? If that's the case then…
  • balearicdynamics
    balearicdynamics over 9 years ago +2
    You have done a very good job. And it's a great project. I think to copy and make one of these in the near future for a project that may arise next months. Enrico
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to jw0752 +2
    John, as you know (by my questions) one of my "best" knowledge lacks is just in the powering system. So I think that one of these can makes the difference just testing and making experiments. Until now…
Parents
  • D_Hersey
    D_Hersey over 9 years ago

    John, hi!  Your control circuit is baffling me, not that it takes much these days, too bad about the Packers.

     

    What if we took a smaller and larger pot, something like a 10:1 ratio, although 5:1 and 2:1 are possible, we could even use 1:1 if we threw a fixed resistor in series with the trimmer?  Let's degenerate them into variable resistors the common way by busing the wiper with one end of the resistor.  Let's knit our brows then pronounce them variable conductors.  We attach one end of each of our variable conductors to a high reference potential.  Let's attach the free ends of these conductors to the summing (inverting terminal -- virtual ground) junction of an op (summing amplifier) amp with the non-inverting input held (matching the input Z's with an R to mitigate current drift) at a lower reference potential

     

    Wouldn't this give you the linearity you are seeking?

     

    Un-knit now

     

    Hoping you and your family are fine!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to D_Hersey

    I think what you are describing is similar to a couple of the circuit options we discussed in the question John posted up a few weeks ago about the creation of a coarse/fine POT setup. I can see why John has gone for the solution he has to replace the existing multi-turn POT of the DC-DC converter board but I expect substituting it for the buffered circuit I gave then would give a nice linear control (probably no need for the buffer on the Vref end as I expect this is just Vout of the PSU connecting back via a potential divider into the FB pin of the IC). I guess the problem could be working out how to power it from what is available and ensure it all starts up correctly.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • rachaelp
    rachaelp over 9 years ago in reply to D_Hersey

    I think what you are describing is similar to a couple of the circuit options we discussed in the question John posted up a few weeks ago about the creation of a coarse/fine POT setup. I can see why John has gone for the solution he has to replace the existing multi-turn POT of the DC-DC converter board but I expect substituting it for the buffered circuit I gave then would give a nice linear control (probably no need for the buffer on the Vref end as I expect this is just Vout of the PSU connecting back via a potential divider into the FB pin of the IC). I guess the problem could be working out how to power it from what is available and ensure it all starts up correctly.

     

    Best Regards,


    Rachael