Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Water Shut Off System Chapter 2 (Sensors)
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 5 Jul 2016 5:41 AM Date Created
  • Views 1303 views
  • Likes 5 likes
  • Comments 16 comments
  • water_sensor
Related
Recommended

Water Shut Off System Chapter 2 (Sensors)

jw0752
jw0752
5 Jul 2016

This is a continuation of:

 

https://www.element14.com/community/people/jw0752/blog/2016/07/02/automatic-water-shut-off-system-for-the-home-chapter-i

 

The goal of this project is to build a system that will sense water leaks in my home and automatically shut off the main water valve to my home. Chapter one gave an overview of the project. I want to thank mcb1, dougw , and beacon_dave for their helpful suggestions on the mechanics of actually moving the valve.

 

The project is progressing very well on all fronts. Today specifically I will show the simple sensors that been prototyped and tested so far.

 

We are all familiar with the customary water sensor that is used to measure whether plants or soil need watering.

 

https://www.sparkfun.com/products/13322

 

I wanted something similar that could be laid out on the floor in critical locations and would detect water quickly and definitely. The moisture detector relies on the conductivity of water which has a very uncertain resistance depending on levels of contamination. Since I would have no way to predetermine the resistance of any leaking water I decided to produce my own contamination in the form of salt. The idea is to have two copper electrodes wrapped in absorbent paper towels some of which has been soaked in salty water and then dried.

 

image

 

Here are two sheets of paper towels that have been soaked in salty water and are now being allowed to completely dry. The next step is to make the copper electrodes for the sensor. Short pieces of 18 Gauge copper wire were cut and wire pigtails were attached.

 

image

 

Here is a pair of electrodes separated by absorbent towels one piece of which has dried salt in it. The towels are wound tightly with the paper and then the paper rolls are secured with a couple pieces of light gauge wire.

 

image

 

These sensors will be placed in locations that are susceptible to leaks. It is hoped that even a few drops of water will soak into the towel, mix with the salt and provide a rich ionic conductor between the two electrodes.

Here is a short video of a test of the prototype sensor.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

These sensors are one shot avalanche type. They should react to a very small amount of water, as you saw in the video, with a significant drop in resistance. Based on the tests of the prototype I will design the circuit to respond to any resistance that is less than 60 K Ohms. Since the dry sensors have very high resistance, (they are still OL on the 50 Meg range of the Fluke), they can be paralleled in the circuit. This will allow me to run one or two sensor lines with multiple sensors on each line. If there is a water leak problem I will have to manually check each sensor to see where the leak is, since the system will not identify a specific location as it is presently being designed. The activated sensor will have to be disassembled, dried, and wrapped with new paper before it is put back into service. I have made up 9 of them at this point and will be refining the locations where they will give the most protection.

 

image

 

The rest of the project is progressing well. I have decided how the mechanics of the water shut off will work and the construction and operation will be reported in Chapter three of this Blog, in the next few days.

 

John

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 10 years ago in reply to jw0752 +2
    When I first saw your idea I thought it was elegant, but others have pointed out the moisture and humidity may cause flase triggers. Not something you want while in the shower ... just like when the gas…
  • shabaz
    shabaz over 10 years ago in reply to jw0752 +2
    Hi John, Thank you for all your interesting projects and valuable information too. It is always exciting seeing what's happening in your lab!
  • michaelkellett
    michaelkellett over 10 years ago +1
    You may have problems with humidity: sodium chloride is quite hygroscopic (and so are paper towels) and will absorb water from the air if the RH is high enough. Test your sensors carefully if you don't…
Parents
  • michaelkellett
    michaelkellett over 10 years ago

    You may have problems with humidity: sodium chloride is quite hygroscopic (and so are paper towels) and will absorb water from the air if the RH is high enough. Test your sensors carefully if you don't want surprise water cut offs.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 10 years ago in reply to michaelkellett

    Hi Michael,

    This is an excellent observation and may very well force me to redesign. The relative humidity in my basement is kept around 40% so I am hoping I can get away with the design. I suppose the first time the system triggers while I am soaped up in the shower I will have to go back to the drawing board. I have never designed anything yet that didn't have surprises waiting for me and unexpected side effects. I was also concerned with the possibility of corrosion on the electrodes which is why I added a second unsalted paper to the wrap. As you pointed out, the salt may pull moisture from the air and make this a bad design.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 10 years ago in reply to jw0752

    Could something like a DHT11 or DHT22 humidity sensor be used as a reference to desensitise the system in the case of high humidity levels ? 

     

    Another sensor approach might be to use the 'flat-pack' foam sponge you get for cleaning your soldering iron tips. That typically expands from around 1mm to 10mm when wet so could be used to close a contact.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 10 years ago in reply to beacon_dave

    Hi Dave,

    You think like an experienced inventor. This is exactly what my mind does when I am looking for a solution. A whole bunch of ideas for approaching the problem from different directions come to mind. I believe that your sponge idea would probably work.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 10 years ago in reply to beacon_dave

    Hi Dave,

    You think like an experienced inventor. This is exactly what my mind does when I am looking for a solution. A whole bunch of ideas for approaching the problem from different directions come to mind. I believe that your sponge idea would probably work.

    John