Personal Blogs
  • Community Hub
  • More
Personal Blogs
Michael Kellett's Blog Efinix Dev Board - PSRAM working
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: michaelkellett
  • Date Created: 8 Jan 2023 4:25 PM Date Created
  • Views 4809 views
  • Likes 13 likes
  • Comments 12 comments
  • fpga
  • effinix
  • aps6404
Related
Recommended

Efinix Dev Board - PSRAM working

michaelkellett
michaelkellett
8 Jan 2023

In the last blog about this board, I talked a little about the PSRAM chips. This blog is about getting them working and some digression into memory controllers in general.

I have two AP Memory APS6404 chips on the board and directly attached to the FPGA. The 4 data IO pins one each memory chip have their own FPGA pins but the chips elect and clock for each PSRAM share FPGA pins.  The idea is to read and write data in 16-bit words to get a faster throughput.

If you want to really get into the detail of these chips then you will need to read the data sheet – which is readily obtainable, just search the part number.

In common with many similar chips the 6404 has a significant overhead each time a random memory address is selected. It can transfer one nibble of data per clock cycle once it gets going, so at first glance you might expect to achieve read and write speeds of up to 133/2 Mbyte/s (the headline max clock is 133MHz).

For speed the chip will always be operated in quad mode so for the following discussion it is assumed that this is the case.

To write to n bytes memory you must send two nibbles of write command, 6 nibbles of address and 2n nibbles of data. (2 nibbles = 1 byte). Any real controller will have a little overhead of its own, my controller and test core require 6 clock cycles per write operation.

Read operation are worse in that they need send two nibbles of read command, 6 nibbles of address and 6 clock cycles of wait time before any read data can be clocked out.

The effect of the overhead can be reduced by reading or writing bursts of many bytes but there are some issues that need to be considered.

The first is that the 6404 only allows a maximum length of data burst of 32 bytes at clock rates above 84MHz.

The maximum permitted chip enable time is 4us for extended temperature range parts and 8us for normal range parts. This sets the maximum burst length for any clock rate to just over 300 bytes.

When you take all these things into account you can work out how fast data can be transferred.

image

Operating the chip at 133MHz is not straightforward. The clock cycle time is 7.5ns and the chip needs data setup and hold times of 4ns total. This does not leave much margin for skew and delay in the driving circuits. AP Memory recommend active tuning to get it right.

On this board, which uses unmatched length tracks and low cost board I sidestep the issue by clocking at 75MHz.

This should allow a maximum read rate of 36.09Mbyte/s, doubled because I have two chips effectively in parallel.

Test Controller Architecture

At the very lowest level the controller architecture is quite simple.

The internal interface has inputs for address, burst length, write data and start, and outputs for read data and busy.

All my internal VHDL logic operates on the rising clock edge. The simplest way of clocking the memory chips is to use the inverse of the main clock, gated as required, to meet the timing requirements of the 6404 for control and data edges relative to clock edges.

The low-level interface is called psram_access because it isn’t really a controller. For testing purposes its driven by a test block which writes 16 bursts of 32 16-bit words to memory. The data is the inverse of the low order 16 bits of the address. The test block then reads the data back and checks it, finally setting the good or bad signals as appropriate.

Top level of design used for simulation and testing

image

PSRAM Control Block

image

VHDL Code for psram_access module

-------------------------------------------------------------------------------
--
-- Title       : psram_access
-- Design      : EFTB
-- Author      : Michael Kellett
-- Company     : MK Electronics Ltd
--
-------------------------------------------------------------------------------
--
-- File        : C:\Docs\Rabbits\Efinix_EFTB_rtl\Aldec\src\psram_access.vhd
-- Generated   : Sun Jan  1 14:15:49 2023
-- From        : interface description file
-- By          : Itf2Vhdl ver. 1.22
--
-------------------------------------------------------------------------------
--
-- Description : 
--
-------------------------------------------------------------------------------

--{{ Section below this comment is automatically maintained
--   and may be overwritten
--{entity {psram_access} architecture {psram_access}}

library IEEE;
use IEEE.std_logic_1164.all;
use IEEE.NUMERIC_STD.all;

entity psram_access is
	 port(
		 clk75 : in STD_LOGIC;
		 res_hi : in STD_LOGIC;
		 r_nwr : in STD_LOGIC;
		 transfer : out STD_LOGIC;
		 start : in std_logic;
		 psr_dat_i : in std_logic_vector(7 downto 0);	 
		 psr_nce : out std_logic;
		 psr_clk : out std_logic;
		 busy : out std_logic;
		 length : in STD_LOGIC_VECTOR(10 downto 0);
		 read_data : out STD_LOGIC_VECTOR(15 downto 0);
		 write_data : in STD_LOGIC_VECTOR(15 downto 0);
		 address : in STD_LOGIC_VECTOR(23 downto 0);
		 psr_dat_o : out STD_LOGIC_VECTOR(7 downto 0);
		 psr_out_en : out STD_LOGIC_VECTOR(7 downto 0);
		 psr_debug : out STD_LOGIC_VECTOR(7 downto 0)
	     );
end psram_access;

--}} End of automatically maintained section

architecture psram_access of psram_access is   

	signal command : std_logic_vector(7 downto 0);	 
	signal bit_count : unsigned(4 downto 0);
	signal address_sr : std_logic_vector(23 downto 0); 
	signal n_words : unsigned(10 downto 0);
	signal read_reg : std_logic_vector(15 downto 0);
	signal write_reg : std_logic_vector(15 downto 0);  
	signal quad : std_logic;  
	signal psr_clk_en : std_logic;

 	TYPE t_psa_state is (PSA_IDLE, PSA_CMND_1, PSA_CMND_2, PSA_CMND_3, PSA_WRITE_1, PSA_WRITE_2, PSA_WRITE_3, PSA_READ_1, PSA_READ_2, PSA_READ_3, PSA_READ_4,
	PSA_QUAD_1);
	signal psa_state : t_psa_state;	


begin

	 -- enter your statements here --

	psram : process(clk75)
	begin
		if rising_edge(clk75) then	
			if res_hi = '1' then 
				psr_nce <= '1';	
				psr_out_en <= (others => '0');
				busy <= '0'; 
				quad <= '1';	
				transfer <= '0';
				psa_state <= PSA_IDLE;
			else
				if psa_state /= PSA_IDLE then
					psr_clk_en <= '1';
				else
					psr_clk_en <= '0';
				end if;
				case psa_state is
					when PSA_IDLE => 
					if start = '1' or quad = '1' then
						busy <= '1'; 
						if quad = '1' then
							command <= "00110101";		-- quad mode command	
						elsif r_nwr = '1' then
							command <= "11101011";		-- read command
						else
							command <= "00111000";		-- write command 
						end if;	
						if quad = '1' then
							psr_out_en <= "00010001";		-- enable drive on SI pins on both PSRAMS 	
						else
							psr_out_en <= "11111111"; 
						end if;
						bit_count <= "00000";			-- will count serial bits sent	
						address_sr <= address; 
						n_words <= (others => '0');
						psa_state <= PSA_CMND_1; 		-- will start clock
					end if;	 
				when PSA_CMND_1	=> 
--					psr_nce <= '0';						-- chip select asserted
					psa_state <= PSA_CMND_2;		
				when PSA_CMND_2 =>
					psr_nce <= '0';						-- chip select asserted	
				    if quad = '0' then
						psr_dat_o(3 downto 0) <= command(7 downto 4);			-- already in quad mode
						psr_dat_o(7 downto 4) <= command(7 downto 4);	  		-- send ms nibble out on SPI to PSRAMS
						command(7 downto 4) <= command(3 downto 0);	 			-- prepare next nibble to send	
						if bit_count = 1 then
							bit_count <= "01000"; 								-- correct bit count (to 8) in case of using spi mode (currently not coded)
							psa_state <= PSA_CMND_3;							-- move on to address sending in 4 bit nibbles 
						else
							bit_count <= bit_count + 1;							-- NB - won't change bit_count before it gets checked in next line
						end if;										   				
					else
						psr_dat_o(0) <= command(7);								-- in spi_mode
						psr_dat_o(4) <= command(7);	
						command(7 downto 1) <= command(6 downto 0);	 			-- prepare next bit to send	 
						bit_count <= bit_count + 1;			-- NB - won't change bit_count before it gets checked in next line
						if bit_count = 7 then				-- will send 8 bits in spi mode
							psa_state <= PSA_QUAD_1;		-- if was only getting into quad mode using spi then it's done
						end if;
					end if;
				when PSA_CMND_3 =>
					psr_dat_o(3 downto 0) <= address_sr(23 downto 20);
					psr_dat_o(7 downto 4) <= address_sr(23 downto 20);
					address_sr(23 downto 4) <= 	address_sr(19 downto 0);
					bit_count <= bit_count + 1;			-- NB - won't change bit_count before it gets checked in next line
					if bit_count = 13 then
						if r_nwr = '1' then
							psa_state <= PSA_READ_1;
						else
							psa_state <= PSA_WRITE_1;
						end if;
					end if;
				when PSA_READ_1 =>	  
					bit_count <= bit_count + 1;			-- NB - won't change bit_count before it gets checked in next line
					if bit_count = 20 then	 			-- 6 wait states for read tweaked from +6 to + 7
						psa_state <= PSA_READ_2;
					end if;
					if bit_count = 14 then 				-- going to read so disable drivers
						psr_out_en <= "00000000";
					end if;
				when PSA_READ_2 => 
					transfer <= '0';									-- clear FIFO write if reading subsequent word
					read_reg(15 downto 12) <= psr_dat_i(7 downto 4);
					read_reg(7 downto 4) <= psr_dat_i(3 downto 0);	-- buffer the ms nibbles
					n_words <= n_words + 1;
					psa_state <= PSA_READ_3;
				when PSA_READ_3 =>
					read_data(11 downto 8) <= psr_dat_i(7 downto 4);
					read_data(3 downto 0) <= psr_dat_i(3 downto 0);
					read_data(7 downto 4) <= read_reg(7 downto 4);
					read_data(15 downto 12) <= read_reg(15 downto 12);
					transfer <= '1';  									-- write data to FIFO
					if n_words = unsigned(length) then
						psr_nce <= '1';
						psa_state <= PSA_READ_4;
					else
						psa_state <= PSA_READ_2;						
					end if;
				when PSA_READ_4 => 
					transfer <= '0';
					busy <= '0';
					psa_state <= PSA_IDLE;
				
				
				when PSA_WRITE_1 =>						-- no wait states needed
					write_reg <= write_data;
					psr_dat_o(7 downto 4) <= write_data(15 downto 12);
					psr_dat_o(3 downto 0) <= write_data(7 downto 4); 
					transfer <= '1';
					n_words <= n_words + 1;
					psa_state <= PSA_WRITE_2;  
				when PSA_WRITE_2 =>
					transfer <= '0';
					psr_dat_o(7 downto 4) <= write_reg(11 downto 8);
					psr_dat_o(3 downto 0) <= write_reg(3 downto 0);  
				    if n_words = unsigned(length) then
						psa_state <= PSA_WRITE_3;
					else
						psa_state <= PSA_WRITE_1;
					end if;
				when PSA_WRITE_3 =>
					psr_nce <= '1';
					busy <= '0';
				    psa_state <= PSA_IDLE;
				
				
				when PSA_QUAD_1 =>
					psr_nce <= '1';
					busy <= '0';  
					quad <= '0'; 
					psr_out_en <= (others => '0');
				    psa_state <= PSA_IDLE;

				when others =>
					psr_nce <= '1';
					busy <= '0';
				    psa_state <= PSA_IDLE;
				end case;	
			end if;
	   end if;
	end process;  
	
	psr_debug <= psr_dat_i;
	psr_clk <= '0' when psa_state = PSA_IDLE else (not clk75);

end psram_access;

VHDL Code for psram_test module

-------------------------------------------------------------------------------
--
-- Title       : psram_test
-- Design      : EFTB
-- Author      : Michael Kellett
-- Company     : MK Electronics Ltd
--
-------------------------------------------------------------------------------
--
-- File        : C:\Docs\Rabbits\Efinix_EFTB_rtl\Aldec\src\psram_test.vhd
-- Generated   : Tue Jan  3 09:25:57 2023
-- From        : interface description file
-- By          : Itf2Vhdl ver. 1.22
--
-------------------------------------------------------------------------------
--
-- Description : 
--
-------------------------------------------------------------------------------

--{{ Section below this comment is automatically maintained
--   and may be overwritten
--{entity {psram_test} architecture {psram_test}}

library IEEE;
use IEEE.std_logic_1164.all;
use IEEE.NUMERIC_STD.all;

entity psram_test is
	 port(
		 clk75 : in STD_LOGIC;
		 res_hi : in STD_LOGIC;
		 start_test : in STD_LOGIC;	
		 ps_busy : in std_logic;
		 good : out STD_LOGIC;
		 bad : out STD_LOGIC;
		 ps_start : out STD_LOGIC;
		 r_nwr : out STD_LOGIC;
		 transfer : in STD_LOGIC;
		 length : out STD_LOGIC_VECTOR(10 downto 0);
		 write_data : out STD_LOGIC_VECTOR(15 downto 0);
		 read_data : in STD_LOGIC_VECTOR(15 downto 0);
		 address : out STD_LOGIC_VECTOR(23 downto 0)
	     );
end psram_test;

--}} End of automatically maintained section

architecture psram_test of psram_test is   

	signal length_reg : unsigned(10 downto 0);
    signal address_reg : unsigned(23 downto 0); 
	signal wr_val : unsigned(15 downto 0); 
	signal n_blocks : unsigned(7 downto 0);	 
	signal timer : unsigned(15 downto 0);  
	signal read_errs : unsigned(23 downto 0);
	
	
	constant K_LENGTH : unsigned(10 downto 0) := "00000100000";			-- will use 32 word bursts to write

 	TYPE t_test_state is (PS_TST_IDLE, PS_TST_WRITE_0, PS_TST_WRITE_1, PS_TST_WRITE_2, PS_TST_WRITE_3, PS_TST_WRITE_4, PS_TST_READ_1, PS_TST_READ_2, PS_TST_READ_3, PS_TST_READ_4, PS_TST_READ_5);
	signal test_state : t_test_state;	

begin

	-- enter your statements here --
	psram_test : process(clk75)
	
	variable new_wr_val : unsigned(15 downto 0);
	begin
		if rising_edge(clk75) then	
			if res_hi = '1' then 
				good <= '0';
				bad <= '0';
				ps_start <= '0';
				length <= std_logic_vector(K_LENGTH); 
				test_state <= PS_TST_IDLE;
			else
				case test_state is
					when PS_TST_IDLE => 
					if start_test = '1' then
						good <= '0';
						bad <= '0';	
						wr_val <= (others => '0');			
						r_nwr <= '0';						-- write mode  
						n_blocks <= (others => '0');
						address_reg <= (others => '0');
						test_state <= PS_TST_WRITE_0; 		
					end if;	 
					
					when PS_TST_WRITE_0 => 
						address <= std_logic_vector(address_reg);
						write_data <= not std_logic_vector(wr_val);		   	-- write data = (not address(15 downto 0) ) 
						test_state <= PS_TST_WRITE_1; 
				
					when PS_TST_WRITE_1 =>
					if ps_busy = '0' then  					-- wait until access block is not busy
						ps_start <= '1';	 				-- start the write 
						n_blocks <= n_blocks + 1;			-- count of blocks of length words written
						test_state <= PS_TST_WRITE_2;
					end if;	
					
					when PS_TST_WRITE_2 =>
					if ps_busy = '1' then  					-- wait until access block is busy (ie has responded to start signal) 
						ps_start <= '0';
						test_state <= PS_TST_WRITE_3;
					end if;	
					
					
					when PS_TST_WRITE_3 =>
					if transfer  = '1' then					-- if the access block has read the data word
						new_wr_val := wr_val + 1;			-- calc new one
						write_data <= not std_logic_vector(new_wr_val);	 -- and output it
						wr_val <= new_wr_val;  
					elsif ps_busy = '0' then 					-- the data block has been written 
						if n_blocks = 16 then
							test_state <= PS_TST_WRITE_4;	
						else  
							address_reg <= address_reg + ("000000000000" & K_LENGTH); 		-- add block length to address
							test_state <= PS_TST_WRITE_0;
						end if;
					end if;
					
					when PS_TST_WRITE_4 =>	
						timer <= "0000010111011100";  	--1500;
						test_state <= PS_TST_READ_1;
						
					when PS_TST_READ_1 =>
					if timer = 0 then
						wr_val <= (others => '0');			
						r_nwr <= '1';						-- read mode  
						n_blocks <= (others => '0');
						address_reg <= (others => '0');
						test_state <= PS_TST_READ_2;
						read_errs <= (others => '0');
					else
						timer <= timer - 1;
					end if;
					
					when PS_TST_READ_2 => 
					if ps_busy = '0' then
						address <= std_logic_vector(address_reg);	
						n_blocks <= n_blocks + 1;			-- count of blocks of length words written
						ps_start <= '1';	 				-- start the write 
						test_state <= PS_TST_READ_3;
					end if;
					
					when PS_TST_READ_3 =>
					if ps_busy = '1' then  					-- wait until access block accepts start
						ps_start <= '0';
						test_state <= PS_TST_READ_4;
					end if;	
					
					when PS_TST_READ_4 =>
					if transfer = '1' then
						if std_logic_vector(wr_val) /= not read_data then
							read_errs <= read_errs + 1;
						end if;
						wr_val <= wr_val + 1;
					elsif ps_busy = '0' then
						if n_blocks = 16 then
							test_state <= PS_TST_READ_5;	
					    else
							address_reg <= address_reg + ("000000000000" & K_LENGTH); 		-- add block length to address
							test_state <= PS_TST_READ_2;
						end if;
					end if;	
					
					when PS_TST_READ_5 =>
					if read_errs = 0 then
						good <= '1';
					else
						bad <= '1';
					end if;
					test_state <= PS_TST_IDLE;
					
					
					when others =>
						good <= '1';
						bad <= '1';
					    test_state <= PS_TST_IDLE;
				end case;	
			end if;
	   end if;
	end process;  


end psram_test;

Extract from Simulation

image

Efinix Dashboard

image

Test Results Using Logic Analayser

Write burst

image

Final read burst - sets 'good' signal

image

Start of final read burst - can be compared with simulation results

image

Architecture of more useful controllers

The very simple setup described so far is fine to test that the ram chips are correctly connected, and that the FPGA can drive them at a useful speed.

A much more complex controller is required to do anything useful.

This is because the memory must be read or written in bursts to get any thing loke its best performance.

Suppose we want to use the memory as a buffer for a data acquisition system that will gather data from, for example, a multichannel ADC and send it on via a Gbit Ethernet interface.

We will need a write port and a read port which must operate simultaneously as far as the world outside the controller is concerned.

This can be done by buffering the write data in a FIFO using on FPGA memory and writing bursts of data to the memory. Data can be read from the memory into a second FIFO which may be read by the Ethernet controller. The memory controller must share the memory bandwidth between the two ports. This is a simple situation because both read and write are to/from sequential addresses. In a real application there may be requests from the Ethernet controller for out of sequence blocks of data if packets should be lost.

A huge jump in complexity occurs if non-sequential blocks of data must be written or read because the memory controller FIFO s must now store block lengths and addresses along with the data.

 

MK

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 3 years ago in reply to shabaz +1
    Those small adapters are quite expensive - I don't think I'll be buying any. To answer your question about how the ram signals connect up to the FPGA. The physical connections are: and the pins…
Parents
  • shabaz
    shabaz over 3 years ago

    Hi Michael,

    Interesting project! How does psr_dat_o and psr_dat_i connect to the two PSRAM chip SIO pins?

    It would be interesting to try the code (probably on a different FPGA board, I have a couple I could attempt it on), I need to get hold of of those chips.

    Incidentally, I found this thing on AliExpress, although I don't think it may be useful for your scenario, where trace length matching is needed to the real chip:

    6x8mm 1.27mm pitch

    That's for a larger device (6x8mm), I needed it for reading and programming a Flash chip. 

    However I just received it, and the quality is really good. So I'm thinking of getting the 3x3mm one (0.65mm pitch). 

    They also have 2x2mm (0.5mm pitch).

    I have no idea if the quality of the 3x3 and 2x2 will be the same as the 6x8mm one. The 6x8 looks darker than the 3x3 and 2x2 ones.

    This is what arrived:

    image

    Zoomed in:

    image

    Other side; I'll need to create a little PCB for this, to adapt to (say) 0.1" header pins, but I might also need an optional level converter on there too:

    image

    As mentioned I don't know if they would be useful for your performance scenario, these may be more useful for pulling data off chips etc.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 3 years ago in reply to shabaz

    Those small adapters are quite expensive - I don't think I'll be buying any.

    To answer your question about how the ram signals connect up to the FPGA.

    The physical connections are:

    image

    and the pins to VHDL looks like this:

    image

    How the 2 chips are connected in the FPGA design.

    The Efinix chips don’t use the usual method for connecting VHDL/Verilog to the outside pins but make use of their peripheral logic supported by the Interface Designer Tool.

    So the 8 bit IO port psr_dat is interfaced to the core logic by three 8 bit registers which can be named as the designer chooses.

    In this design they are psr_dat_i(7 downto 0) for input, psr_dat_o(7 downto 0) for output and psr_out_en(7 downto 0) for output enable.

    In the psram_access process there is code like this:

    if quad = '1' then

    psr_out_en <= "00010001";           -- enable drive on SI pins on both PSRAMS   

    else

           psr_out_en <= "11111111";

    end if;

     

    The signal ‘quad’ means that the switch to quad mode command is being transmitted in single data line SPI mode – so only one drive pin on each PSRAM chip is enabled. In actual quad mode working all the data pins are enabled to drive (at this part of the process).

     

    A more typical FPGA design (Lattice, Altera, Xilinx) would define signals for psr_dat_o and psr_dat_i and define psr_data as inout (if using VHDL). You would also need to define additional signals (single bit) for ls_bits_drive and ms_bits _drive.

    To read data in you would use code like:

    read_data <= psr_dat;

    To write data you would write it to the psr_dat_o signal:

    psr_dat_o <= write_data;

    Outside the process you would need code like this to control the pins.

    psr_dat(0) <= psr_dat_o(0) when (ls_bits_drive = ‘1’) else ‘Z’;

    psr_dat(4) <= psr_dat_o(4) when (ls_bits_drive = ‘1’) else ‘Z’;

    psr_dat(3 downto 1) <= psr_dat_o(3 downto 1) when (ms_bits_drive = ‘1’) else “ZZZ”;

    psr_dat(7 downto 5) <= psr_dat_o(7 downto 5) when (ms_bits_drive = ‘1’) else “ZZZ”;

    psr_dat_i <= psr_dat;

     

    On balance I quite like the Efinix way !

    You could either edit the psram_access module or add a translator at a higher level. I expect the synthesisre.fitter will end up with much the same thing in the end.

    Which FPGA are you thinking of trying ?

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to shabaz

    These psram chips are really neat. This micropython spi memory driver in 1-bit mode worked out of the box for me.

    https://github.com/peterhinch/micropython_eeprom 

    I could either access memory as a large bytearray or format a littlefs filesystem on it. Of course, the same is true for fram/flash serial memories too, so if you don't need more than say 16 MB you can just use a $1 flash chip versus an SD card!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to scottiebabe

    Ohh very neat! Nice that someone's already made the effort to port to Python, I'll be interested to try using it with Pico too at some point.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to michaelkellett

    I have a ICE40 dev-board, but figured this would be a good opportunity to lay out a custom board; going to prototype it first!

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 3 years ago in reply to shabaz

    If you are doing a new board, depending on what you want from it, it might be worth considering using the ICE40x5 parts in 48 pin QFN packages.

    ICE40UP5K-SG48I,  - Farnell even have stock !

    Tried to post a link to the spec sheet but no luck with Verint this morning.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 3 years ago in reply to michaelkellett

    image

    Working now, breakfast time rush over ?

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelkellett
    michaelkellett over 3 years ago in reply to michaelkellett

    image

    Working now, breakfast time rush over ?

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • shabaz
    shabaz over 3 years ago in reply to michaelkellett

    That's much nicer! I'd become so disillusioned about chip availability, I had not even checked to see what was now in stock.

    I don't need as much I/O, I'd rather have the huge increase in resources.