Personal Blogs
  • Community Hub
  • More
Personal Blogs
Michael Kellett's Blog Fast Test Amplifier - Part 1
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: michaelkellett
  • Date Created: 10 Aug 2018 5:04 PM Date Created
  • Views 1287 views
  • Likes 10 likes
  • Comments 9 comments
  • test amplifier
Related
Recommended

Fast Test Amplifier - Part 1

michaelkellett
michaelkellett
10 Aug 2018

A while ago (July 5th) in the discussion

 

https://www.element14.com/community/message/241748/l/programmable-frequency-generator#241748

 

I suggested an approach to building a low cost high frequency power amplifier.

The idea was to keep the design as simple as possible and base it on the classic 1970s bipolar transistor based HiFi power amplifier.

 

I've taken the idea a bit further and designed some boards, and finally got round to putting the parts on one and doing a bit of testing today.

 

The final schematic looks like this:

 

image

And the board looks like this:

 

image

 

I've been testing it cautiously using +/- 12V supplies (should be OK up to +/-18) and a 20 ohm load.

So far it looks quite good, small signal bandwidth is up to 10MHz but it can't do anything like full power at that frequency.

All the tests below were 12V pk-pk into 20 ohms:

 

Sine wave at 1MHz:

image

 

And the spectrum of the same:

 

image

 

Square wave at 500kHz:

 

image

 

And a close up to look at the slew rate:

 

image

 

So far it doesn't look too bad - quite a bit more testing to do and almost certainly some tweaking. I'm hopeful of meeting my target spec of 10W into 8 ohm load up to 2 MHz.

 

If anyone wants to build one I'll be posting the BOM and will put the Gerber files on Dropbox or similar.

 

MK

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 8 years ago +3
    Hi Michael, That's really neat, it could have science applications, or working with transducers. I'd be interested to replicate at some stage when you get the info posted. I've been busy on a DDS project…
  • DAB
    DAB over 8 years ago +3
    Nice update. Are you going to show the bandwidth response? DAB
  • three-phase
    three-phase over 8 years ago +3
    Looks like a very neatly laid out PCB. Kind regards
Parents
  • DAB
    DAB over 8 years ago

    Nice update.

     

    Are you going to show the bandwidth response?

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 8 years ago

    Nice update.

     

    Are you going to show the bandwidth response?

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • michaelkellett
    michaelkellett over 8 years ago in reply to DAB

    Here's a plot of the small signal (1.7Vpk-pk) frequency response, still 20 ohm load. Some more work perhaps to tame the HF peaking (not too grim at about 3dB but should be less).

     

    image

     

    I've been using a Picoscope 5444 to do these measurements and used the free response plotting app that will work with it and any other signal generating Picoscope.

     

    I'm very impressed with the Picoscope, the hardware of the front end isn't quite up with the big four (Keysight, Tek, R & S or LeCroy) but the price runs at a small fraction (maybe 10 - 20%).

    The basic control software is good and things like decoders or FRA are free.

     

    Back to the amplifier - my plan is to use it with a control pcb which will buffer and bandwidth limit the input  as well as manage DC offsets and power supply regulation. You may have noticed the tap off point at R33/34 - this will allow the control board to measure DC offset on input and output and inject a compensating DC offset so that there is no overall DC  error but without resorting to AC coupling. Because this requires an offset injecting DAC it will also be possible to deliberately dial up any DC offset you like. The Rigol offers this feature and I wonder if they have gone down the same path to get there ...

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to michaelkellett

    michaelkellett  wrote:

     

    Here's a plot of the small signal (1.7Vpk-pk) frequency response, still 20 ohm load. Some more work perhaps to tame the HF peaking (not too grim at about 3dB but should be less).

     

    image

     

    I've been using a Picoscope 5444 to do these measurements and used the free response plotting app that will work with it and any other signal generating Picoscope.

     

    I'm very impressed with the Picoscope, the hardware of the front end isn't quite up with the big four (Keysight, Tek, R & S or LeCroy) but the price runs at a small fraction (maybe 10 - 20%).

    The basic control software is good and things like decoders or FRA are free.

     

    ..l

     

    MK

    That ‘ll be a lesson for me. I used to see the picoscope as “not real compared to real scopes”. You’re opening my eyes.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 8 years ago in reply to Jan Cumps

    I too have been using a picoscope, just the basic 10MHz version, but I love the big screen, data capture and analysis capabilities.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down