Personal Blogs
  • Community Hub
  • More
Personal Blogs
Michael Kellett's Blog Hiland Power Supply Testing
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: michaelkellett
  • Date Created: 23 Mar 2020 4:00 PM Date Created
  • Views 1996 views
  • Likes 4 likes
  • Comments 3 comments
  • power_supply
  • test instrumentation:
Related
Recommended

Hiland Power Supply Testing

michaelkellett
michaelkellett
23 Mar 2020

23/03/2020

 

This project was sparked off by John's blog:

One of My Favorite Building Blocks

jw0752

I've been thinking about power supply designs and read John's blog just after reading the power supply project in "The Art of Electronics, The X Chapters" (ISBN 978-1-108-49994-1).

The AOE design is rather complicated so I decided to try this board first. I bought mine from Amzon https://www.amazon.co.uk/gp/product/B077G8PK9Y/ref=ppx_yo_dt_b_asin_title_o06_s00?ie=UTF8&psc=1

They took a while to come and cost a bit more than John paid.

 

I built on the other day, the 56k resistor was missing and the resistors were possible the worst quality I've seen in 20 years but everything works. If you wanted one of these to be reliable it would be worth considering buying better resistors. But I wasn't interested in reliability but in how well the basic design works.

 

I started off with the power supply board powered by an AIM TTi bench supply supplying -4.5V limited to 50mA and +20V limited to 3.5A. For the load I used a Rigol Electronic load DL3031A, set for a steady current of 0.5A and a pulse current of 3A for 100ms. The power supply board was set for an output of 15V and the current limit at about 1A.

 

image

 

 

image

 

The scope trace shows the rather horrible result. The blue trace is the supply output, the purple trace is the current (actually voltage across R) and the yellow is the voltage on the output of U3.

It takes a bit of thought to work out what's happening, it helps to have John's nicely annotated schematic:

image

 

When steady with an output current of 0.5A, well below the limit setting, there is about 1/4V across R7 and the ouput of U3 idles at about +18V.

Once the load starts to draw extra current U3 's output starts to drop but takes a very long time to get below the voltage output demand on the anode of D9.

The load current peaks to more than the 3A I set it for, reaching a maximum of about 4.3A. The it drops back to the programmed 3A until current through D9 starts to reduce the voltage demand.

If the electronic load was a perfect current sink the current would not reduce at this point but it has limited slew rate.

The output of U3 goes -ve and eventually, about 5.5 divisions from the start, the load current drops to zero.

U3 output rises because there is no longer an over current and the output voltage rises a little. Then the Rigol load shows it's true colours and suddenly demands 5A or more.

I think this is because it winds up the internal current demand if there is no applied voltage.

Of course the power supply current limit action repeats and we get the horrible oscillation.

 

The next step is to prove this analysis, so I replaced the Rigol load with a 23.5R resistor in series with 3.3R resistor and a big MOSFET driven by a pulse generator to short the 23.5R.

 

image

 

This gave the scope trace below:

 

image

 

This is much more respectable, there is still a long time before the current stabilises at the limit level (230us) and it spends a scary 100us limited only by external resistance.

The really hideous second current pulse is clearly a problem with the load.

 

 

More testing to do, but so far the £9 power supply is probably doing its job a bit better than the £1200 electronic load.

 

I'm not quite sure why the output of U3 changes so slowly - first thing is to use a known real TL081 - I'm testing with the chips that came with the board.

 

 

Replace U3 with a known real TL081:

 

image

 

That's a dramatic improvement - overcurrent time down to 42us from 92us, U1 won't matter much but U2 will - I changed them both for good parts.

 

image

 

That gets the overcurrent time down to 36us and improves the current control a lot.

 

So John was right - throw away the "TL081"s that come with the kit !

 

And be very cautious about all the other bits too !

 

The basic design is not that bad - I'll see if I can think of  a mod that will improve that dead time while U3 slews 20V to get the voltage down.

 

MK

  • Sign in to reply

Top Comments

  • DAB
    DAB over 6 years ago +2
    Nice project. You definitely need to verify the specs on any of these cheap products. DAB
  • jw0752
    jw0752 over 6 years ago +1
    Hi Michael, Thank you very much for the time and effort you spent on the Hiland Board. I have printed your blog and I will put it with my file on the unit. I was very happy to see that the unit greatly…
  • colporteur
    colporteur over 6 years ago +1
    Those are some big *** load resistors! What ever happened to a string of light bulbs? Enjoyed reading the project.
  • colporteur
    colporteur over 6 years ago

    Those are some big *** load resistors! What ever happened to a string of light bulbs?

     

    Enjoyed reading the project.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 6 years ago

    Hi Michael,

     

    Thank you very much for the time and effort you spent on the Hiland Board. I have printed your blog and I will put it with my file on the unit. I was very happy to see that the unit greatly improved with the OEM TL -81 Op Amps. When I first started buying these a few years ago they came with quality parts including the ICs but recently the parts have been coming with junk replacements. Still for $4 or $5 dollars I still like them.

     

    Thanks

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 6 years ago

    Nice project.

     

    You definitely need to verify the specs on any of these cheap products.

     

    DAB