Browse By Tags

  • Measuring DC-DC converter Efficiency

    This blog is about my test rig for measuring DC-Dc converter efficiency in the range Vin/Vout 2-50V and Iin/Iout 1-10A. It can also be used to measure the power consumption of DC systems in same range. The test rig ready to run (power supply and device…
  • An isolated low noise +/-5V DC power supply

    Introduction I’m working on test rig for accurately measuring the efficiency of DC-DC regulators or converters. It uses 2 precision current shunts to measure the input and output current. These need very low noise pre-amplifiers which must each be powered…
  • Silent Switcher - LT8640s meets KiCad

    The first part of this project kicked off with a blog “First Design with KiCad (8.0)” about 4 weeks ago. The idea was to build a replacement for obsolete TO3 can linear voltage regulators using the Linear Technologies (now owned by Analog Devices) LT8640s…
  • Does anyone knows. How a duracell powercheck feature works ?

    Does anyone knows. How a duracell powercheck feature works. I need complete detail about it. like what is the current consumption, resistance of the strip etc.
  • First Design with KiCad (8.0)

    I’ve been using the same PCB design software for over 20 years (Easy PC) and it’s served me well during that time. It’s had an update pretty much every year and it can still load files from 20 years ago. It hardly ever crashes and I’ve probably designed…
  • ANP117 | Impact of output capacitor on feedback loop stability of a power supply

    APPLICATION NOTE Impact of output capacitor on feedback loop stability of a power supply ANP117 by Eleazar Falco 1. INTRODUCTION AND THEORETICAL BACKGROUND A switching power supply requires one or more capacitors across the output voltage rail…
  • Maintain power long enough for SBC to power down

    Hello, I have connected my 3D printer to an Orange Pi Lite running Octoprint as it is much more user friendly when it comes to managing my prints. This works just fine but required an additional power source and so I opened the printer and connected…
  • LED Worklight and teardown

    My workshop areas have eight 4 foot double tube fluorescent worklights in the man-cave. I installed the 4 foot floursecent fixtures 35 years ago. As the tubes fail, they get consolidated, and one by one empty fluorescent fixtures get replaced with LED…
  • diode zener

    HI can any one help me to know the refernce of zener diode1 "ZD1" in this board XP POWER VFT80US24
  • Designing my first AC Mains Filtering Circuit - what are the jellybean components

    I'm working with some Power-Line Communication modules. Here is an example of the sort of module I'm talking about: store.rakwireless.com/.../lx200v50-evb-power-line-communicationplc-module These would be using the same technology as you would find…
  • ANS019 | Bipolar power supply and isolated signal transmission with MagI³C-FIMM

    Application Note Bipolar power supply and isolated signal transmission with MagI³C-FIMM ANS019 BY Timur Uludag 01. INTRODUCTION Industrial plants, such as warehouse logistics, filling plants, rolling mills, conveyor belts and printing presses…
  • Single Phase to three signal generator.

    Hello everyone, I am designing a low voltage power supply that will run single phase to three phase circuit and will be using ultrosonic frequency as its signal input. The current circuit design uses three operational amplifiers that has a 60 degress…
  • Heatsinks

    Recently /members/andrewj posted about some issues with heatsinks. It so happened that he was thinking of using heatsinks similar to one I'd already chosen for a resistor based adjustable load. I'd run into some issues using active loads with a power…
  • Inaccurate Readings from Thermal Imaging Camera on Copper Heatsink-Anyone Else Had this Happen?

    I have a Fluke Ti25 Thermal Imaging Camera that I used on a 1,200 watt PFC Controller to measure the power FET and power diode temps. The Fluke camera has an adjustment for emissivity, which I set to copper (I don't recall the value). I chose this as…
  • What happens if remote sense leads open?

    This post and other great tips and tricks for Keysight Power Products can be found on the Watt's Up? blog . For more information on Keysight Power Products visit: www.keysight.com/find/power Wednesday, October 31, 2012 What happens if remote sense leads…
  • What is a bipolar power supply?

    This blog post and other great tips and tricks for Agilent Power Products can be found on the Watt's Up? blog . For more information on Keysight Power Products visit: www.keysight.com/find/power Friday, October 26, 2012 What is a bipolar (four-quadrant…
  • Power Supply Resolution versus Accuracy

    This and other great tips and tricks on Power Products can be found on Keysight's Watt's Up? blog. For more information on Keysight Power Products visit: www.keysight.com/find/power Power Supply Resolution versus Accuracy One of the questions that we…
  • Tips to prevent voltage droop from tripping low voltage detection circuits

    This and other great tips and tricks can be found on Keysight's Watt's Up? Blog . More information on Keysight Power Products can be found at: www.keysight.com/find/power Thursday, January 31, 2013 Tips to prevent voltage droop from tripping low voltage…
  • New microchip can provide its own power

    Chances are the microchip your using in your computer, phone, or Teddy Ruxspin is being powered by some electrical source other than their own. While that’s the norm with today’s microchips, the future may bring chips that can be powered by their own…
  • Identifying the Triplets in a Power Supply Front End

    There are three components routinely used in the power input section of many linear and switching power supply that have confused me over the years and have often been difficult to identify. In this blog I would like to call your attention to them, show…
  • Design a Digital Power Supply in just 3 days !

    to Coordinated Universal Time
    Munich - Garching
    Biricha Digital's Collaboration with Texas Instruments is focussed on providing Digital Power Supply design workshops. http://www.element14.com/community/docs/DOC-35973/l/design-a-digital-power-supply-in-just-3-days--ti-design-workshop-munich
  • Desin a Digital Power Supply in just 3 days !

    to Coordinated Universal Time
    Milan
    Biricha Digital's collaboration with Texas Instruments is focussed on providing digital power supply design workshops. http://www.element14.com/community/docs/DOC-35972/l/design-a-digital-power-supply-in-just-3-days--ti-design-workshop-milan
  • FREE Farnell and ADI webinar: Switch Mode Power Supply Critical PCB Layout Rules and Advances in Switching Regulators

    to Coordinated Universal Time
    Online
    Overview of topic: The board layout of a switch mode power supply is key in any DC/DC converter design. Following a few simple rules will improve the power design dramatically and will help to pass EMI tests. Also Advances in switching regulators with...
  • Dc-Dc Point of Load Apps: Accelerating device selection, circuit design and simulation w/IR's SupIRBuck On-line Design tool

    to Coordinated Universal Time
    Webinar
    Join Cahit Gezgin, South Central FAE, as he discusses the use of the SupIRBuck on-line design tool for accelerating design cycle as compared to manually selecting, matching and testing high and low side FETS in Point of Load applications. He will demonstrate...