Personal Blogs
  • Community Hub
  • More
Personal Blogs
Michael Kellett's Blog PCB micro surgery.
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: michaelkellett
  • Date Created: 1 Feb 2026 12:14 PM Date Created
  • Views 505 views
  • Likes 15 likes
  • Comments 8 comments
  • soldering
  • flux
  • surface mount
Related
Recommended

PCB micro surgery.

michaelkellett
michaelkellett
1 Feb 2026

Soldering tiny pull-up resistors to a TSSOP package.

Spurred on by  Jan Cumps recent (and on-going) review  of the Weller Micro Soldering Kit I decided to buy some de-soldering tweezers.

I used to have an Ersa soldering station with tweezers but they made that line obsolete many years ago and I usually use two soldering irons, one in each hand, rather than tweezers.

It's a reasonable approach for some things but not perfect.

I went for what felt like a mid price system (might be more low price), YIHUA 982D-1 PRO at about £250 for iron and tweezers. It uses the common C120 and C245 tips.

I bought mine from Amazon  - you may get it a little cheaper from Aliexpress.

This isn't a review of the YIHUA - suffice to say that it works fine, seems to be reasonably well made, has a nice clear display - and uses widely available tips.

It looks like this:

image

image

And has a weird tilting screen feature:

image

image

So - enough background - now for the problem.

I'm working on bringing up a board which is part of a set of three which make up a quite complicated power supply with super capacitor backup. I hit a snag where, because I had used the LSF02024 level shifter before, I thought I knew how it worked. It turns out that I didn't - it IS bi-directional but is not symmetrical - one side is push pull drive but the other is open drain. I used it the wrong way round and was confronted by the need to bodge in 4 pull up resistors in a hurry and with not very good access to the relevant tracks on the board.

I decided the easiest way to do would be to use a tiny resistor array that would line up with the pins on the LSF0204 and could be soldered directly to them.

Farnell sell a suitable part:

image

But I didn't want to waste Sunday and Monday waiting for them to arrive. My son suggested scavenging from some old gear. Obviously only quite new old gear contains suitable parts  - the first few old video boards drew a blank but I found some 2 way 1k arrays in an HP computer.

The new de-soldering tweezers did there first real work and removed two resistor arrays - there were no problems but I can't use the camera microscope to take pictures and tweeze at the same time - I tried  but need more practice.

Once the arrays were out I used a spiky tip on the new iron to solder the arrays and a tiny bit of connecting wire to the chip. The trusty Wartons Future 315 flux came into play. You can see the mess it leaves in the picture. The C245 type soldering bit does a good job getting a fair bit of heat through the tiny spiky point.

image

The second picture shows the board after two rinses with isopropyl alcohol. Using Safewash in the ultrasonic cleaner does a much better job but takes much longer   - this will do for now. I've also cleaned up some mess I made on the adjacent chip when adding some debugging wires.

image

So there it is - how to add un-expected pull up resistors. (And a reminder, if one is needed, that you should never throw stuff away - even a dead computer can be a source of useful parts !)

MK

  • Sign in to reply
Parents
  • DAB
    DAB 8 months ago

    Nice work.

    Your eyesight and skills are beyond mine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB 8 months ago

    Nice work.

    Your eyesight and skills are beyond mine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • michaelkellett
    michaelkellett 8 months ago in reply to DAB

    It's all done by trickery.

    Id the soldering under the camera microscope - it takes a little while to learn to make your hand do what you want while looking up at the screen rather than down at what you are doing - but once you get used to it then it is a huge step forward.

    A cheap C lens camera with a stand and decent sized monitor (27" in my case) is way better than a multi thousand dollar optical microscope (IMO !).

    The trick with precision manual work is to arrange support for your hands  - no one is steady enough to keep the soldering iron tip within a few thou of where it is wanted while supporting the weight of their hands - so arrange for them to rest on the bench or suitable spacer, and learn to control the tip position by rotating or sliding your hands and flexing your fingers. In extreme case finger support may help.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps 8 months ago in reply to michaelkellett

    These work best for me: magnifiers in a hat

    image

    Caveats:

    • range is not excellent, so you are somewhat bent over the work area
    • solder rest is usually out of focus. You have to look "under the glasses" to aim the iron in its rest
    • I get motion sick when using the X8. My preferred pair is x2.5 
    • my partner takes photos of me wearing them, and posts them on social media