Personal Blogs
  • Community Hub
  • More
Personal Blogs
Michael Wylie's Blog Distributed Fiber Optic Sensing - A Taste of What's to Come
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: michaelwylie
  • Date Created: 23 Apr 2014 3:56 AM Date Created
  • Views 679 views
  • Likes 1 like
  • Comments 2 comments
  • fiber
  • temperature
  • optical
  • sensor
Related
Recommended

Distributed Fiber Optic Sensing - A Taste of What's to Come

michaelwylie
michaelwylie
23 Apr 2014

Over the last 30 years or so, a lot of research has made distributed fiber optic sensors a viable option in the commercial market. This blogpost will discuss the idea of distributed sensing in general with regard to temperature. Our cars tell us the temperature, our phones look up the local temperature for us ... we basically have temperature sensors everywhere. But these sensors are limited, in the sense that they are measuring the temperature at a single point in space. Figure 1(a) shows the classic LM335 temperature sensor that most of us are familiar with.  Suppose we wanted to not only know the temperature at a single point, but at multiple points along, say, a pipeline. Historically we would place many temperature sensors along the beam and multiplex the signals to read the temperature gradient along the pipe or we would hold the gradient in question steady and use a single sensor to make discrete measurements along the pipe (see the bottom of Figure 1 (a)). This is terribly inefficient and only practical in a laboratory setting.

 

Now, hopefully you are asking, "why would I care about the temperature along a pipeline?" One good example would be natural gas pipelines, which deliver natural gas via pressurized pipelines. When a pipe ruptures, the expanding gas causes a localized temperature drop in the vicinity of the leak. If you could detect this temperature drop, you could shut down the pipeline, hopefully before anything catastrophic occurs.

 

image

Figure 1: (a) - Traditional LM335 Temperature Sensor and a (b) Multiplexed Temperature Profile Scheme.

 

Enter the invention of distributed fiber optic sensing. Fiber is a long, very thin piece of glass. It turns out, that not only is this piece of glass great for transmitting signals but it also has other properties that make it one very long temperature sensor. Based on the method used to take the readings, the temperature can be resolved to within the spatial resolution of the interrogating system. Figure 2 shows what would be a typical result from a distributed fiber sensor. This graph shows an entire temperature profile over the length of a fiber (distance). Any temperature read from the graph will have an accuracy and a spatial resolution. The spatial resolution refers to the potential error of the distance where the event in question occurred. For example, in the graph of figure 2 temperature T1 occurs at position X1. Let T1 be 90 °C and X1 be 4.5 km. If the spatial resolution were 100 meters, the temperature T1 could occur anywhere between 4.4 km and 4.6 km.

 

Fullscreen contentimage_31074.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

Figure 2: (a) - Typical Temperature Profile from a Fiber Distributed Sensor.

 

 

This concludes the first post on distributed fiber sensors. Look for more information next time!

  • Sign in to reply

Top Comments

  • DAB
    DAB over 12 years ago +1
    Having watched the Fiber development over the last four decades, I have been amazed at some of the applications that have come forth. I have seen fiber speed go from KHz to THz with just about everything…
  • COMPACT
    COMPACT over 12 years ago in reply to DAB +1
    I was amazed with what we did with DSPs managing to get 56Kbps from a 3KHz bandwidth copper phone line! When I first started it was 110bits per second.
Parents
  • DAB
    DAB over 12 years ago

    Having watched the Fiber development over the last four decades, I have been amazed at some of the applications that have come forth.

     

    I have seen fiber speed go from KHz to THz with just about everything in between.

     

    I do think that a broader range of sensors can be integrated with optical fibers, especially with some of the Graphene development.

    Integrating sensors to Fiber taps would enable a good way to take remote measurements with minimum signal noise in the RF regions.

    I wish there were a simple kit that would enable makers a chance to integrate Fiber to the embedded world.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 12 years ago

    Having watched the Fiber development over the last four decades, I have been amazed at some of the applications that have come forth.

     

    I have seen fiber speed go from KHz to THz with just about everything in between.

     

    I do think that a broader range of sensors can be integrated with optical fibers, especially with some of the Graphene development.

    Integrating sensors to Fiber taps would enable a good way to take remote measurements with minimum signal noise in the RF regions.

    I wish there were a simple kit that would enable makers a chance to integrate Fiber to the embedded world.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • COMPACT
    COMPACT over 12 years ago in reply to DAB

    I was amazed with what we did with DSPs managing to get 56Kbps from a 3KHz bandwidth copper phone line!

    When I first started it was 110bits per second.