Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen: Component Documentation: Annunciator, SELCAL, Custom
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 29 Nov 2022 11:39 PM Date Created
  • Views 2400 views
  • Likes 6 likes
  • Comments 12 comments
  • flight simulator
  • nexgen
  • diy hardware
  • diy cockpit
  • arduino mega 2560
Related
Recommended

NexGen: Component Documentation: Annunciator, SELCAL, Custom

phoenixcomm
phoenixcomm
29 Nov 2022

NexGen: Component Documentation: Annunciator, SELCAL, Custom

SELCAL is a signaling method that can alert an individual aircraft that a ground station wishes to communicate with it even if the radios are muted. SELCAL signals can be transmitted over either HF or VHF RTF. A SELCAL transmission consists of a combination of four preselected audio tones which takes approximately two seconds to transmit
Below the table shows the letters and their associated frequency.

CODE FREQUENCY CODE FREQUENCY CODE FREQUENCY CODE FREQUENCY
A 312.6HZ E 473.2HZ J 716.1HZ P 1083.2HZ
B 346.7HZ F 524.8HZ K 794.3HZ Q 1202.3HZ
C 384.6HZ G 582.1HZ L 881.0HZ R 1333.5HZ
D 426.6HZ H 645.7HZ M 977.2HZ S 1479.1HZ

I had an old SELCAL unit that was in pieces, so it become my doner. I will have to make the unit's aluminum backplate 5 3/4" wide and will be .375" x 3 which is 1.125" in height. the .375" is center to center of a Dzus rail1, 2.  After which I will print the front plate with the proper clearances for the two Dzus fasteners on each side. There are 3 lights: HF Com #1, HF Com #2, and SATCOM Msg, and they will be driven by three relays. There are also 2 volume controls, Audio, and Tone. The Arduino Mega will also provide the audio tones. and the two-volume controls are potentiometers, the Arduino will give up 2 of its analog inputs for measuring the voltage of the pots.
The lamps are 23 mm x 11mm and they mount by the use of a sleeve behind the panel they were made by Ducommun part number 30288RBS1-2.
The pots were also salvaged from the unit the volume pot is 250Ω with an on-off switch, the tone pot is 10kΩ with a push switch incorporated as well. Unfortunately, I can't find the part number and there were no manufacturer marks or 5-digit cage code. The 250Ω pot has a part number of C0162080 and the 10kΩ part number is C0162081. They have date codes 9641 and 9642, which means most likely they were made in 1996 and the 41 and 42 weeks of the year. 

When I'm stumped for parts numbers or manufacturers, I use my way back machine catalog  image image

#106 from Newark Electronics. And they were not there!

footnotes: 

  1. Quarter Turn - PA-3500 Line Receptacles
  2. Panel building focussed on dimensions. “It’s all in the inch...Slight smile”
  • Sign in to reply
Parents
  • Jan Cumps
    Jan Cumps over 3 years ago

    Side story: my first IT job was a c++ developer in a company that wrote software for aviation, rail and harbor industry. One aspect was in-flight aircraft communication (ACARS). I never worked on that :).

    There are still a few screen shots online of software I wrote in the mid-90s for airport ground handling and management of the now defuct German Mitropa railroad company.

    image

    image

    image

    image

    image source: B.Rekencenta N.V.
    software: me

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 3 years ago

    Side story: my first IT job was a c++ developer in a company that wrote software for aviation, rail and harbor industry. One aspect was in-flight aircraft communication (ACARS). I never worked on that :).

    There are still a few screen shots online of software I wrote in the mid-90s for airport ground handling and management of the now defuct German Mitropa railroad company.

    image

    image

    image

    image

    image source: B.Rekencenta N.V.
    software: me

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Jan Cumps

    these screens use MVC (model view controller) in Microsoft MFC. If you see 3 or 4 views in the same screen, they all operate on the same data model.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 3 years ago in reply to Jan Cumps

    neet. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 3 years ago in reply to phoenixcomm

    Now all I need to do is draw it in CAD but I don't know one except tinkerCAD and measurements are kind of crappy. When I was in college I use to use Autocad (2D) but now every thing is in 3D and I can't get started. LOL

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to phoenixcomm

    Would a base model to import into TinkerCAD help any?

    I couldn't see any photos of 3 Dzus unit high SELCAL units online, most are 4 Dzus units high.

    From what you describe and the attached resources above, I ended up with something like this:  

    image

    which may be completely wrong... Slight smile

    I started out with AutoCAD (2D) v2.0 when it fitted on a single floppy disk. It's changed a little bit since then.

    However, most of the above can be done in 2D layers with a final extrude to 3D.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 3 years ago in reply to beacon_dave

    I'm wrong. the unit should be 38.10.mm high and the holes from edge to center are 9.525mm. To fit I will need the equivalent of 3 diameters in the center + 2  1/2 for the plate edge. where the aluminum backplate holes are 6.4mm.