Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen: Fuel Indicator: Testing The Display
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 4 Nov 2020 7:49 PM Date Created
  • Views 4089 views
  • Likes 6 likes
  • Comments 19 comments
  • flight simulator
  • nexgen
  • arduino mega 2560
  • hdsp-213x
  • can bus
  • diy aircraft cockpit
  • recycleretrofitch
  • canaerospace
  • c progrmming
  • diy electronics
  • i2c expander
Related
Recommended

NexGen: Fuel Indicator: Testing The Display

phoenixcomm
phoenixcomm
4 Nov 2020

imageThis picture on the left is just to remind you all of what I am trying to get working.  Each HDSP-2131 display has 24 pins that give you 48 pins to deal with. Now let us complicate the issue the pins come out on a 30-pin connector of which 4 are for power and ground. So now I have 28 pins for the interface.image

Other people have used similar displays ie  Wise Time with Arduino and others. Most implementations I have seen use a Flip-Flop to load the characters, but why go to that solution? The Arduino Mega 256  has only 54 digital GPIO pins. My pin count is higher as  I needed 20 pins +  8 Data  = 28 pins + 5 pins for my switches (reduced to 3-bit BCD and one interrupt pin), CAN module on pins 53, 52, 51, 50,  and the USB driver and interrupts.  This makes my head hurt! image

So I freed up my 8-bit Data-Ports pins by using an 8-bit I2C port expander which is mounted on the same  PCB that holds the 30-pin header that the display plugs into.

 

image

My biggest problem is that the CAN libraries (Arduino) are Master-Slave.
But CANbus is democratic which means any node can become the Master.
  And this is where the problem lies.

I still don't have a clue where to mount my Arduino Mega. image  My CAN bus modules output will be routed to a USB-A  or an RJ45F connector.

So to speed up testing before  I use my jumpers.  The only pins I will be Wire-Wrap will be the Data Port to the display header.

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 5 years ago +1
    It's a lot of hardware and a lot of pins to deal with. Is your goal to stick with the original technology? I see you lower the count by using the expander. Maybe we can work together here to create a design…
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to DAB +1
    DAB Nope I pan on using CANaerospace which is built on top of CAN specification itself, which is also "democratic". So there is more work than I can do in 10 days. ~~ Cris
  • michaelkellett
    michaelkellett over 5 years ago in reply to michaelkellett +1
    Actually you don't need that many pins, I think you can common all the pins on the display chips except /CE, so for two displays you need only 15 pins on the processor. An ATmega168 in a 28 pin DIL package…
Parents
  • Jan Cumps
    Jan Cumps over 5 years ago

    It's a lot of hardware and a lot of pins to deal with. Is your goal to stick with the original technology?

    I see you lower the count by using the expander.

    Maybe we can work together here to create a design that uses the same display but avoid that the microcontroller needs to drive that many individual I/Os.

    CAN alone should be enough to tell the display what to do. The rest could be added to the display unit by adding a single CAN-aware microcontroller close to the display ...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to Jan Cumps

    Jan Cumps  In CAN aerospace there is a lot going on the CAN bus itself.

    First, you have to deal with the "heartbeat" (node 0), this happens every so often each node responds with its status good, bad, or whatever.  What heartbeat does it let you do is to add or removes nodes at will. Without a power down.

    Two, you have to deal with receiving a query for this node, as this node can respond to over eight addresses. this is normally handled by filtering.

    Three, you have to deal with its switches, and outbound messages.

    This would be to FILL tank number 4.

    First, you would have to move the up/down  switch appropriately till the lower display indicated #4

    Second, you will receive 20 from the host

    Third, you will receive  tank 4 max = 30

    Forth, the lower display now indicates #4 20 - 30

    Fifth, You now raise FILL sending a message to the host.

    Sixth, the lower display now displys, #4 - 30G

    Seventh, The upper display will display the weight (load) of fuel in tank #4

     

    also take al look at the spec. https://www.stockflightsystems.com/tl_files/downloads/canaerospace/canas_17.pdf

    one of the cool things most nodes they have  the parameter name, Suggested Data Type,  Units, Note;

    if you look up nodes 668-675 (34.57), Fuel Tank # quantity, FLOAT SHORT2, kg but here kg is, not appropriate as fuel is pumped in US Gallons.  This is the job of the crew chief to do the conversion for weight and balance.   Car and AVi Gas both come in at 6.36 pounds per gallons. So my weight in tank #4 with 20 USG is 127.2 pounds or × 0.45359237 = 57.696949464 kg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to phoenixcomm

    Yes but in the end you want to display something simple on the simplest of displays. Abstract a little?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to Jan Cumps

    Jan Cumps  Simple?  Sujestions Pelase

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 5 years ago in reply to phoenixcomm

    Why not use a little processor (or even FPGA) on a board right next to the display pcb and let it talk to your CAN controller via a two wire UART interface. By far the neatest solution would be to design a pcb of your own for it but you might find something ready made. A 64 pin processor should have enough IO pins for your display. Does the display work with 3.3V logic - if only 5V then that will impact your choice of micros but I think there will be  AVRs that will do.

     

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelkellett
    michaelkellett over 5 years ago in reply to phoenixcomm

    Why not use a little processor (or even FPGA) on a board right next to the display pcb and let it talk to your CAN controller via a two wire UART interface. By far the neatest solution would be to design a pcb of your own for it but you might find something ready made. A 64 pin processor should have enough IO pins for your display. Does the display work with 3.3V logic - if only 5V then that will impact your choice of micros but I think there will be  AVRs that will do.

     

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • michaelkellett
    michaelkellett over 5 years ago in reply to michaelkellett

    Actually you don't need that many pins, I think you can common all the pins on the display chips except /CE, so for two displays you need only 15 pins on the processor.

     

    An ATmega168 in a 28 pin DIL package would do - you could design a little pcb which should plug onto your display board - and connect via UART  (or I2C if you must) but UART interfaces can reliably support long distances but I2 C can't. By putting intelligence on the display you can send high level commands to it.

     

    On reflection I'm not at all sure that these suggestions are addressing your problem .................

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to michaelkellett

    michaelkellett I'm really not up to par with an  FPGA or have the tools, and PCB boards I would have to go and lay out the damn thing. for me, Wire-Wrap is still the way to do it.

    I have Arduino Megas laying around, I think maybe a TI Stellaris LaunchPad would be far better (ARMRegistered CortexTm-M4F-based microcontrollers) I even have one of the larger boards which has two complete set of a dual row of pins. + Ethernet! Lots of IO

    ~~ Cris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to michaelkellett

    michaelkellett  The above solution is sort of what I have, from the factory,  Adress and Data lines, as well as the Write line, is shared be between both the Upper and Lower Display, which is 14pins,  what you end up with is 6 lines per display that are not shared so that's  12pins. So I need  26 pins.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to michaelkellett

    michaelkellett I think your pin math is way off you say I only need 15 pins ouch! Data = 8pins,  Address = 5 pins, Control = 7 pins so that's 20 pins!  I don't want to make a new PCB for the display. You should understand part of my mantra: please read NexGen: Audio Panels Ins and Outs I am using the original display PCB. If I try and remove the display and screw it up, I'm out $150.00, so removing and rebuilding the display PCB is a non-starter. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 5 years ago in reply to phoenixcomm

    I missed the address pins, still the basic idea holds, the suggestion was not that you remove the display chips from their boards but make a board that would plug into the exisitng display board. But the only picture I have to work on is the one with you holding the board in your hand.

     

    MK