Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen: Fuel Load Indicator: Pinouts Redux
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 22 Sep 2020 3:47 PM Date Created
  • Views 856 views
  • Likes 5 likes
  • Comments 2 comments
  • flight simulator
  • nexgen
  • diy hardware
  • recycle & retrofit
  • fuel load indicator
  • diy software
Related
Recommended

NexGen: Fuel Load Indicator: Pinouts Redux

phoenixcomm
phoenixcomm
22 Sep 2020

I have decided to update my Fuel Load Indicator which has only outputs for a human. My goal is to Recycle & Retrofit this indicator so that it can talk over the CANaerospace network. The network responds to node 0 for multicast, and also nodes 668 - 675 (tank_1 - tank_8).image

I have not been able to get the display to fire up with the pinouts here. Starting from the beginning I have gotten somethings wrong, ie the pinouts of the display connector.
On most IDE connectors the side with the notch is pin 1 on the right.
Not so this time the side without the notch and on the right. So here are the pinouts that I have found.
I have identified pin 1 by looking at the pins on the bottom of the display under magnification, and I found one of the pads square notifying pin #1.

The table on the right is correct for pin-outs (I hope)  ---> (DB-b has a notch, DB-a does not)

Pin-Outs
DB-aDB-bFunction
1A4
2Vdd
3A3
4
5RSTU1
6RSTU2
7CLKU1
8D7U1
9CLKU2
10D7U2
11RDU1
12CEU1
13CEU2
14RDU2
15
16WR
17FL
18
19A0
20A2
21A1
22D2
23D3
24D1
25D0
26D5
27GND
28GND-LOGIC
29D6
30D4

 

One day God called the Devil, and asked "How are things going in hell?"
The Devil responded, "Great we have flush toilets, elevators, and air conditioning!" God said, "Wow how did you do all that!?"
The Devil said I got my self an engineer.
God said, "You were not supposed to get the engineer; Return him at once."
The Devil said, "NO!"
God said, "I'll sue!"
The Devil said, "And bother of mine where are you going to get a lawyer?!"

Comments

 

I originally thought that the control lines were tied together.image

( He should find his way to engineer hell)

Signal  TypeSizeColor
Data Bus8
Address Bus5
U1 Control Lines5
U2 Control Lines5
Other Control Lines2
  • RSTU1 ::= Signal RST,  U1 Display 1,  (Low Active)
  • CLKU1 ::= Signal CLK, U1 Display
  • Signal CLK, U1, Display

 

 

 

Parts List

  • Interface Board (Custom)
  • Display  Board 0EUW0ASSY8E-010081-Rev B
  • (8) 2-56x1/4  Screw. Pan Head, Phillips, stainless steel
  • (8) #2 Washer, Flat,  stainless steel
  • 30-pin (2x15) Header, Female, WW leads
  • 5-pin Header, Male, WW leads
  • Sign in to reply

Top Comments

  • ajcc
    ajcc over 5 years ago +2
    Great post! I didn't know you could make colored tables in the blog posts. It's looking very neat with the colors and proper subscripts.
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to ajcc +2
    ajcc yes It is just straight forward CSS <td style= "background-color: 'css-std color' which can be found on line. oh an d the superscript for I2C is I<sup>2</sup>C fir subscruot H20 would be H<sub.2>2…
Parents
  • ajcc
    ajcc over 5 years ago

    Great post! I didn't know you could make colored tables in the blog posts. It's looking very neat with the colors and proper subscripts.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ajcc
    ajcc over 5 years ago

    Great post! I didn't know you could make colored tables in the blog posts. It's looking very neat with the colors and proper subscripts.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to ajcc

    ajcc  yes It is just straight forward CSS  <td style= "background-color: 'css-std color' which can be found on line.

    oh an d the superscript for I2C is I<sup>2</sup>C

    fir subscruot H20 would be H<sub.2>2</sub>O

     

    ~~Cris