Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen: Getting the lab working: Drill Press X-Y table
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 11 Jun 2018 10:42 PM Date Created
  • Views 2304 views
  • Likes 6 likes
  • Comments 15 comments
  • nexgen
  • x-y table
  • cnc
  • diy
  • drill press
  • nexgen flight simulator
Related
Recommended

NexGen: Getting the lab working: Drill Press X-Y table

phoenixcomm
phoenixcomm
11 Jun 2018

So I figured out what I need for the drill press. A nice sturdy X-Y table that I can move around manually and of course electrically. The bed should be about 12" square. So far this is just a pipe dream, but just maybe.image

DESIGN:   First I'll need two lengths of V-Rail, Aluminum 6063-T5, each one about 500mm long. Since I have a much smaller work surface I will have to get creative. I really only need to drill 5 holes at a time for aircraft instruments. Five inches is the largest circle for mounting aircraft instruments. (see the picture on the right, the bottom profile).image

DescriptionOptionsManufacturerPart No.Quan
2080 Series Aluminum Extrusion, V-SlotRegistered 20x40 500mmOpen Builds155-LP6
8mm T8x2 Lead Screw Threaded Rod Trapezoidal ACME with brass flange nut500mmT8x2-500mm2
Nema17 Stepper MotorRemovable WiresKayroadKR42HS40-17042
5mm-x-8mm Shaft Coupler (Al w/ Anti-BacklashCoupler2

V-Wheel Kit, Delrin,  Solid

OD: 23.90

Pack of 10BULK-MAN 3DOX-CNC/3284911
Mini GantryLink CNCMini Gantry Kit8
Dual Bipolar Stepper Motor Shield for ArduinoDFRobotDRI00231
Arduino Mega 2560 R21
Ethernet Shield for the Arduino1

I'm going to build this in the shape of a pound sign (#).  This may evolve into something else but for now, that's fine.

  1. The bottom two rails are going to be mounted at 500mm on center and mounted rigidly to the base
  2. Then you will need 4 mini-gantries, one per mounting point.
  3. Then attach a rail to each pair of mounts, now this will be our X-Axis.
  4. Then attach 4 more mini-gantries.
  5. Then attach a rail to each pair of mounts, now this will be my Y-Axis
  6. Now attach a custom gantry to the top 4 mini-gantries. ( Al, Wood, Plastic, etc.) In this way, I can build custom fixtures

 

It looks like I will most likely drive this with G-CODE (RS-274), a standard, I most likely will need a couple of micro-switches for alignment, and a few more to tell it when at its limits, and stop. There are a few Arduino G-Code Interpreters/Routers out there, but I kind of like the one I found at Marginally Clever Robots.   I think that for software on the PC I will use UGS or Universal Gcode Sender as it is written in JAVA so it will run on my lab pc which runs Linux.

 

I'll let you know how this turns out.

~~Cris H. image

 

Back to the Indeximage

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 7 years ago in reply to phoenixcomm +2
    So I've been playing with my CNC (600 x 600 x 75mm height) and finding out more about dealing with plastic. They recommend a single flute cutter with a reasonable feed speed so the chips get removed and…
  • genebren
    genebren over 8 years ago +1
    Sounds like fun! I could not find the picture that describes your instrument mounting, but I am very familiar with the layout (having built cockpit simulators for 747/757/767 aircraft). We used to have…
  • phoenixcomm
    phoenixcomm over 8 years ago in reply to genebren +1
    My G-d That's brute force at work. I have a nice template that I'm making. basically, I have a sheet of 1/4" plexiglass about 8" square now draw an X from corner to corner drill the center hole, now drill…
  • mcb1
    mcb1 over 7 years ago in reply to phoenixcomm

    Looks like their site is broken ... in some places.

    Not the first time the other day Wordpress somehow decided it wasn't installed .image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 7 years ago in reply to mcb1

    thanks for the info your link though is a bust please fix it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 7 years ago in reply to phoenixcomm

    So I've been playing with my CNC (600 x 600 x 75mm height) and finding out more about dealing with plastic.

     

    They recommend a single flute cutter with a reasonable feed speed so the chips get removed and it reduces heat build-up in the material.

    ChipX are making a few at reasonable prices and this is apparently excellent https://chipx.co.nz/shop/cutting-tools/chipx-tools/router-bits/cm025-025-1f-30dg-58/

     

    image

    It used to be sharp and pointed until someone added a piece of aluminium and forgot to reset the Z axis (4mm v 0.25mm is NOT the same)

    I'm sure you could knock up something similar for a dremel.

     

     

    The control board is based on a Smoothie design and their own drivers as the Stepper motor driver chip market is getting tight (too many 3D printers being made)

     

    Don't underestimate the rigidity required, you don;t want it flexing when moving in the X or Y direction.

     

    Cheers

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 8 years ago in reply to ntewinkel

    Nico Nice nab when its free. I need something to handle bigger things.  8.5" x 5" is what I need currently but my jig is almost has a tool path of 3"x11".image And I need a clearance of about 8" under the tool. with my drill press, I have 2+ inches between the chuck and the top of the jig. My two cutters are Rotozip 1/8" cutter for the plunge and hogging out material, then finish work with a Dremel 1/8" side ceramic grout cutter for really sharp corners. I really can't put a lot of side pressure on the Dremel cutter as it could break but remember this is only poly-pro. LOL image

    The victims Sterilite Small Clip Clear Storage Box With Latched Lid 19618606 - 11"L x 6-5/8"W x 2-3/4"H

    Oh yes, I will have to bring the drill speed up.

    Cris

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to phoenixcomm

    This was my comment to Mark earlier, with picture:

    https://www.element14.com/community/community/design-challenges/bluetoothunleashed/blog/2018/06/13/btsentry-bluetooth-op…

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>