Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen: Getting the lab working: Drill Press X-Y table
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 11 Jun 2018 10:42 PM Date Created
  • Views 2289 views
  • Likes 6 likes
  • Comments 15 comments
  • nexgen
  • x-y table
  • cnc
  • diy
  • drill press
  • nexgen flight simulator
Related
Recommended

NexGen: Getting the lab working: Drill Press X-Y table

phoenixcomm
phoenixcomm
11 Jun 2018

So I figured out what I need for the drill press. A nice sturdy X-Y table that I can move around manually and of course electrically. The bed should be about 12" square. So far this is just a pipe dream, but just maybe.image

DESIGN:   First I'll need two lengths of V-Rail, Aluminum 6063-T5, each one about 500mm long. Since I have a much smaller work surface I will have to get creative. I really only need to drill 5 holes at a time for aircraft instruments. Five inches is the largest circle for mounting aircraft instruments. (see the picture on the right, the bottom profile).image

DescriptionOptionsManufacturerPart No.Quan
2080 Series Aluminum Extrusion, V-SlotRegistered 20x40 500mmOpen Builds155-LP6
8mm T8x2 Lead Screw Threaded Rod Trapezoidal ACME with brass flange nut500mmT8x2-500mm2
Nema17 Stepper MotorRemovable WiresKayroadKR42HS40-17042
5mm-x-8mm Shaft Coupler (Al w/ Anti-BacklashCoupler2

V-Wheel Kit, Delrin,  Solid

OD: 23.90

Pack of 10BULK-MAN 3DOX-CNC/3284911
Mini GantryLink CNCMini Gantry Kit8
Dual Bipolar Stepper Motor Shield for ArduinoDFRobotDRI00231
Arduino Mega 2560 R21
Ethernet Shield for the Arduino1

I'm going to build this in the shape of a pound sign (#).  This may evolve into something else but for now, that's fine.

  1. The bottom two rails are going to be mounted at 500mm on center and mounted rigidly to the base
  2. Then you will need 4 mini-gantries, one per mounting point.
  3. Then attach a rail to each pair of mounts, now this will be our X-Axis.
  4. Then attach 4 more mini-gantries.
  5. Then attach a rail to each pair of mounts, now this will be my Y-Axis
  6. Now attach a custom gantry to the top 4 mini-gantries. ( Al, Wood, Plastic, etc.) In this way, I can build custom fixtures

 

It looks like I will most likely drive this with G-CODE (RS-274), a standard, I most likely will need a couple of micro-switches for alignment, and a few more to tell it when at its limits, and stop. There are a few Arduino G-Code Interpreters/Routers out there, but I kind of like the one I found at Marginally Clever Robots.   I think that for software on the PC I will use UGS or Universal Gcode Sender as it is written in JAVA so it will run on my lab pc which runs Linux.

 

I'll let you know how this turns out.

~~Cris H. image

 

Back to the Indeximage

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 7 years ago in reply to phoenixcomm +2
    So I've been playing with my CNC (600 x 600 x 75mm height) and finding out more about dealing with plastic. They recommend a single flute cutter with a reasonable feed speed so the chips get removed and…
  • genebren
    genebren over 8 years ago +1
    Sounds like fun! I could not find the picture that describes your instrument mounting, but I am very familiar with the layout (having built cockpit simulators for 747/757/767 aircraft). We used to have…
  • phoenixcomm
    phoenixcomm over 8 years ago in reply to genebren +1
    My G-d That's brute force at work. I have a nice template that I'm making. basically, I have a sheet of 1/4" plexiglass about 8" square now draw an X from corner to corner drill the center hole, now drill…
  • ntewinkel
    ntewinkel over 8 years ago in reply to DAB

    DAB  wrote:

    >Did you see the CNC mill Nico found?

    It's little, but for only about $200 USD it's a great start (perfect for me anyway).

    http://canada.newark.com/pcduino/108302018/cnc-engraver-assembled/dp/33AC0136?st=cnc%20engraver

    Plus expanding it looks like a fairly easy process - buy extended versions of all the long parts.

     

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 8 years ago in reply to DAB

    no never did please send me the link. thanks

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 8 years ago in reply to phoenixcomm

    Chris,

     

    Did you see the CNC mill Nico found?

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 8 years ago in reply to DAB

    Mills and CNC drills are really the same things but the drill is much smaller and a Mill could be Computer controlled as well but the older ones are cheap, and they last forever. and with very little effort can be converted to CNC control.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 8 years ago in reply to DAB

    whats the dif??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>