Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen: Lab:B&K Precision 3010 Function Generator - Repair
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 13 Apr 2020 6:14 PM Date Created
  • Views 1664 views
  • Likes 7 likes
  • Comments 8 comments
  • test equipment
  • b&k precision 3010
  • restorerepairch
  • function generator
Related
Recommended

NexGen: Lab:B&K Precision 3010 Function Generator - Repair

phoenixcomm
phoenixcomm
13 Apr 2020

THENimage

NOWimage

 

  • Black (Hot) and White (Neutral) ended up switched so 110 VAC ended up on my ground-plane! Push on connectors are a must! image
  • I replaced the bridge with 4 100vdc 5 amp monsters.  imageIt took quite a bit of heat to solder the big leads so I sub in an IR bridge  12DB6A
  • I have a lot of harmonics to fix.
  • The function generator parts still work. imagethat is to say triangle, sine and square wave are ok just with harmonics. Most likely killed some caps!

 


PROBLEMimage

DEAD DIODESimage

FIXEDimage

NEW BIG DIODESimage
  • Sign in to reply

Top Comments

  • cstanton
    cstanton over 6 years ago +3
    D: but what died!?
  • DAB
    DAB over 6 years ago +2
    Good job. DAB
  • phoenixcomm
    phoenixcomm over 6 years ago in reply to cstanton +2
    cstanton not sure, but there is only AC on the 600-ohm outputs. So I had do get some stiffer diodes(4) for the bridge!
Parents
  • skan743
    skan743 over 5 years ago

    Currently he tried to repair the same generator for my studies, I have replaced capacitors and potentiometers in bad condition and at the moment I have managed to obtain all types of signals, however I have not been able to see them in the 600ohm output. Until Q9 everything works great (test point 11), however at the 600ohm output there is only a static -14.XX VDC and no AC signals.

    The TTL output works great.

     

     

    Any idea what might be failing? image

     

     

    As for the harmonics I recommend checking the symmetry in test point 1 ^^image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to skan743

    skan743 I am looking at my schematic I wonder what you see at the top the amplitude pot? I feeds the base of Q9. its collector (11) feeds the base of Q11 which drives the output pairs Q12 & Q13.

    BTW it is a pain to work on out of the case.

    ~~Cris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to skan743

    skan743 I am looking at my schematic I wonder what you see at the top the amplitude pot? I feeds the base of Q9. its collector (11) feeds the base of Q11 which drives the output pairs Q12 & Q13.

    BTW it is a pain to work on out of the case.

    ~~Cris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • skan743
    skan743 over 5 years ago in reply to phoenixcomm

    Today I was observing test point 11 again and I obtained a different result than yesterday, during today's tests up to test point 8 the results coincide with the graphs provided by the schematic, from IC7 everything is a disaster, all The pots around it are damaged, although that does not explain the problem of the --14.XX VDC on the output.  Tomorrow I will test that stage from the amplitude pot without any AC or DC signal at the base of Q9, I have simulated it and it should have the same DC voltages at each point that the schematic diagram specifies if I adjust the DC offset pot at 0vdc image

     

    Pd: the simulator is Proteus and thanks for the comment and the help.