Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen: Landing Gear Subsystem
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 14 Jan 2021 12:35 AM Date Created
  • Views 1326 views
  • Likes 5 likes
  • Comments 5 comments
  • flight simulator
  • nexgen
  • landing gear lever
  • rudder pedals
  • diy aircraft cockpit
  • toe brakes
  • canaerospace
  • c progrmming
  • canbus
  • arduino mega
Related
Recommended

NexGen: Landing Gear Subsystem

phoenixcomm
phoenixcomm
14 Jan 2021

This subsystem is part of the Pilot Controls (node id 100) consisting of the following subsystems. Inter-subsystem is handled by CAN.imageimage

  • Side Stick
  • Throttle
  • Landing Gear Lever lamps and sensors
  • Rudder Pedals with differential braking.

The subsystem consists of the following:

  • Landing Gear Control Lever (CANid: 1175)
  • 3 Red Indicators (CANid: 1400, 1, 2 )
  • 3 Green Indicators (CANid: 1403, 4, 5)
  • WOW, Weight on Wheels, (CANid: 1176)  this sensor, prevents Landing Gear retraction while on the ground. See the movie "No Highway in the Sky" about 1hr in. imageFor WOW to be TRUE all the sensors have to agree. WOW  on the main wheels is responsible for moving the front canard down, until there is weight on the nose wheel at which time the canard goes to 90 degrees to act as a speed brake. as well as enabling nose wheel steering.
  • Gear Down and Locked sensor (CANid: 1406, 07, 08)
  • Gear Up and Locked sensor. (CANid: 1409, 9810, 11 )


Aircraft have 3 wheels Left, Nose, Right. Each pair of Red/Green Indicator  shows the status of each  wheel:

  • RED SOLID, Gear UP, and Locked.
  • RED BLINKING:
    • Landing Gear Lever  UP  selected and gear not up and locked (gear retraction)
    • Landing Gear Lever DOWN selected disagrees with landing gear not down and locked (gear extension)
  • GREEN SOLID, Gear Down, and Locked

Landing Gear Lever
So to recap that's wires, 13 wires plus grounds. Since I only have two contacts, (UP & DOWN) on the Landing Gear Lever which is not used very much, I can catch them with an interrupt by putting a 2-input Or Gate followed by Schmitt Trigger connected to the Arduino Mega pins 20, 21. using the rising mode. You have to keep in mind that the switch once in the UP or Down position does not move, except in takeoff and landing, therefore the interrupt is detected on the rising edges.

UPDATE 1: To understand the logic behind my RED lamps which can be solid on or blinking at about 1 Hz, I have included a schematic for you to wonder about.

UPDATE 2: I have decided NOT to try and use the timers instead I will just use a lowly NE555. Its output is 1Hz with a 50% duty cycle.

// The Arduino Mega has 6 interrupt pins 2, 3,  18, 19, 20, and 21

Arduino pins and their mnemonic:

20 LGLUP                  attachInterrupt( digitalPinToInterrupt(LGLUP), ISR20, RISING );

21 LGLDOWN          attachInterrupt( digitalPinToInterrupt(LGLDOWN), ISR21, RISING );

int LGLstatus :: = TRUE == 1 == UP; FALSE == 0 == DOWN; LGLstatus is set by ISR20 && ISR21

pins 22, 23, 24 are SOLID  ON

22 BLR

23 BRL

24 BLC

// pins 25, 26, 27  are BLINK Enable

25 BLR_EN

26 BLL_EN

27 BLC_EN

// RED LAMP

28 GRR

29 GRL

30 GRC

// GREEN LAMPS

31 GGR

32 GGL

33 GGC

//CANbus -- SPI interface

50 MISO

51 MOSI

52 SCLK

53 SS

19  CANint.               attachInterrupt( digitalPinToInterrupt(CANint), ISR19, RISING );

 

 

OPTIONAL:  I possibly can include  3 analog input to read the Rudder Pedals (one channel) and Right and Left Toe brakes.  These are just potentiometers.

 

A1 Rudder position

A2 BRPR

A3 BRPL

**Please Note that CANids of 1300 to 1499 are not reserved.

  • Sign in to reply

Top Comments

  • colporteur
    colporteur over 5 years ago +1
    CH are you building an airplane like JOHNNY CASH - ONE PIECE AT A TIME - CADILLAC VIDEO? https://www.youtube.com/watch?v=Hb9F2DT8iEQ
Parents
  • colporteur
    colporteur over 5 years ago

    CH are you building an airplane like JOHNNY CASH - ONE PIECE AT A TIME - CADILLAC VIDEO?

    https://www.youtube.com/watch?v=Hb9F2DT8iEQ

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to colporteur

    colporteur ROFL!!! No, I sort of know, what I want and need to do: as I have been working on this monster for about 20 years I lost quite a bit when my house was foreclosed! along with my auto engine on the test stand., with a custom EFI which would have turned into my FADEC the computer where cross-coupled for redundancy. The reason why the picture of the Sonic Cruiser is pictured I like the configuration.  2 multi-stage ducted fans using a size 11 e-motor, the motors are driven by 2 small gas automotive engines. ie No batteries. The project's name was Phoenix2000 ie fly in 2000. LOL  OH BTW this beast is a large Canard and will be fast the main wing is mounted on top of the fuselage, like a fighter, this gives me more maneuverability. The ducted fans are in the wing.  As I am playing games with the fans to increase thrust with little penalty. Fuel will be stored in tanks or bladers the will allow pumping fuel from one tank to another to keep the trim front, to back.  The fuel system can measure the fuel in any tank, and be refueled from one point. The wing in the front, the canards, are movable like the Saab 37 Viggen, on landings as this plane is very slippery its landing speed is considered high for most small planes. So once there is  weight on the main wheels the canard can pitch down to bring the nose wheel down when that is done the canard goes to 90 degrees acting like a speed brake.

    In a way, it will be sort of the song. LOL

    ~~Cris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to colporteur

    colporteur ROFL!!! No, I sort of know, what I want and need to do: as I have been working on this monster for about 20 years I lost quite a bit when my house was foreclosed! along with my auto engine on the test stand., with a custom EFI which would have turned into my FADEC the computer where cross-coupled for redundancy. The reason why the picture of the Sonic Cruiser is pictured I like the configuration.  2 multi-stage ducted fans using a size 11 e-motor, the motors are driven by 2 small gas automotive engines. ie No batteries. The project's name was Phoenix2000 ie fly in 2000. LOL  OH BTW this beast is a large Canard and will be fast the main wing is mounted on top of the fuselage, like a fighter, this gives me more maneuverability. The ducted fans are in the wing.  As I am playing games with the fans to increase thrust with little penalty. Fuel will be stored in tanks or bladers the will allow pumping fuel from one tank to another to keep the trim front, to back.  The fuel system can measure the fuel in any tank, and be refueled from one point. The wing in the front, the canards, are movable like the Saab 37 Viggen, on landings as this plane is very slippery its landing speed is considered high for most small planes. So once there is  weight on the main wheels the canard can pitch down to bring the nose wheel down when that is done the canard goes to 90 degrees acting like a speed brake.

    In a way, it will be sort of the song. LOL

    ~~Cris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • colporteur
    colporteur over 5 years ago in reply to phoenixcomm

    My understanding is that a plane sporting the air surfaces shown in the drawing REQUIRES computers to fly. The pilot(s) would not be able to manage the controls to keep the plane stable. Any truth to my understanding?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to colporteur

    colporteur  No you don't need a computer for a Canard Configuration. Burt Rutan's Varieze. But there are other things to consider than just the wing configuration or Planform. While the Varieze was a Canard, it was a Mid-Wing aircraft. while mine is a classical High-Wing design. and my Canard (front wing) and the main wing are not on the same mean-cord, In th eVarieze the Canard wing would tend to wash out the main wing, So my Canard in mounted below the main wing's Cord. And Yes A computer will help. image any more questions? just ask.

    ~~Cris