Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen: RSS: Hacking a Control, Radio Set: C-3436A/ARN-30D
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 16 Jun 2014 10:13 PM Date Created
  • Views 1138 views
  • Likes 1 like
  • Comments 4 comments
  • nexgen
  • c-3436a/arn-30d
  • hardware
  • radio_sub_system
  • rss
  • c_language
  • arduino
  • diy_cockpit
  • software
Related
Recommended

NexGen: RSS: Hacking a Control, Radio Set: C-3436A/ARN-30D

phoenixcomm
phoenixcomm
16 Jun 2014

THE ANALYSIS: The radio head C-3436A was used in the 1960's. It is used for both VOR and ILS. It has three (3) ARC connectors in the rear. I had built some cables for the unit a few ago but then never did anything with it.  So I need to test the RSS so I pulled out this unit. I am going use the term "Hacking" loosely as I am not going to damage the Control Set in any way.  image

 

image
Fullscreen 1157.contentimage_134098.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>
Radio Control Set
Figure 1
The Radio Control Set Opened for Testing
Figure 2
image
Radio Control Set Interface
Figure 3

THE PLAN:

1. The first thing I had to do was ring out the connectors (Please see Figure 2) as I did not have the schematics as the TM 11-1520-211-35 Google Book did not scan them properly. ( I have attached a sheet of the result of the ring out but as yet I do not have the weighting for each line.)

 

2. The next thing is to build an interface board to go between the Control Set, and an Arduino Mega2560. The board will have two (2) DB25F jacks to plug into my cables.  There are also two (3) 16 pin IC Sockets. As this interface board is a one-off I will Wire-Wrap it.  There will be most likely a small relay to handle the lighting and a Molex 4-pin connector for the power.

 

3. The next thing is to jumper the board to the Arduino via the rear header (Digital I/O Pins 21 through 53).

 

4. At this time I am not going to worry about the following items: Lights, Volume, nor Squelch.

 

 

  image Keep tuned in, more to come!

   ~~Cris

Attachments:
https://community.element14.com/cfs-file/__key/communityserver-blogs-components-weblogfiles/00-00-00-03-00/C_2D00_3436A.ods
  • Sign in to reply

Top Comments

  • DAB
    DAB over 12 years ago +1
    Hi Chris, Brings back memories of my work on integrated avionics where they incorporated VOR/ILS into the demonstration hardware. I will check to see if I have any documentation on the VOR/ILS functions…
  • DAB
    DAB over 12 years ago in reply to phoenixcomm +1
    Hi Chris, Unfortunately I indeed tossed all of my old documentation. It never fails. As soon as you convince yourself that you will have no further need for something and toss it, someone asks if you still…
Parents
  • DAB
    DAB over 12 years ago

    Hi Chris,

     

    Brings back memories of my work on integrated avionics where they incorporated VOR/ILS into the demonstration hardware.

    I will check to see if I have any documentation on the VOR/ILS functions, but I think I dumped all of it a few years ago, though knowing my normal habits, it is probably still somewhere in my stash.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 12 years ago in reply to DAB

    DAB do you by any chance have the "maintenance manual" for C-3436A/ARN-30D??  I am looking for the defines of the pins of the 3 connectors in the rear.. Cris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • phoenixcomm
    phoenixcomm over 12 years ago in reply to DAB

    DAB do you by any chance have the "maintenance manual" for C-3436A/ARN-30D??  I am looking for the defines of the pins of the 3 connectors in the rear.. Cris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • DAB
    DAB over 12 years ago in reply to phoenixcomm

    Hi Chris,

     

    Unfortunately I indeed tossed all of my old documentation.

    It never fails.  As soon as you convince yourself that you will have no further need for something and toss it, someone asks if you still have it. image

     

    After twenty years I am not sure where you can go for that information.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 12 years ago in reply to DAB

    I know the feeling so I have kept quite alot... I only toss it when its on an e-pub... Now I am thinking of scanning some of my own stuff.. But thats ok if you have unbound stuff.. its easy but you have to scan it twice.. (both sides), and if there are fold outs.. done by hand.... BUT if its bound slit it and go with the first choice or build a DIY scaner that turns pages, LOL