Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen: RSS: Radio Set 3436A/ARN-30D: Interface Card
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 22 Jun 2014 8:25 PM Date Created
  • Views 713 views
  • Likes 2 likes
  • Comments 3 comments
  • hardware
  • radios
  • wire-wrap
  • rss
  • nexgen_flight_simulator
  • arduino_mega
  • diy_cockpit
  • software
  • linux
Related
Recommended

NexGen: RSS: Radio Set 3436A/ARN-30D: Interface Card

phoenixcomm
phoenixcomm
22 Jun 2014

THE PLAN (Step 2):  Well the first thing we need is a piece of Vector Board, about 4" x 4"  or about 10 x 10 cm ( Do not buy any cheap crap off of ebay.. It must be FR-4, glass-epoxy ).

image
Vector Board before for clean up
Figure 1

I need cut 2 holes in the board about  2" x .5" (Figure 1), or you can use a DB25 punch if you are lucky enough to own one, $$$$.  I cut the two holes with my Dremel multi-tool, but it is very hard to control, I now have to clean it up, anyway, with my Dremel. If I had the right blade for the rotary tool it would have been easier. Then I need to mount the adapter plate(s)(Figure 2) to the Vector Board and the DB25(s) to them as well.


The next thing is to mount the three 16 pin IC sockets, a little dab of hot glue, or crazy glue and that should do it. But remember to leave room for the 4 pin Molex connector that is common on disk drives, and fans, Molex Part Number image
15-24-4441, Molex Specification Sheet, and a relay that control the panel lamps.

 

I  really like this relay module I found on eBay (Figure 3) and the cool part is I don't have to build it. There is all so a 2 channel module as well. BTW they are cheaper than I can build them..lol
Now the only this to do is break out the Wire Wrap stuff and wire it up (Figure 4).

 

image  Keep Tuned In, More To Come
~~ Cris H.

BTW Long to finish got sick anyway just finished now on to the next part.

I am having the adapter plates made for me. Let me know if you think you can use them. I might get a small run of 100 made. My guess is they will be about 5 to 8 bucks each.
image

1 Channel Isolated 5V Relay Module

Figure 3

imageimage
Interface board finished *
* The power connector, nor is the relay wired in yet..
Figure 4

                                                                                                                                                                                                                                                                                                                                                                  One more note: I have found some food containers used in the food business NR2402P-BLK my interface bolts right in. Oh yes the white dots in the photos in figure 4 are nylon 4-40 screws and nuts. image

  • Sign in to reply

Top Comments

  • DAB
    DAB over 12 years ago +1
    I assume that the cargo container stuck in the engine was a reason to use the radio to call in a problem? Meanwhile, it looks like you are making good progress on the build. DAB
  • phoenixcomm
    phoenixcomm over 12 years ago in reply to DAB +1
    maybe... but I just got my dremel cutters.. and the relay came in.. was supposed, not, I got a freekn servo motor....Duh!!!
  • phoenixcomm
    phoenixcomm over 12 years ago in reply to phoenixcomm +1
    Cool I just got my relay..But I need some 4-40 nylon machine screws - but after a trip to Home Depot.. they dont carry them, not even in stainless or whatever... have to wait to order them.. from my jobber…
Parents
  • DAB
    DAB over 12 years ago

    I assume that the cargo container stuck in the engine was a reason to use the radio to call in a problem?  image

     

    Meanwhile, it looks like you are making good progress on the build.

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 12 years ago

    I assume that the cargo container stuck in the engine was a reason to use the radio to call in a problem?  image

     

    Meanwhile, it looks like you are making good progress on the build.

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • phoenixcomm
    phoenixcomm over 12 years ago in reply to DAB

    maybe... but I just got my  dremel cutters.. and the relay came in.. was supposed, not, I got a freekn  servo motor....Duh!!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 12 years ago in reply to phoenixcomm

    Cool I just got my relay..But I need some 4-40 nylon machine screws - but after a trip to Home Depot.. they dont carry them, not even in stainless or whatever... have to wait to order them.. from my jobber here in town... 80 cents per 100 :) (Stainless) So Im bored so Im going to drill out the FR4 board, lash it up, and wire it.. then the testing begins..