Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen: Software Development: arduino sketch & eclipse on Linux. Part 1
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 21 Aug 2015 9:32 PM Date Created
  • Views 2119 views
  • Likes 3 likes
  • Comments 6 comments
  • software_development
  • eclipse
  • arduino_tutorials
  • avr_plugin
  • arduino
  • linux
Related
Recommended

NexGen: Software Development: arduino sketch & eclipse on Linux. Part 1

phoenixcomm
phoenixcomm
21 Aug 2015

Ok, Hold on buckle in. This post will not be pretty.  THE PROBLEM: Is the Arduino's instance on their IDE and a crippled ANSI C/C++ language called Sketch.  By the time, you have written a couple of what they call a Sketchs. They have really messed with you. As the two functions that basically you use are setup() and loop(). My aim here is not to teach you how to write a nice program in ASNI C/C++.

 

harrison@Whirlwind ~ $ ls Tools

2wgs

eclipse-avr QnewB
3wgs FileZilla3 Renesas
arduino Git Scintilla
AutoScan-Network-Linux-1.50.sh kompozer wingbody.for
BridgePoint poky-fido-13.0.0 yoxos
ceasiom100-v4.0 qcad qcad-3.9.8-linux-x86_64
eclipse
harrison@Whirlwind ~ $

My Tool Directory

Figure 1

My Goal: Is to show you the light, just to guide you. My "go to" tool for Integrated Software Development Environment is the Eclipse IDE with standard GNU toolchains, running on my LinuxMint 17r2 desktop. I do not work in a M$ environment so I will not distract you with those comments.  I have several specialized versions of Eclipse such as eclipse-avr, which is what I will be talking about. OK, let's get started. Fist we have to download a bunch of stuff. Now I put all my tools in my Tools directory (Figure 1). Use my directory structure it will make you life easier for you, so try it. Note: All downloads are for Linux 64 bit ubuntu distro.

 

  1. Arduino's IDE
  2. eclipse IDE.
  3. Java Runtime 6 or higher (use your package manager. Synaptic) It comes with the distro.
  4. AVR plugin for eclipse. (Well get this in eclipse itself)
  5. The GNU-AVR toolchain. You will need to execute this command string in your terminal:
    sudo apt-get install gcc-avr binutils-avr gdb-avr avr-libc avrdude

 

image
Screen Shot of Synaptic Package Monitor
Figure 2

OK let's start in your arduino directory and we will install the arduino-1.6.2-linux64.tar.xz as arduino/arduino-1.62.

Now go to your eclipse-avr directory and will install the eclipse-cpp-mars-R-linux-gtk-x86_64.tar.gz as eclipse/eclipse

If you haven't executed the command to get the GNU-AVR toolchain, then do so now.  Now is a good time to check for the JAVA Runtime 6. If you have 7 you don't need 6 (Figure 2).

 

Ok, now we have to launch eclipse, click on the eclipse icon in your Tools/eclipse-avr/eclipse/ directory. It will ask you for you default workspace (say yes), you can always change it. DO NOT CHECK THE BOX "Use this as the default and do not ask again." Now the eclipse IDE will launch.  So let's add the AVR plugin. Go to: Help > Install New Software. A new window called Install will open. Near the top is a drop-down box with "work with:" to it's left. Click the box and type http://avr-eclipse.sourceforge.net/updatesite/ then click add. In the pop-up box that appears type AVR Eclipse Plugin into the "name" box (Figure 3).

image

Screen Shot of eclipse Install/Add Repository

Figure 3

 

 

 

 

 

Now Please restart your eclipse IDE File > Restart. When eclipse restarts  your eclipse IDE should now look like this (Figure 4):

 

image

AVR plug-in installed

Figure 4

 

 

 

 

Keep Tuned In, More To Come
~~ Cris image

 

UPDATE 8/23 Blame this on Mario... He though that NetBeans IDE might also work for the AVR programming. Here's what I got after hours of getting it configured. It looks like I will have to put it out of its misery, and remove a really bad tool.  ~~ CAH

 

 

image

Utter Failure, What a Joke

Figure 5

  • Sign in to reply
  • jomoenginer
    jomoenginer over 8 years ago in reply to phoenixcomm

    Uh, but now you are referring to an IDE not the underling language.   Most of the Arduino boards use an Atmel/Microchip MCU so you could use AVR Studio or even Visual Studio which give you debug capability.  Eclipse has an Arduino package that can easily loaded giving you support for various Arduino boards, which I'm guessing you found out. Eclipse is nice, but it can be a mess to work with as well.  However, in the end, you still are using the same libs as used in the Arduino IDE.  You could roll your own libs though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 8 years ago in reply to jomoenginer

    Ok but now I just use eclipse that I built just for Arduino, really very easy to use.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 8 years ago in reply to phoenixcomm

    phoenixcomm  wrote:

     

    Still it's a brain-dead version of C.

     

     

    Well, I wouldn't go so far as to say that.   It's intent was to be a prototyping tool build on Processing for both software folks as well as artists with an idea of collaboration.  It's not pure C and it's not pure C++; you could write code either way but much of the libraries are written in C++.  It's actually a quite useful tool and used to teach students hardware and software interaction in Universities. It's not for everyone though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 8 years ago in reply to jomoenginer

    you are correct Jon I bow to you. Still it's a brain-dead

    version of C.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 8 years ago

    The Arduino based language is Wiring.  A Sketch is the code/program you create.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>