Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen: Tech Tip II. Micrometer Repair.
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 21 May 2018 5:08 AM Date Created
  • Views 1411 views
  • Likes 10 likes
  • Comments 7 comments
  • nexgen
  • diy cockpit
  • 436-1
  • starrett
  • diy repair
  • micrometer
Related
Recommended

NexGen: Tech Tip II. Micrometer Repair.

phoenixcomm
phoenixcomm
21 May 2018

This is a really nice find at my local pawn shop. I uncovered this jewel in the Dollar box.  It was sticking badly. It really needed a good cleaning. It was a Starrett model 436-1.  I retracted the spindle into the sleeve and then removing it. by continuingly rotating the thimble counter-clockwise. This took a few tries but finally separated it.  I used a lightweight oil and a new Scotch-BriteRegistered Stainless Steel Scrubbing Pad to clean the spindle. I had to repeatably fully insert and remove the spindle from the barrel. You could use a piece of printer paper with lightweight oil to then polish the spindle.imageimage

imageimageimage
Spindle & SleeveBurn Mark on SpindleFins -- Good Enough

The micrometer now runs in and out smoothly. It is off .001" but I need a special wrench to set it back to 0.000". The micrometer is missing the ratchet stop (it's jammed), and the spindle lock nut is non-functional at the moment.

 

 

Back to the Indeximage
  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 8 years ago +4
    Looks like it had a very hard life ... No micrometer should be subjected to that sort of abuse .... There's a good writeup here. Evaluate, Repair and Adjust a Second-Hand Micrometer You should be able…
  • jw0752
    jw0752 over 8 years ago +3
    When I was 16 I worked for an automotive parts house that also did motor rebuilding in a back shop. The rebuilder was a very very precise man, much like the tools with which he worked everyday. One day…
  • genebren
    genebren over 8 years ago in reply to jw0752 +3
    John, That is a great story. So you were a wise guy way back then. Thanks for the huge smile that I got as I read your story Gene
Parents
  • jw0752
    jw0752 over 8 years ago

    When I was 16 I worked for an automotive parts house that also did motor rebuilding in a back shop. The rebuilder was a very very precise man, much like the tools with which he worked everyday. One day for the fun of it I walked back into his space and pointed up at the set of micrometers hanging on the wall and with a very straight face I said, " Hey Lars, I need to borrow another one of those C-Clamps to hold a shelf in place while I nail it." I don't know which was more surprising, the ashen appearance of Lars' face or how quickly he spun around and counted the number of micrometers that were still on the wall. To this day I can't interact with a micrometer without seeing Lars' face in that moment.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 8 years ago

    When I was 16 I worked for an automotive parts house that also did motor rebuilding in a back shop. The rebuilder was a very very precise man, much like the tools with which he worked everyday. One day for the fun of it I walked back into his space and pointed up at the set of micrometers hanging on the wall and with a very straight face I said, " Hey Lars, I need to borrow another one of those C-Clamps to hold a shelf in place while I nail it." I don't know which was more surprising, the ashen appearance of Lars' face or how quickly he spun around and counted the number of micrometers that were still on the wall. To this day I can't interact with a micrometer without seeing Lars' face in that moment.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • genebren
    genebren over 8 years ago in reply to jw0752

    John,

     

    That is a great story.  So you were a wise guy way back then.

    Thanks for the huge smile that I got as I read your story

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 8 years ago in reply to jw0752

    Never knew that was an approved use!  imageimage

     

    Cris

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 8 years ago in reply to phoenixcomm

    A welding clamp is even better!

    John