Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen TPMS or Tire Pressure Monitoring System: The Gap
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 22 Jul 2015 11:25 PM Date Created
  • Views 599 views
  • Likes 1 like
  • Comments 2 comments
  • tpms
  • flight_simulation
  • wheels
  • tpms_systems
  • test_flight
  • landing_gear
Related
Recommended

NexGen TPMS or Tire Pressure Monitoring System: The Gap

phoenixcomm
phoenixcomm
22 Jul 2015

Ok this is more of a bather than a post. Buckle up the ride will not be smooth! The US National Highway Traffic Safety Administration (NHTSA) in April 8, 2005 said it should be on all cars by 2008 and now trucks.. ok thats cool. Commercial Aircraft have had them for years BC (Before Cars) .. But in between those 2 camps there is a huge Black Hole. Whatever  you wish to call the tires, ie: rubber, skins, sneakers, and others. Tires are the most ignored, or understood part of your plane.image

Your cars tires life is pretty easy compared to an aircraft tire. You could use your car's tires to take off.. But landing is a whole nother kettle of fish. You, that is your wheels hit the runway at 70 to 200  knots. Try this stunt with car tires and they will shred.  And then you most likely will die. Game over. No do overs. Why is this you ask? Well it has to do with several factors: strong centrifugal forces,  and Traction Waves. Every time you land your tires distort. The forces on a Boeing 747 is about 6,000G. This has to do with the weight of the plane and the speed that you touch down.. Even a light aircraft landing at 100kn you tires will take a wallop.

Analysis:  Ok now what do we need? Ok lets use a car's TPMS as a model.

  1. We need the sensor in the tire with a transponder.. The data that we need and would like to capture:
    • Tire Pressure.. most of the damage is to under inflation.
    • Tire Temperature..
    • Tire mounted accelerometers to generate X and Y This tell you the amount of defection in the tire.
  2. We need a rf receiver at 428Mhz to acquire the data
  3. We need a rf transmitter near each wheel sending 127Khz to be the initiator.
  4. The receiver should send data to the embedded microprocessor via a bus, ie. CAN, TCPIP  etc.
  5. The display system and master caution will receive its data from the embedded microprocessor via a bus.


  • Sign in to reply

Top Comments

  • DAB
    DAB over 11 years ago +1
    I had some friends who worked at the Wright Patterson tire test center where they tested various aircraft tires for landing abuse. I had suggested that it would be easy to have the tires rotate at the…
  • dougw
    dougw over 11 years ago +1
    Way back when... I worked on a system to measure the rolling resistance of truck tires on real roads. Imagine how much money would be saved if the rolling resistance of all truck tires could be reduced…
  • dougw
    dougw over 11 years ago

    Way back when... I worked on a system to measure the rolling resistance of truck tires on real roads. Imagine how much money would be saved if the rolling resistance of all truck tires could be reduced by 1%. In addition to measuring all the forces on the tires, our system monitored the tire pressure and interior temperature. Interestingly the air temperature could rise to around 100 degrees C just from flexing friction, even in the middle of winter - this could make the tire pressure increase from 50%. So it might be useful to also measure temperature. Incidentally, that system could also adjust the tire pressure up or down on the fly or regulate it to a constant pressure regardless of temperature. (One thing we wanted to do was correlate tire pressure to rolling resistance). Instrumented tires might help reduce fuel costs by comparing tire readings to fuel consumption. If a database is used to collect the data it could help people choose more efficient tires, so internet connection adds a little more value. Another thing we were interested in is how the road surface affected fuel consumption. So if the data indicates the relative fuel efficiency of the road surface, and it is tied to GPS readings it may help people plot the route with the lowest cost of fuel. Even when electric vehicles take over, tire and road efficiency will still be very relevant.

    Doug

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 11 years ago

    I had some friends who worked at the Wright Patterson tire test center where they tested various aircraft tires for landing abuse.

     

    I had suggested that it would be easy to have the tires rotate at the airspeed with just a few modifications.  A moving tire would reduce the wear and tear on the tires by a considerable degree, but no body wanted to propose it as a solution.

     

    So I am not surprised that tire issues are still a problem in the aviation field.

     

    Car and truck tires suffer more from operator neglect than just about any other form of abuse.

    A low inflation value is usually a sign of more serious problem and I suspect that all the warning will do is have the people just put more air into the tire rather than doing a close examination for other problems.

     

    DAB