Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen: Using BJTs to drive pinlite displays
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 8 Oct 2020 5:36 PM Date Created
  • Views 751 views
  • Likes 4 likes
  • Comments 2 comments
  • pinlite
  • flight simulator
  • nexgen
  • diy hardware
  • arduino mega 2560
  • kw-105-al
  • cp-1252asn-128
  • diy software
  • bjt
Related
Recommended

NexGen: Using BJTs to drive pinlite displays

phoenixcomm
phoenixcomm
8 Oct 2020

Redacted April 10, 2024

imageStatement: Driving Pinlight Lamps is very challenging. The design requirements are 4vdc @ 15ma per segment, if you are interested look here.

So for the 7-segment displays, the total current is 7 x 15ma. or 105 ma. Now multiply that by 19 displays x 150ma or 1995 ma or just under 2 amps. For the 16-segment displays, of which there are 4 the total current is 16 x 4 x 15ma or 960 ma or just under 1 amp. An Arduino can't even handle one segment. So I need to buffer the displays from the Arduino.

The Plan: By the use of complementary BJT that is to say with a PNP Collector connected to the Power Rail and an NPN Emitter connected to the ground. By using the BJTs I can switch columns from the NPNs Base and each lamp segment from the PNPs Base. I don't think I will need a limiting resistor between the Power Rail and the NPNs Collector.

Power Rail
image
image

Ground Railimage

Most likely I will be using 2 BCD to 7-segment encoder as problems with fan out might occur.  The 4 16-segment lamps will be driven directly from one 16-bit port. So using a quick math of total-segments == (16x4) + (7x19) == 64 + 133 = 197 segments! At .2 seconds per segment = 39.4 seconds to access all 197 segments. Uyk! If I ran the multiplexer twice that speed or rather half the total time per segment = 17.2 seconds. Better but still cruddy.  So what would happen If I divided the tasks?

Possible Solution 1: Use four separate 74LS247 BCD  to 7-Segment  Decoders, each one called port A, port B, port C, port D and one Port E (16-bits). By using 3 x BCD to 1 of 8 decoders 74LS138 ganged together without using other gates.

Possible Solution 2: The mega has 50-odd digital ports? so 50/3 = 17 so I only need 6 more digital ports. here is my pin list:  (NOPE!!)

~~Cris H.>

 

Arduino Pin# 22 23 24 25 26 27 28 29 30 31 32 33 34 35 36
Reference Display 0 Display  1 Display 2 Display 3 Display 4
Arduino Pin# 37 38 39 40 41 42 43 44 45 46 47 48 49 50 51
Display 5 Display 6 Display 7 Display 8 Display 9

 

Possible Solution 3: In reality this will be the way to go. 1 will be using I2C 16-bit io-expanders I can use 15 bits from each expander to run 5 lamps. So this implies I will need 4 expanders to run the lamps. Now I can use 16 digital I/O or one more expander for the data lines for the 16-segment displays. (WINNER-WINNER-CHICKEN DINNER)

KISS METHODE

  • Sign in to reply

Top Comments

  • DAB
    DAB over 5 years ago +2
    Yes, it takes a bit of current to drive these displays, but then they need to be seen under a wide range of lighting conditions. DAB
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to DAB +1
    That's true, now add in dimming I most likely use a PWM signal as an input to a tri-state buffer. ~~Cris
Parents
  • DAB
    DAB over 5 years ago

    Yes, it takes a bit of current to drive these displays, but then they need to be seen under a wide range of lighting conditions.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to DAB

    That's true, now add in dimming image I most likely use a PWM signal as an input to a tri-state buffer.

    ~~Cris

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to DAB

    That's true, now add in dimming image I most likely use a PWM signal as an input to a tri-state buffer.

    ~~Cris