Ok, am I a little harsh, maybe, but when you have a keyboard that you don't use very much, just think of the wasted CPU cycles scanning the Keyboard! I one minute, in one hour? So what to do? In steps our 8 input to 3-line, Priority Encoder TI SN74x148.
| A0 | A1 | A3 | = | GS |
|---|---|---|---|---|
| H | H | H | 0 | H |
| 0 | 0 | 1 | 4 | L |
| Table 1 | ||||
Ok, you ask what is a Priority Encoder? Put it simply it is a device that will generate the proper output for any given key. Without a keypress, the encoder's output is 0.(update #2) So let's say you pressed 4 to a ground state, its output would be 001 hex or 4 (table 1). Plus the GS pin will go low. Cool. But beware if you doing this method you will be generating a processor interrupt, so you must eliminate switch bounce with a Schmitt Trigger.
The picture below is from the TI datasheet mentioned in the link above. Please remember that to pull the TTL device to the ground from a high, one of the switches must be connected to the ground while the other side of the switch is wired to a pin on the priority encoder is high which means that you will need a pull-up resistor.
The Priority Flag Pin must be connected to a Schmitt Trigger for debounce which is connected to your interrupt pin. (update #1)
So the only thing your software has to do when the interrupt is active is to read the 4 BCD data lines and perform a table lookup.
So in recap here is what you need:
- SN74x148 Priority Encoder
- SN74x08 or SN74x00
- SN74x14 Schmitt Trigger
- Resistor Networks x2 (9 pin 8 10k ohm) for pull-ups
- RC network for Schmitt Trigger.
OBTW
Your software is now simplified as if you know the value of the nibble, a simple 1-dimensional table would be all you need as you most likely want ASCII output. A quick review of C ints and Chars are the SAME! My keyboard has 0-9, ENT, KBD, CLR, TGT
| 30 | 31 | 32 | 33 | 34 | 35 | 36 | 37 | 38 | 39 | 10 | 41 | 42 | 43 |
| 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 | 8 | 9 | ENT | CLR | KBD | TGT |
char keyboardDecoder( int value ) {
static int decoder[ ] = { 30, 31, 32, 33, 34, 35, 36, 37, 38, 39, 10, 41, 42, 43 }
return ( decoder[ value ] ); }
UPDATES
- Added the sentence starting with The Priority Flag Pin 1/18/2020 CAH
- Added the sentence with Without a keypress 1/18/2020 CAH
- To make decoding without the zero as an input you can start as the array index as 1, not zero so my array would start as 1 outputting 30. 1/18/2020 CAH
- PLEASE NOTE: The implied decimal zero condition requires no input condition, as zero is encoded when all nine data lines are at a high logic level. TI DATA BOOK
- UPDATED PAGE after "They Moved to a new provider" JUNE 7, 2023 -CAH
Top Comments
-
Jan Cumps
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
-
phoenixcomm
in reply to Jan Cumps
-
Cancel
-
Vote Up
+2
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Comment-
phoenixcomm
in reply to Jan Cumps
-
Cancel
-
Vote Up
+2
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Children