Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator The Lab: As The World Tuns
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 13 Apr 2025 8:47 PM Date Created
  • Views 1336 views
  • Likes 9 likes
  • Comments 6 comments
  • phoenixcomm.net
Related
Recommended

The Lab: As The World Tuns

phoenixcomm
phoenixcomm
13 Apr 2025

imageAs The World Turns, Things still don't stand well. I had a forward-facing server with a public IP, for well over more than a few decades. About 2 weeks ago. I got nailed, So I had to put the server on an Internal class C address (192.168.xx.xx). I was going to use one of my Pies for a Proxy Server, with My Public address with a virtual private address on the same LAN cable It will look something like this when Im done, so for now, I have a lot work on my plate, I have not forgotten about the build for the Shift It, Move it blogs. I will eventually get to it but it will be a while as I cant find my Pie3 for the Proxy Server, So I will be using my Beagle board 1 witch does not have enough any USB-3.0 slots for the HD, or the second network adapter. So I will have to upgrade it to the Pie when I turns up. At the moment our Sites are Dark.~~ Cris H. phoenixcomm.net, phoenixaerospace.us, smarthab.us and others. :(>image

  • Sign in to reply
Parents
  • COMPACT
    COMPACT over 1 year ago

    Sorry to hear that. Edge protection is vital.

    Backup, Backup, Backup with regularly properly tested recovery procedures is one of my mottos!

    One of my systems died and with today's multichannel PCI-e channel storage (in disbelief) I was able to recover 110+GBytes and be back up online within 10 minutes.

    Damned amazing. - However if it can be recovered that quickly imagine how fast it can be trashed!

    Cheers to all!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 1 year ago in reply to COMPACT

     community.element14.com/.../compact what sw did you use slow.i use r-linux had a lot out and pdfs plus my myaql which is redundant with RAID 5 over 3 drives. One of my ups failed a my lost the whole thing. But not realy I lost the drive reg.not fstab , took a week but rebuilt the raid a registered the drive and presto back on the air.but I need to upgrade the os debian from 10.x to 12.x fun.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • COMPACT
    COMPACT over 1 year ago in reply to phoenixcomm

    I use Acronis CyberProtect which AFAIK is not for linux. Interestingly I was once a proponent of UPS on workstations but have had far more reliability without them on workstations. One issue is periodic expensive battery replacement & being perpetually hassled by the vendor to upgrade the hardware citing that the old hardware is unreliable. Undersizing them is also an issue. IMHO you need to have at least twice the calculated capacity to cater a subsequent outage if the battery has already been drained by outage. (However it doesn't cater for an outage after a battery drain test!).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • COMPACT
    COMPACT over 1 year ago in reply to phoenixcomm

    I use Acronis CyberProtect which AFAIK is not for linux. Interestingly I was once a proponent of UPS on workstations but have had far more reliability without them on workstations. One issue is periodic expensive battery replacement & being perpetually hassled by the vendor to upgrade the hardware citing that the old hardware is unreliable. Undersizing them is also an issue. IMHO you need to have at least twice the calculated capacity to cater a subsequent outage if the battery has already been drained by outage. (However it doesn't cater for an outage after a battery drain test!).