Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator Why does it matter?!
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 30 Jan 2025 6:41 PM Date Created
  • Views 1179 views
  • Likes 8 likes
  • Comments 14 comments
  • wifi
  • matter protocol
Related
Recommended

Why does it matter?!

phoenixcomm
phoenixcomm
30 Jan 2025

Most of my work is in aviation and avionics where wifi is plage along with 'on the go' usb ports on routers so almost 99% is WIRED, and wifi turned off! This type of paranoia extends in my SmartHab project. We don't want my house security to be snooped or hacked! So in the long run matter does not mater. It's a hole you can't close! Wifi is the hole you can't close the door once you open it. Like a wifi printer on you desk, are you that lazy that you can't run a usb cable 3 feet? ~~ Cris H 

  • Sign in to reply

Top Comments

  • phoenixcomm
    phoenixcomm over 1 year ago in reply to kmikemoo +1
    kmikemoo New Builds are very easy most of the time. Post Builds are FPITA. In my office I do something that saves my but! I use PVC pipe it very cheap! I use 1.5" pipe but next time i will use 2". The…
  • phoenixcomm
    phoenixcomm over 1 year ago in reply to Jan Cumps +1
    Jan Cumps Yup so do I. last 15 years or so. but I grab PVC and run it around the ceiling. BTW I started with this madness when I had the ISP (still up -400+ customers. now 2 box on a 1Gb fiber line from…
  • phoenixcomm
    phoenixcomm over 1 year ago in reply to kmikemoo

     kmikemoo New Builds are very easy most of the time. Post Builds are FPITA. In my office I do something that saves my but! I use PVC pipe it very cheap! I use 1.5" pipe but next time i will use 2". The problem comes when you pull wires through the tube, so I cut abut 1" slot in the pipe NEVER cut into the ends or the pipe looses its friction fit. Here is what I did. 

    imageimage

    imageimage

    Not shown is the Cisco VOIP Router/Switch this is on a shelf which is at a right angle to picture 1. In picture 2 you will notice the slit in the PVC, It does not go to the ends of the pipe as then the interference fit will not work. I don't have glue on any of my joints, just friction. Now this is a big error in the pipe in picture 2  you will not in the corner I used the wrong fitting I used a 'L' instead of a 'swept-L' you can see a 'swept-Y' in picture 1. The other thing that could be changed was that I only used 1.5" PVC I should have used 2" but 1.5 would be fine for down tubes. 

    Dont be put off by the amount of work. Oh one more thing I did not use a Jack Panel. As you can see the between pictures 1 and 4 the colors match, and that Ids whats in what port. BLUE = NexGen Net, RED/ORANGE = Office Net, Then you have WHITE and TAN one is for the VOIP phone system  and I think one is a spare. Oh yes I have to clean use the rats nest in picture 1 and get the wire inside the tube in picture 2 but other things keep popping up.  

    BTW  kmikemoo  "PLETHORA of USB cables" thats not even close. I have 3 monitors (1 HDMI + TV) the rest are DVI, 2 network cables A Cisco VOIP with cable, USB Keyboard Dell, and a Trackman Mouse. Video CAM, Barcode scanner, My TARDIS USB hub, And Lastly my computer Tall case ~~ Cris

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 1 year ago

    Hehe controversial! ; ) I can't recall if the printer I use is wired or wireless (testament to how reliable it's been, I've never checked the connection), but I have to say, I love the capability to send it print jobs from the mobile phone. Or laptop, or if family members visit and bring their laptop for whatever purpose, and need to quickly print something without needing to find a cable for the printer (I think some laptops don't have USB type A any more).

    It is an old printer model now, but the mobile capability is excellent for quickly printing off PDFs etc without needing to turn on the PC and re-navigating to whatever document I might have been looking at on the mobile phone. I'm sure there are far better printers now, mine is Brother MFC-L8690CDW if anyone is curious about the model. I've had it for 7 years so far, it's still on the original ink cartridges.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago

    I'm wireless wherever possible. I rent an apartment. Can't put new wires in a wall and don't want network cables on the floor.  Wirless printer allows me to put it aside, so that it doesn't use prime space on or near my work area. It sits in a closet.

    I also move my work area to whatever is the nicest place that day. In the winter in the rooms where there is sunshine. In the summer to where there is shadow. 

    Even my HDMI for TV is wireless. Works really well, and I don't have an HDMI cable on the living room floor between access point and where the TV is. There is a walkway between those two points

    image

    image

    Wireless equals freedom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kmikemoo
    kmikemoo over 1 year ago

    Joy I just installed a new (to me) Wi-Fi capable printer last night - and asked myself a similar question.  Why would I choose the slower connection?  Besides, I have a PLETHORA of USB cables.     I was quite disappointed when I got new "cable" for the TV.  I have a Cat5 drop right behind the TV, but the cable box only does Wi-Fi.  I had to pull my range extender from the garage into the house to get a strong enough signal for the box to work reliably.  Again... 3 foot of cable could have resolved that issue.
    It's hard to beat the dependability of wired.  It's just a PITA to install. Joy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<