Personal Blogs
  • Community Hub
  • More
Personal Blogs
Nico teWinkel's Blog FRM-KL25z, installing headers
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ntewinkel
  • Date Created: 12 May 2013 6:29 PM Date Created
  • Views 1689 views
  • Likes 2 likes
  • Comments 9 comments
  • tutorial
  • freescale
  • frdm
  • frdm-kl25z
  • soldering
  • codeexchange
Related
Recommended

FRM-KL25z, installing headers

ntewinkel
ntewinkel
12 May 2013

Unfortunately, the Freescale Freedom FRDM-KL25z does not come with headers installed, or even included.

This set me back a few weeks having to wait for some headers to arrive in the mail - although I admit that as a good electronics nerd I should have already had some of these on hand image

 

Last week I finally received some double headers for my Freescale Freedom board. Hooray!

 

I purchased some 2x40pin headers for the job. The FRDM board uses 1 of 2x6, 2 of 2x8, and 1 of 2x10 headers, so it would be easier to just buy sets of those instead. I probably should have done that, but I think at the time I just couldn't find the ones I needed. The 2x40 are very inexpensive, so it does save a few dollars and since I don't foresee doing this regularly it also keeps me from hoarding more parts image

 

In any case, one 2x40 piece is enough for the FRDM board. The trick is to score across a connector on both sides and then snap it off there, losing one connector in the process. For example, to cut the 2x10 piece, I used a hobby knife to score across the 11th connection.

image

 

A little bit of cleanup at the snapped ends, and viola! I have the pieces I need:

image

 

So I soldered them on.

That takes a little bit of fiddling soldering effort, but it's good practice and it's not difficult to do. I would even consider it a great learning opportunity for beginner students.

For those who haven't done any soldering before, Lady Ada has come up with a nice list of tutorials: http://www.ladyada.net/learn/soldering/thm.html

I'm by no means an expert, so I should probably have a look at them to see if I can pick up on any new techniques image

 

One little trick I did use is that I plugged in a shield to help keep the headers all aligned squarely.

 

This is what the board looks like now, ready to connect external bits:

image

 

And this is the soldered side:

image

Like I said, I'm no expert. But I think I got some nice connections - the little pyramids are not looking too bad. I double checked with a magnifying lens to make sure I didn't short anything out. On a side note, that magnifying lens is part of the soldering "helping hands" I bought recently - highly recommended! I don't know how I ever soldered little bits without them. Probably because I used to have better eyes, steadier hands, and much more patience image

 

However, my soldered bits never look as nice and shiny as the ones you see on commercially produced boards, and I always end up with the flux sorta coating the area. I usually wipe around as best as possible using a kleenex and q-tips.

 

Can any soldering experts give me some advice on what I can do to change that?

Is it the solder I'm using?

Can I wash off the flux without harming the board? I've heard of maybe using a toothbrush to do that, but I would hate to get water staying under the chips, for example.

 

Cheers,

-Nico

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 13 years ago +1
    Hi Nico, I think it may rather be the type of solder. Some traditional solders have rosin flux, which works very well but does leave a mess (which can be cleaned with isopropanol - and a firm brush as…
  • mcb1
    mcb1 over 13 years ago in reply to shabaz +1
    Nico Your headers look strangely like the ones I had ..too long. The magnifying glass is almost a given now ...the smd are the hard part, so plenty of light. Luckily at work we have a multitude of flux…
  • mcb1
    mcb1 over 13 years ago in reply to ntewinkel +1
    I think they just set up alias'es. I have given Hanno (12blocks) one to play with while he travels around the states. He nearly fell over when I told him the price. It shouldn't be hard for him to add…
Parents
  • shabaz
    shabaz over 13 years ago

    Hi Nico,

     

    I think it may rather be the type of solder. Some traditional solders have rosin flux, which works very well but does leave a mess (which can be cleaned with isopropanol - and a firm brush as you say, but you may wish to have an antistatic brush - I use this one, it has lasted years so it's worth the cost. (After the IPA, I believe deionized water can be used, but currently I'm using some MG chemicals mix of IPA and deionized water because that's all I had, and it gets the board spotless).

    You still need a flux-cored solder, but maybe a non-rosin based one; it will likely leave a clean joint (but will require a clean board and clean component wires).

    You may need a recommendation based on the country you're in. I use a UK-based manufacturer.

    Since most components are clean and untarnished, a non-rosin solder is good enough (bare copper PCBs need some cleaning however).

    This is just personal findings based on prototyping stuff - I'm no expert on commercial production methods.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to shabaz

    Nico

    Your headers look strangely like the ones I had ..too long.

    The magnifying glass is almost a given now ...the smd are the hard part, so plenty of light.

     

    Luckily at work we have a multitude of flux removing types all from E14 of course.

     

    However at home methylated spirits works well.

    You need to scrub a little, and holding the board vertical allows it to run off the edge (isn't gravity neat).

     

    If you hunt around the mbed site, someone has started an Arduino library that basically allows a copy and paste.

    It's not complete, but will be a valuable asset if someone has the time to complete it.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 13 years ago in reply to shabaz

    Nico

    Your headers look strangely like the ones I had ..too long.

    The magnifying glass is almost a given now ...the smd are the hard part, so plenty of light.

     

    Luckily at work we have a multitude of flux removing types all from E14 of course.

     

    However at home methylated spirits works well.

    You need to scrub a little, and holding the board vertical allows it to run off the edge (isn't gravity neat).

     

    If you hunt around the mbed site, someone has started an Arduino library that basically allows a copy and paste.

    It's not complete, but will be a valuable asset if someone has the time to complete it.

     

    Mark