Personal Blogs
  • Community Hub
  • More
Personal Blogs
Nico teWinkel's Blog Nail Polish Short-proofing?
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ntewinkel
  • Date Created: 26 May 2018 11:57 PM Date Created
  • Views 3553 views
  • Likes 10 likes
  • Comments 18 comments
  • nail polish
  • conformal
  • heat_shrink_tube
  • conformal coating
Related
Recommended

Nail Polish Short-proofing?

ntewinkel
ntewinkel
26 May 2018

Hi all,

 

I just kind of randomly came across a thread discussing using nail polish to cover electrical connections to avoid shorts, especially for the backs of home made PCBs.

There are commercially available "conformal coatings" you can use, but they are somewhat more pricey, and I guess a fair bit more boring image

 

So I went to the dollar store yesterday and picked me up some of this!

image

 

Only $1.50 (Canadian dollars even!)

I was thinking I might use it on a past or future PCB to coat the back.

 

This is the first time I've ever bought nail polish, which I think explains the conservative colours image

It says "Kozmic Colours", so just imagine the variety available! I thought I'd avoid the sparkly ones though, as I wasn't sure if that might be conductive.

 

Then today I soldered a light resistor onto some wires, and then wished I had remembered to put on some heat shrink tubes. The shrink tubes were aaaalll the way in the workshop and I was being lazy image

Then I realized I could probably use the nail polish for this!

imageimage

 

It looks like it does the trick - as you can see in the pictures, it has fully coated the exposed wires. It's easier than dealing with heat shrink tubing, and can be added as an afterthought. It's not as rugged as heat shrink tubing, but for many of these smaller light-duty cases it's perfect.

 

Next time - red and black!

 

Cheers,

-Nico

 

edit: I just did a quick resistance test, and I can clip the test leads right beside each other on a (coated) pin of the sensor with full resistance.

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 7 years ago +5
    Hi Nico, I would be interested in learning more about its insulation value. I am sure you could increase the insulation value by putting multiple coats on it. If smell is any indication it should be pretty…
  • mcb1
    mcb1 over 7 years ago +4
    This is the first time I've ever bought nail polish Are you sure .... For higher power/mains systems I can't see it meeting any sort of voltage rating, but for low voltage, if it gets you out of a problem…
  • mcb1
    mcb1 over 7 years ago in reply to jw0752 +4
    I'm starting to get worried now that you boys are becoming proficient in buying and using nail polish. The proper coatings might be a worthwhile roadtest. What do you think rscasny ( about the road test…
Parents
  • DAB
    DAB over 7 years ago

    Hi Nico.

     

    Did you verify the insulation using a multimeter?

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 7 years ago in reply to DAB

    Hi DAB,

    >Did you verify the insulation using a multimeter?

    Yes, but only for the basic "does it conduct" case, not anything more fancy.

    image

     

    However, after a few times fiddling around trying to get a good picture, the polish already came off due to the clips scratching it, and then it conducted again! (I can see the shiny wire, so it's not the nail polish conducting)

    I'll add another layer.

     

    -Nico

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ntewinkel
    ntewinkel over 7 years ago in reply to DAB

    Hi DAB,

    >Did you verify the insulation using a multimeter?

    Yes, but only for the basic "does it conduct" case, not anything more fancy.

    image

     

    However, after a few times fiddling around trying to get a good picture, the polish already came off due to the clips scratching it, and then it conducted again! (I can see the shiny wire, so it's not the nail polish conducting)

    I'll add another layer.

     

    -Nico

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mcb1
    mcb1 over 7 years ago in reply to ntewinkel

    after a few times fiddling around trying to get a good picture, the polish already came off due to the clips scratching it

    I suspect any coating that drys hard, will chip of break when moved, so it has limited use.

     

    We had the same sort of issues when trying to seal antenna with RTV and other types of sealant that set.

    In the end an almost grease like substance sorted the issue, and never let moisture in over years.

     

    I suspect a simple layer or two of insulation tape might achieve exactly what you want.

    I've been known to wrap one wire, then with the same piece of tape, join the second wire onto the (taped) first wire, and wrap a couple of layers over both wires.

     

     

    I'm beating that next time you'll go " blast and bother, I forget the heatshrink ... best I redo this" (substitute your own adjectives) image

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to mcb1

    I've been known to wrap one wire, then with the same piece of tape, join the second wire onto the (taped) first wire, and wrap a couple of layers over both wires.

    I do that sometimes as well image

    • Cancel
    • Vote Up +2 Vote Down