Personal Blogs
  • Community Hub
  • More
Personal Blogs
Nico teWinkel's Blog Nail Polish Short-proofing?
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ntewinkel
  • Date Created: 26 May 2018 11:57 PM Date Created
  • Views 5265 views
  • Likes 10 likes
  • Comments 18 comments
  • nail polish
  • conformal
  • heat_shrink_tube
  • conformal coating
Related
Recommended

Nail Polish Short-proofing?

ntewinkel
ntewinkel
26 May 2018

Hi all,

 

I just kind of randomly came across a thread discussing using nail polish to cover electrical connections to avoid shorts, especially for the backs of home made PCBs.

There are commercially available "conformal coatings" you can use, but they are somewhat more pricey, and I guess a fair bit more boring image

 

So I went to the dollar store yesterday and picked me up some of this!

image

 

Only $1.50 (Canadian dollars even!)

I was thinking I might use it on a past or future PCB to coat the back.

 

This is the first time I've ever bought nail polish, which I think explains the conservative colours image

It says "Kozmic Colours", so just imagine the variety available! I thought I'd avoid the sparkly ones though, as I wasn't sure if that might be conductive.

 

Then today I soldered a light resistor onto some wires, and then wished I had remembered to put on some heat shrink tubes. The shrink tubes were aaaalll the way in the workshop and I was being lazy image

Then I realized I could probably use the nail polish for this!

imageimage

 

It looks like it does the trick - as you can see in the pictures, it has fully coated the exposed wires. It's easier than dealing with heat shrink tubing, and can be added as an afterthought. It's not as rugged as heat shrink tubing, but for many of these smaller light-duty cases it's perfect.

 

Next time - red and black!

 

Cheers,

-Nico

 

edit: I just did a quick resistance test, and I can clip the test leads right beside each other on a (coated) pin of the sensor with full resistance.

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 8 years ago +5
    Hi Nico, I would be interested in learning more about its insulation value. I am sure you could increase the insulation value by putting multiple coats on it. If smell is any indication it should be pretty…
  • mcb1
    mcb1 over 8 years ago +4
    This is the first time I've ever bought nail polish Are you sure .... For higher power/mains systems I can't see it meeting any sort of voltage rating, but for low voltage, if it gets you out of a problem…
  • mcb1
    mcb1 over 8 years ago in reply to jw0752 +4
    I'm starting to get worried now that you boys are becoming proficient in buying and using nail polish. The proper coatings might be a worthwhile roadtest. What do you think rscasny ( about the road test…
  • jw0752
    jw0752 over 8 years ago in reply to ntewinkel

    Hi Nico,

    No I never buy the shimmery stuff either. I wish it was a little more opaque though. At first I thought it was translucent because I wasn't stirring it well enough but now I think it is just because it costs 1$.

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to jw0752

    Oh interesting!

    And it sounds like you've been using it successfully for some time now, for quite the high current application.

     

    >and used some green to seal the solder pad.

    I was actually looking for green, but all they had was the shimmery stuff.

    LOL I never thought we'd be discussing nail polish colours in this forum - mcb1 might be justified with his worries image

     

    -Nico

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to jw0752

    I'm starting to get worried now that you boys are becoming proficient in buying and using nail polish. image

     

     

    The proper coatings might be a worthwhile roadtest.

    What do you think rscasny (about the road test, not which colour nail polish image )

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 8 years ago

    Hi Nico,

     

    I would be interested in learning more about its insulation value. I am sure you could increase the insulation value by putting multiple coats on it. If smell is any indication it should be pretty good as it smells just like the spray we used to use on TVs to eliminate corona in the high voltage sections. I too use the dollar store version to touch up solder connections on sterilizer circuit boards as they operate in a moist environment. I also like that I can buy colors like the green and black

    which blend in with the existing coatings. I just finished working on a board this evening and used some green to seal the solder pad.

     

    image

     

    This is a design problem with a main control board where the fuse clips are under rated for the current and they eventually over heat and carbonize the circuit board. By the time I get them the solder pad itself is loose and sitting on blackened circuit board. the blacken board is cut out and a new piece of resin inserted. I replace the clips with 30A rated instead of the original 15A and I use solder braid that goes through the circuit board and around the base of the fuse clip and then back to the rail under power.

     

    John

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to shabaz

    > Smells nice while it is drying too : )

     

    I was expecting it to be a lot more toxic smelling, but it didn't really have much of a smell... maybe the solder flux was still numbing my senses image

     

    >For higher power/mains systems it may be risky

     

    Right, personally I'd avoid it for anything other than the low voltage USB or lower projects, as it seems to be a kind of soft coating (judging by the many chips and scrapes the ladies get on them).

     

    > it contains flammable stuff? I'm no chemist though : ) Maybe it is non-flammable when dry, since so many people stick it on their nails : )

    I'm pretty sure the fumes the wet stuff gives off will burn. I might have to test flammability of the dry stuff, now that you brought it up, and it has nothing to do with my pyromaniac issues image

    But yes, it's not often we see smokers have their nail coatings catch on fire image  You'd think that would be a great incentive to stop, but then again the danger factor might be another incentive for them to start. image

     

    > I wonder what other fast-drying paint-on coatings are easily available too.

     

    Good question. It's amazing actually how often inexpensive easy-to-find everyday items can come in handy for our projects!

    This stuff comes to mind: Plasti DipRegistered Liquid | Canadian Tire

    It's a thick rubberized coating sort of thing. It's $25, but that's a huge amount of it.

     

    -Nico

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>