Personal Blogs
  • Community Hub
  • More
Personal Blogs
Nico teWinkel's Blog New heat shrink solder connectors
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ntewinkel
  • Date Created: 13 Jul 2023 9:50 PM Date Created
  • Views 1280 views
  • Likes 11 likes
  • Comments 4 comments
  • Heat shrink
  • solder
Related
Recommended

New heat shrink solder connectors

ntewinkel
ntewinkel
13 Jul 2023
New heat shrink solder connectors

I saw these on a new discount website (in Canada) and thought I’d try them out, as they are fairly inexpensive. I thought they might be handy when fixing something on the in-law’s boat or golf cart, for example.

image

The idea is that they solder and shrink and water seal the connection, just using a heat gun.

image

It seems to do a decent job, and I can see that the solder flowed.

I probably should have used flux on the wires, and I think that center ring is also a crimp ring, so I probably should’ve crimped the connection first. But it’s a strong connection even without it.

I think I’ll be using this next time I need to fix something there. Much easier than soldering and heat shrink sealing separately.

EDIT: Here's a video by BigCliveDotCom on YouTube, where he reviews these connectors: https://www.youtube.com/watch?v=unxEdyW8RP8

  • Sign in to reply

Top Comments

  • dougw
    dougw over 3 years ago +1
    nice integrated solution
  • ntewinkel
    ntewinkel over 3 years ago in reply to ntewinkel +1
    Ps, I’m guessing it would be extra handy for field fixes when all you need is a cigarette lighter.
Parents
  • Fred27
    Fred27 over 3 years ago

    It's certainly an easy fix and it looks like reasonably quality, but hard to tell from a photo. I assume that must be a fairly low temperature solder if it will flow at the sort of temperatures you'd get when heat shrinking.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 3 years ago in reply to Fred27

    Correct, it’s “reasonable quality”, probably not “excellent”. A hand made solder joint would be much better. It does say it’s a low temperature solder, yes.

    But all I had to do was twist the wires together a little bit and slide the connector over (I’ll definitely also crimp it next time), so it’s far less effort. 80/20 rule Laughing 

    The little red bands seem to add extra strength and water sealing, which is cool. They shrink tightly into place. Hard to tell exactly how water tight it is though.

    Mostly I think it will be good for those trailer / ATV / golf cart type fixes when I’d rather not be in the weather too long!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ntewinkel
    ntewinkel over 3 years ago in reply to Fred27

    Correct, it’s “reasonable quality”, probably not “excellent”. A hand made solder joint would be much better. It does say it’s a low temperature solder, yes.

    But all I had to do was twist the wires together a little bit and slide the connector over (I’ll definitely also crimp it next time), so it’s far less effort. 80/20 rule Laughing 

    The little red bands seem to add extra strength and water sealing, which is cool. They shrink tightly into place. Hard to tell exactly how water tight it is though.

    Mostly I think it will be good for those trailer / ATV / golf cart type fixes when I’d rather not be in the weather too long!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ntewinkel
    ntewinkel over 3 years ago in reply to ntewinkel

    Ps, I’m guessing it would be extra handy for field fixes when all you need is a cigarette lighter.