Personal Blogs
  • Community Hub
  • More
Personal Blogs
Ralph Yamamoto's Blog Filament LED Failure Conundrum
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 18 Nov 2021 11:17 PM Date Created
  • Views 8485 views
  • Likes 10 likes
  • Comments 6 comments
  • outdoor led lights
  • premature led failure
  • garage lights
  • st64_st21
  • filament led bulbs
  • edison led bulbs
  • dimmable leds
Related
Recommended

Filament LED Failure Conundrum

ralphjy
ralphjy
18 Nov 2021

I recently started having problems with an LED bulb "burning out".  I've used LED filament lights for a few years.  I have noticed that they don't seem to have the lifespan of the more prevalent individual chip on substrate lights that I normally use.  If the chip on substrate LEDs fail early it is usually due to the LEDS having a poor bond to the heatsink which causes thermal induced failure (once I had a component fail in the current source).  These filament bulbs normally seem only to last 2-3 years @ ~4000hrs/year.  I use them in my outdoor garage lamps to get the old style "filament" appearance.

 

One of my older filament bulbs started to get dim, so I replaced it with a new one.  After about a week I noticed that the new bulb was also dim.  I verified that the bulb itself was bad and replaced it with another new one - only to have it also fail after a few days.

 

This bulb is on a circuit with with 4 other bulbs (3 lamps on the garage and 2 on my entry).  All of the other bulbs are doing fine.

image

 

In old incandescent bulbs this would usually indicate an intermittent socket contact causing the filament to burn out..

 

 

These are the bulbs that I'm using:

 

Vintage Dimmable Edison LED Light Bulbs 100W Equivalent, E26 Base ST64/ST21 8W LED Filament Bulbs, 2700K Warm White, 1200Lumens, Antique Clear Glass Light Bulbs.

image

 

 

I took a quick look on wikipedia: https://en.wikipedia.org/wiki/LED_filament .

image

 

Some excerpts of interest:

"The LED filament consists of multiple series-connected LEDs on a transparent substrate, referred to as chip-on-glass (COG). These transparent substrates are made of glass or sapphire materials. This transparency allows the emitted light to disperse evenly and uniformly without any interference. An even coating of yellow phosphor in a silicone resin binder material converts the blue light generated by the LEDs into light approximating white light of the desired colour temperature—typically 2700 K to match the warm white of an incandescent bulb."

 

"The lifespan of LED emitters is reduced by high operating temperatures. LED filament bulbs have many smaller, lower-power LED chips than other types, avoiding the need for a heatsink, but they must still pay attention to thermal management; multiple heat-dissipation paths are needed for reliable operation. The lamp may contain a high-thermal-conductivity gas (helium) blend to better conduct heat from the LED filament to the glass bulb."

 

"The life expectancy of the LED chips correlates to the junction temperature (Tj); light output falls faster with time at higher junction temperatures. Achieving a 30,000 hour life expectancy while maintaining 90% luminous flux requires the junction temperature to be maintained below 85 °C.  Also worth noting is that LED filaments can burn out quickly if the controlled gas fill is ever lost for any reason."

 

But nothing that suggests that this is a typical early failure mode.  I doubt that it is caused by bad filaments since they all went dim at the same time.  More likely caused by the electronics in the socket base.

 

Anyone else experience this type of repeated failure where only a single bulb in a parallel circuit is going bad?  I guess I'll have to deconstruct the bulb to determine what actually failed.  I noticed that this is a "dimmable" bulb.  At least now I have a couple of bad ones to play with image.

  • Sign in to reply

Top Comments

  • scottiebabe
    scottiebabe over 4 years ago +2
    I can sympathize with your LED woes. It is that time of year again for decorative string lights! The LEDs last a lifetime, but the cheap plated steel lead frames corrode out in a few weeks. Hurray for…
Parents
  • kmikemoo
    kmikemoo over 4 years ago

    ralphjy  I have also been greatly disappointed with my LED light bulbs.  The regular lamp bulbs don't last any longer than the incandescent ones they replaced.  I have had two flame out in the base.  My foray into LED Christmas lights was an abysmal disaster.  At least one of the three strings dies each year.  They aren't any better or any different than the normal string lights - except that they cost a lot more.  I only used them 3 years.  I've gone back to the old school C9's.

    I bought 6 COB LED panels.  Oh, my!  They heat up as efficiently as a stove element - except that I don't want to cook anything with them.  I'm still thinking about a heat recovery system and I'll turn them into a micro-cogeneration plant.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • kmikemoo
    kmikemoo over 4 years ago

    ralphjy  I have also been greatly disappointed with my LED light bulbs.  The regular lamp bulbs don't last any longer than the incandescent ones they replaced.  I have had two flame out in the base.  My foray into LED Christmas lights was an abysmal disaster.  At least one of the three strings dies each year.  They aren't any better or any different than the normal string lights - except that they cost a lot more.  I only used them 3 years.  I've gone back to the old school C9's.

    I bought 6 COB LED panels.  Oh, my!  They heat up as efficiently as a stove element - except that I don't want to cook anything with them.  I'm still thinking about a heat recovery system and I'll turn them into a micro-cogeneration plant.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ralphjy
    ralphjy over 4 years ago in reply to kmikemoo

    kmikemoo, I've actually had pretty good luck with LEDs since I converted the whole house over about 5 years ago.  I had a few infant mortalities - probably due to manufacturing defects - that I got replaced under warranty.  Just not with these filament bulbs that I use outside on the garage.  I tried a couple of different manufacturers, so it must be a design issue.  I can tolerate a lifespan of a few thousand hours, but with this new failure mode I'll probably try different bulb types.