Personal Blogs
  • Community Hub
  • More
Personal Blogs
Ralph Yamamoto's Blog OAK-D-Lite - DepthAI Camera
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 15 Jan 2022 9:54 PM Date Created
  • Views 19113 views
  • Likes 10 likes
  • Comments 1 comment
  • movidius
  • kickstarter
  • openvino
  • lux-esp32
  • oak-d-lite
Related
Recommended

OAK-D-Lite - DepthAI Camera

ralphjy
ralphjy
15 Jan 2022

Last year Luxonis ran a Kickstarter campaign to add another camera to their OAK-D DepthAI lineup -> the OAK-D-Lite.

Like the other DepthAI cameras it uses the Intel Movidius Myriad-X VPU as its vision engine and has the familiar 3 camera setup (2 lower resolution monochrome cameras for depth and a high quality 4K color main camera).

I've not used the original OAK-D cameras, but I have a LUX-ESP32 (OAK-D-IoT-40) that I used in a Hackster project last year: AI Enhanced Security Camera.

The OAK-D-Lite is cost optimized and neatly packaged in a compact housing (28x91x18mm).  The two depth cameras have reduced resolution from other OAK-Ds -> 1280x800 to 640x480.  Most depth applications were running at the lower resolution, so this saved on the camera cost.  The target retail cost is $99 which is half the price of the LUX-ESP32.  Of course, it does not have the ESP32 processor for wireless communication or the external power module (it is powered by the USB-C jack).  I think that they were good tradeoffs for most users and it is nice to get robust packaging (LUX-ESP32 is bare board assembly).

Here is the Kickstarter link: OpenCV AI Kit - Lite.

image

I just got my unit about a week ago.  Here are pics showing a size comparison of the two units.  The LUX-ESP32 is in a homebrew open frame tripod mount that I printed.

image

image

Hardware Specifications

image

The DepthAI cameras are reasonably straightforward to use.  They normally power up a USB bootrom which allows you to upload the VPU firmware over USB,

Just need to verify that it has been recognized as a USB device:

image

There is a Windows Installer that will get you up and running quickly with a demo program.

The demo program allows you to configure the Depth and Main Cameras and also allows choosing between a fair sample of AI models.  In the video you can see the load time for the model firmware.  I tried switching between mobile-net ssd, face-detection and tiny-yolo-v3

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The nice thing about using a Movidius VPU is that there are many AI models available in the Intel OpenVino Model Zoo.

Unfortunately for me, I have a very full schedule for a few months - so I'll have to wait to do a project with this.  I think what I would like to try is integrating this with a Raspberry Pi Zero 2 W that I used in this post: Raspberry Pi Zero 2 W MotionEyeOS.

  • Sign in to reply
  • DAB
    DAB over 4 years ago

    I was tempted by the offer, so I am very interested in what you come up with using this device.