Personal Blogs
  • Community Hub
  • More
Personal Blogs
Ralph Yamamoto's Blog Preparing to add a laser to my CNC router
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 7 Nov 2019 4:38 PM Date Created
  • Views 2799 views
  • Likes 9 likes
  • Comments 5 comments
  • genmitsu cnc 3018-pro
  • laser engraving
Related
Recommended

Preparing to add a laser to my CNC router

ralphjy
ralphjy
7 Nov 2019

Earlier this year I got a low cost CNC router to complement my 3D printing capabilty.  The Genmitsu 3018 Pro is a great low cost router with a working volume of 300mm x 180mm x45mm and it also has the option on its controller board to use a PWM output to control a laser module (actually has 2 connector ports).  The diameter of the spindle clamp would allow it to use common 30mm x 30mm laser modules without any modification.  So, with the addition of a laser module and LaserGRBL software I could do laser engraving and cutting,  I'm thinking that will be my Christmas present from Santa this year.

image

 

I had an exchange of messages with shabaz and Fred27  about laser safety and decided that before I get my laser module that I should get some safety equipment.  Here's what I decided to get.

 

Safety Equipment

  1. Protective eyewear
  2. Fire extinguisher
  3. Remote monitor

 

Protective eyewear

I took Shabaz's recommendation and got the LS02 Safety Glasses from Edmund Optical.  I am going to get a laser in the 450 - 500nm range and these glasses are rated with an Optical Density >7 @ 180 - 532nm.

image

 

This particular model fits over my prescription glasses.  I like that the working range is marked on the front of the lens.

image

image

image

Link:  https://www.edmundoptics.com/p/arg-lasershield-safety-glasses/41399/

 

 

Fire extinguisher

I'm still looking for a small CO2 extinguisher because the dry chemical ones make too much of a mess.  I'll probably need to find an industrial supplier.

 

 

Remote monitor

I decided to mount a Pan/Tilt IP camera on the ceiling so that I could monitor the laser from the adjacent room on a computer or mobile device.  The pan and tilt capability also lets me monitor other activity in the workroom like when I am using the 3D printer.  I put presets in the camera for a wide view and also zoomed in views of the CNC router and the 3D printer.

image

A short video showing the preset views:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

 

Warning light?

The other feature that I've considered is a warning light outside the door of the workroom to indicate that the laser is in operation.  That may be overkill for a home setup

  • Sign in to reply

Top Comments

  • mp2100
    mp2100 over 6 years ago +4
    Very nice. This is really safety first, buying the safety equipment before Santa deliveries your gift.
  • dubbie
    dubbie over 6 years ago +4
    It is good to see safety being seriously considered with lasers as it only takes one mistake. Eyes don't heal well after a lasering. An alternative approach would be to put the laser cutter inside a box…
  • shabaz
    shabaz over 6 years ago +3
    Hi Ralph, Nice reminder about the extingusher, I need to get one too. The camera set-up is very cool! That style of glasses fits really well, I could not tell that there are prescription glasses behind…
Parents
  • mp2100
    mp2100 over 6 years ago

    Very nice.  This is really safety first, buying the safety equipment before Santa deliveries your gift.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mp2100
    mp2100 over 6 years ago

    Very nice.  This is really safety first, buying the safety equipment before Santa deliveries your gift.

    • Cancel
    • Vote Up +4 Vote Down