Personal Blogs
  • Community Hub
  • More
Personal Blogs
Ralph Yamamoto's Blog Wii Fit Plus - 4000 days
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 18 Feb 2020 1:38 AM Date Created
  • Views 1918 views
  • Likes 8 likes
  • Comments 7 comments
  • nintendo wii
Related
Recommended

Wii Fit Plus - 4000 days

ralphjy
ralphjy
18 Feb 2020

In today's world of planned obsolescence of consumer electronics products, I am always delighted when I'm able to use something well past its expected expiration date.  It took me a long time to swap out all of my CRTs (TVs, monitors, oscilloscopes) because they were all still functioning but that's another story......   I bought a Nintendo Wii back in March of 2009 and it's been reminding me lately that I'm nearing a milestone of 4000 days since I started using it.  I've played a few games on it but my primary purpose was to use it with their fitness program, Wii Fit Plus, that uses a balance board and the handheld remote to monitor fitness and do exercises.  I've used it daily whenever I'm at home and it still works like new.  I have added an HDMI adapter cable to interface to the new TV.  I thought I'd take a moment to celebrate its longevity as I'm not sure that it will get to 5000 days.

 

image

 

{gallery} Wii Fit Plus

image

Wii Fit Plus: Program Start Screen

image

Wii Fit Plus: 4000th Day

image

Wii Fit Plus: 4000th day greeting

image

Wii Fit Plus: Center of Balance

image

Wii Fit Plus: BMI

image

Wii Fit Plus: BMI History

image

Wii Fit Plus: Age

 

When I bought the Wii I was still working and I was 25 lbs heavier and had an unhealthy BMI.  I think the fitness tracking and exercise helped me to lose about 10 lbs but retirement and the granddog are what got me to my current weight.  I've been able to maintain my current weight for the past 5 years.  I can still manage to score a Wii Fit Age of 20 most of the time.  I hope the Wii will last well beyond 5000 days as I still enjoy using it daily.  They stopped making these in 2013 and also stopped making its successor, the Wii U, in 2017.  If I needed to replace it today I'd need to get a Nintendo Switch.

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 6 years ago +3
    Hi Ralph, This is a really nice thing to read. Congrats on sustaining the healthy lifestyle like this, It's awesome to hear how you managed it, and the commitment. 25lb difference is amazing!!
  • cstanton
    cstanton over 6 years ago +3
    The Wii U is a great upgrade to the Wii for using Wii Fit, the updated version of Wii Fit adds some nice features and you can carry across your data from the Wii version. You get more exercises using the…
  • ralphjy
    ralphjy over 6 years ago in reply to cstanton +2
    Nice to know that the Wii U is a good upgrade. Too bad these aren't available new anymore. I've seen mixed reviews on the refurbished units.
Parents
  • cstanton
    cstanton over 6 years ago

    The Wii U is a great upgrade to the Wii for using Wii Fit, the updated version of Wii Fit adds some nice features and you can carry across your data from the Wii version. You get more exercises using the 'tablet' , and some extra ones which use both controllers and the board, (Wii motion plus controllers are also worthwhile getting for the Wii U update).

     

    I still use my Wii U for Wii Fit as well, I've gone through phases, ashamedly, of being too heavy for the board, through to being light enough to start using it again image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • cstanton
    cstanton over 6 years ago

    The Wii U is a great upgrade to the Wii for using Wii Fit, the updated version of Wii Fit adds some nice features and you can carry across your data from the Wii version. You get more exercises using the 'tablet' , and some extra ones which use both controllers and the board, (Wii motion plus controllers are also worthwhile getting for the Wii U update).

     

    I still use my Wii U for Wii Fit as well, I've gone through phases, ashamedly, of being too heavy for the board, through to being light enough to start using it again image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ralphjy
    ralphjy over 6 years ago in reply to cstanton

    Nice to know that the Wii U is a good upgrade.  Too bad these aren't available new anymore.  I've seen mixed reviews on the refurbished units.