Documents New Member: The 555
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: patkelly
  • Date Created: 4 Aug 2011 2:19 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 3:02 AM
  • Views 2233 views
  • Likes 3 likes
  • Comments 22 comments
Related
Recommended

New Member: The 555

imageThe 555 timer IC is an integrated circuit (chip) used in a variety of timer, pulse generation and oscillator applications. The IC design was proposed in 1970 by Hans R. Camenzind and Jim Ball. After prototyping, the design was ported to the Monochip analogue array, incorporating detailed design by Wayne Foletta and others from Qualidyne Semiconductors.

 

http://uk.farnell.com/productimages/farnell/standard/42268233.jpgSignetics (later acquired by Philips) took over the design and production, and released the first 555s in 1971. The full part numbers were NE555 (commercial temperature range, 0 °C to +70 °C) and SE555 (military temperature range, −55 °C to +125 °C). As with most parts of the era, these were available in both high-reliability metal can (T package) and inexpensive epoxy plastic (V package) packages. Thus the full part numbers were NE555V, NE555T, SE555V, and SE555T.

 

It has been hypothesized that the 555 got its name from the three 5 kΩ resistors used within, but Hans Camenzind has stated that the number was arbitrary. The part is still in widespread use, thanks to its ease of use, low price and good stability. As of 2003, it is estimated that 1 billion units are manufactured every year. The circuit arrangement of the 555 is said to be even more common, being incorporated in thecharge pump of many single-voltage Flash and other electrically-erasable ICs.

 

Source: http://en.wikipedia.org/wiki/555_timer_IC

  • become-an-expert
  • ranking
  • status
  • ic
  • expert
  • your-expert
  • new-member
  • 555
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • DAB
    DAB over 12 years ago +1
    The 555 chip is one of the most elegantly designed and versatile chip that I use. So far, I have not seen anyone who has come up with a better analog/digital chip in 40 years. Learn it well, it will always…
  • mmohit00007
    mmohit00007 over 12 years ago +1
    i use this 555 timer IC many times
  • babusingh9211
    babusingh9211 over 12 years ago in reply to mmohit00007 +1
    great share
  • paulyvee
    paulyvee over 11 years ago

    I one built a display unit with several hundred miniature incandescent lamps - long before LED;s existed almost entirely controlled by 555's. I started off with one being used as a timer, into a CMOS counter the outputs of which triggered other 555's  Each of the second group had a transistor connected across the timing cap and produced a nice clean ramp on it's collector.  These ramps then were fed into 741;s giving control over ramp height, direction and angle by driving as inverters or not and into saturation and then fed out to a f***king great row of 2N3055's to drive the lamps.

    I must say that given I was replacing a series of cam timers which switched resistors in series - it was for the time quite innovative.

    We are looking at 25+ years ago remember.

    As a matter of fact I saw the same display unit in use only a couple of years ago - still with the same electronics AND the same bulbs so the gentle ramping of volts across them didn't do them any harm.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    her in the Philippines we it LM555 timer :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Thanks, good to know some history

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to Problemchild

    I've always called it the 5-5-5 or N-E-5-5-5.  Back when I first learned about it the data sheets were Signetics.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to fustini

    5,5,5 and tripple 5 seem to be the most common by far

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to mcb1

    Some people have done Logic and even complete calculators with them so there seems to be little you can't do with the humble 555 if you have enough of them and an acreage of PCB!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 12 years ago

    Are you going to do one on the next "New" member the 741?

     

    I see a section dedicated to New old members and maybe stuff made from them

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to e14 Contributor

    Dan

    I've used them as a PWM for dimming 12v 50w lamps, to one shot timers using a capacitor in the trigger line to stop it continually timing.

     

    I think I have at least one book ... (for the 'instant generation' that's something you went out and brought in the days before internet and the Personal Computer).

    They still sell a 76 page one at Jaycar.

     

    There are some links here

    http://www.555-timer-circuits.com/

    http://www.talkingelectronics.com/projects/50%20-%20555%20Circuits/50%20-%20555%20Circuits.html

    http://www.instructables.com/id/47-projects-to-do-with-a-555/

    http://makezine.com/2012/08/24/555-timer-weekend-projects/

    and the 1977 book http://www.ebook3000.com/555-Timer-It-s-Applications_87023.html

    https://www.mne.psu.edu/me345/Lectures/The_555_Timer_IC.pdf

    http://www.doctronics.co.uk/555.htm

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to mcb1

    Mark  I think I may need to do a write up on the 555 Timer, Maybe learn some new uses and new information as well. Back in 1994 Is when I learned about it in school so maybe some new things have come out since then and some new projects I am not yet aware of. What do you think Maybe a Collaborative article? Or anyone in the community wish to collaborate I am very open to other points of view and knowledge to make a great article

     

    Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago

    In the x hundred years it's been around, I've heard and called it the 'Triple 5'.

     

    It is an extremely versatile chip, and I've sometimes debated whether or not to replace with an ATiny85 .... but with 200mA output, it drives most items directly.

     

    I think it needs to do more blogs, and some road tests in order to improve its points....

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>