Documents New Member: The 555
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: patkelly
  • Date Created: 4 Aug 2011 2:19 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 3:02 AM
  • Views 2184 views
  • Likes 3 likes
  • Comments 22 comments
Related
Recommended

New Member: The 555

imageThe 555 timer IC is an integrated circuit (chip) used in a variety of timer, pulse generation and oscillator applications. The IC design was proposed in 1970 by Hans R. Camenzind and Jim Ball. After prototyping, the design was ported to the Monochip analogue array, incorporating detailed design by Wayne Foletta and others from Qualidyne Semiconductors.

 

http://uk.farnell.com/productimages/farnell/standard/42268233.jpgSignetics (later acquired by Philips) took over the design and production, and released the first 555s in 1971. The full part numbers were NE555 (commercial temperature range, 0 °C to +70 °C) and SE555 (military temperature range, −55 °C to +125 °C). As with most parts of the era, these were available in both high-reliability metal can (T package) and inexpensive epoxy plastic (V package) packages. Thus the full part numbers were NE555V, NE555T, SE555V, and SE555T.

 

It has been hypothesized that the 555 got its name from the three 5 kΩ resistors used within, but Hans Camenzind has stated that the number was arbitrary. The part is still in widespread use, thanks to its ease of use, low price and good stability. As of 2003, it is estimated that 1 billion units are manufactured every year. The circuit arrangement of the 555 is said to be even more common, being incorporated in thecharge pump of many single-voltage Flash and other electrically-erasable ICs.

 

Source: http://en.wikipedia.org/wiki/555_timer_IC

  • become-an-expert
  • ranking
  • status
  • ic
  • expert
  • your-expert
  • new-member
  • 555
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • DAB
    DAB over 12 years ago +1
    The 555 chip is one of the most elegantly designed and versatile chip that I use. So far, I have not seen anyone who has come up with a better analog/digital chip in 40 years. Learn it well, it will always…
  • mmohit00007
    mmohit00007 over 12 years ago +1
    i use this 555 timer IC many times
  • babusingh9211
    babusingh9211 over 12 years ago in reply to mmohit00007 +1
    great share
Parents
  • paulyvee
    paulyvee over 11 years ago

    I one built a display unit with several hundred miniature incandescent lamps - long before LED;s existed almost entirely controlled by 555's. I started off with one being used as a timer, into a CMOS counter the outputs of which triggered other 555's  Each of the second group had a transistor connected across the timing cap and produced a nice clean ramp on it's collector.  These ramps then were fed into 741;s giving control over ramp height, direction and angle by driving as inverters or not and into saturation and then fed out to a f***king great row of 2N3055's to drive the lamps.

    I must say that given I was replacing a series of cam timers which switched resistors in series - it was for the time quite innovative.

    We are looking at 25+ years ago remember.

    As a matter of fact I saw the same display unit in use only a couple of years ago - still with the same electronics AND the same bulbs so the gentle ramping of volts across them didn't do them any harm.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • paulyvee
    paulyvee over 11 years ago

    I one built a display unit with several hundred miniature incandescent lamps - long before LED;s existed almost entirely controlled by 555's. I started off with one being used as a timer, into a CMOS counter the outputs of which triggered other 555's  Each of the second group had a transistor connected across the timing cap and produced a nice clean ramp on it's collector.  These ramps then were fed into 741;s giving control over ramp height, direction and angle by driving as inverters or not and into saturation and then fed out to a f***king great row of 2N3055's to drive the lamps.

    I must say that given I was replacing a series of cam timers which switched resistors in series - it was for the time quite innovative.

    We are looking at 25+ years ago remember.

    As a matter of fact I saw the same display unit in use only a couple of years ago - still with the same electronics AND the same bulbs so the gentle ramping of volts across them didn't do them any harm.