Polls What do you think is the best Single board Computer in the market?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 31 Mar 2016 8:12 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:57 PM
  • Views 2370 views
  • Likes 1 like
  • Comments 40 comments
Related
Recommended

What do you think is the best Single board Computer in the market?

There are too many options to choose from now. There is no right or wrong answer here. Please tell us why in the comments section below.

 

I have created this document so that we can compare all the SBCs in one place. Please edit it and add information on the SBCs you know about for the benefit of the community.

 

Comparison of SBCs in the market.

  • rasberry pi
  • single board
  • best
  • computers
  • beagle bone
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 10 years ago +5
    Reference: http://wiki.pine64.org/index.php/Main_Page For USD 39.00 + shipping, the Pine A64+ (see details at reference) + 2GB DDR3 RAM, WiFi, 10/100/1000 Mbps Ethernet RJ45, and Bluetooth. No GPS built…
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to rsc +3
    Yo Scott! I hear ya. I have been assembling Mini-ITX systems for folks since their inception; small is beautiful. I am still running a Zotac IONITX-F-E (Dual-core Intel Atom 1.6GHz + Nvidia ION graphics…
  • rachaelp
    rachaelp over 10 years ago +3
    There are so many options and the "best" really does depend on what your project requirements are. For the same person the best may well change a lot depending on the design requirements for what they…
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    I was tempted by the Raspberry Pi but I got won over by the Beagleboard Black, well more so due to the two PRU (programmable real time units) or 200MHz MCUs which share the same memory as the Linux kernel. This meant I could use Debian and all its goodies, and still use the PRUs for interrupts (circumventing the non-prempetive Linux kernel) which gives me a true embedded fit-for-anything board which one can program at both, high and low level, concurrently.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 10 years ago

    I was tempted by the Raspberry Pi but I got won over by the Beagleboard Black, well more so due to the two PRU (programmable real time units) or 200MHz MCUs which share the same memory as the Linux kernel. This meant I could use Debian and all its goodies, and still use the PRUs for interrupts (circumventing the non-prempetive Linux kernel) which gives me a true embedded fit-for-anything board which one can program at both, high and low level, concurrently.