Polls What do you think is the best Single board Computer in the market?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 31 Mar 2016 8:12 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:57 PM
  • Views 2386 views
  • Likes 1 like
  • Comments 40 comments
Related
Recommended

What do you think is the best Single board Computer in the market?

There are too many options to choose from now. There is no right or wrong answer here. Please tell us why in the comments section below.

 

I have created this document so that we can compare all the SBCs in one place. Please edit it and add information on the SBCs you know about for the benefit of the community.

 

Comparison of SBCs in the market.

  • rasberry pi
  • single board
  • best
  • computers
  • beagle bone
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 10 years ago +5
    Reference: http://wiki.pine64.org/index.php/Main_Page For USD 39.00 + shipping, the Pine A64+ (see details at reference) + 2GB DDR3 RAM, WiFi, 10/100/1000 Mbps Ethernet RJ45, and Bluetooth. No GPS built…
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to rsc +3
    Yo Scott! I hear ya. I have been assembling Mini-ITX systems for folks since their inception; small is beautiful. I am still running a Zotac IONITX-F-E (Dual-core Intel Atom 1.6GHz + Nvidia ION graphics…
  • rachaelp
    rachaelp over 10 years ago +3
    There are so many options and the "best" really does depend on what your project requirements are. For the same person the best may well change a lot depending on the design requirements for what they…
Parents
  • rsc
    rsc over 10 years ago

    If you need a real SBC, go with a mini-itx board.  I like Zotac myself, but there are several suppliers.

    These boards have everything you need including SATA , 4-64GB mem slots, usually have a PCI and/or PCI-E slot,

    some are fanless. Add a Ni-Daq card and labview and take 16 channels of data at 20khz sample rate no problem.

     

    For $150 you can get:

    Zotac ZBOX PI320 Quad Core Atom Z3735F Fanless Pico PC with 2GB RAM, 32GB Internal SSD, External 3-in-1 Card Reader, Wi-Fi, Bluetooth and Windows 10 Home

    mini-itx.com - store - ZBOX Pico PCs

     

    On the other end of the spectrum,  If all you need to do is run a couple of servos, then a NXP LPC810 is all you need. $2.50 each

    https://learn.adafruit.com/downloads/pdf/getting-started-with-the-lpc810.pdf

    The rest of the boards on your list are somewhere in-between, and most of your time will be spent figuring out what toolchain to use for development and programming.

    Clear as mud, eh?

    Scott

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to rsc

    Thanks Scott. I did not know about the Mini-ITX systems before your comment here. I am an electronics Engineering student and new to DIY. I tried searching for mini-ITX systems in local market but it seems that India is not into it yet.

    I am now looking at feasibility to import it and try it out. Thanks a lot.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    India is definitely into Mini-ITX.  E.g. http://www.pricedekho.com/motherboard/mini-itx+motherboard-price-list.html

     

    Mini-ITX is simply a is a 17 × 17 cm form factor for motherboards, pioneered by VIA Technology in Taiwan.  Most if not all board manufacturers offer products in this size.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    One word of warning about Intel "Cedar Trail" GMA mobos (https://en.wikipedia.org/wiki/Intel_GMA) like the Intel ATOM MUD and MUD2 boards: Intel, the graphics supplier, Imagination Technologies (PowerVR), and the various Linux distro communities  do not support Linux on them.  Hence, one has to settle for a buggy form of vanilla VGA graphics.

     

    An example of one of these non-Linux mobos is the "Intel D2700 MUD".

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    ooh. I've seen these. But these are too large for my applications. I'll go for them at a later time when required.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    Thanks a lot. This is the kind of information only experienced users can help us out with.

     

    It would be helpful if you can write an article on selecting the best mini ITX for your application for a noob like me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    You said above that Mini-ITX is too large for your purposes.  Look up.

     

    Most folks at this site would be bored with a blog on selecting the best Mini-ITX as they are understandably into very small footprints (very different from 17 × 17 cm form factor) or they are already experts with more traditional computer assembly.  However, which Mini-ITX (or any other mobo/SBC) you need depends on your purpose.  One type does not fit all.  It is very personal.

     

    There are many DIY guides/forums on-line for DIYers like Tom's Hardware (http://www.tomshardware.com/ ) and AnandTech (AnandTech: Hardware News and Tech Reviews Since 1997 ).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    P.S. If you are ever going into a conventional build project such as ATX, Micro-ATX, Mini-ITX, or Mini-STX and you can specify an application (E.g. one of workstation, file server, or HTPC), then I would be able to make some recommendations for you.

     

    In general:

    • File servers typically need wired Ethernet connections, minimal graphics, and probably no audio.  What (eSATA/EIDE/USB) storage will be used?
    • Workstations need graphics and audio.  What level of quality is desired for both?
    • HTPCs also need graphics and audio.  HDMI to a high definition TV is normally used for Video.  Audio too or will audio pipe into a separate device like a sound system of some sort?

     

    I should stop there.  There are a lot of personal preference and usage questions to answer regardless of the application.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    P.S. If you are ever going into a conventional build project such as ATX, Micro-ATX, Mini-ITX, or Mini-STX and you can specify an application (E.g. one of workstation, file server, or HTPC), then I would be able to make some recommendations for you.

     

    In general:

    • File servers typically need wired Ethernet connections, minimal graphics, and probably no audio.  What (eSATA/EIDE/USB) storage will be used?
    • Workstations need graphics and audio.  What level of quality is desired for both?
    • HTPCs also need graphics and audio.  HDMI to a high definition TV is normally used for Video.  Audio too or will audio pipe into a separate device like a sound system of some sort?

     

    I should stop there.  There are a lot of personal preference and usage questions to answer regardless of the application.