Polls Your base OS for development or your favourite Workbench OS!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: xeonaj
  • Date Created: 21 Oct 2019 8:03 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:59 PM
  • Views 3370 views
  • Likes 1 like
  • Comments 55 comments
Related
Recommended

Your base OS for development or your favourite Workbench OS!

i recently had a good long argument on using Windows or Linux Os for development. I am a serious Windows 10 fanboy. So I just wanted to know how many use Linux, Windows 10 and MacOS.

I know these OS's are un-comparable but I just want to show my friends the voting down by real engineers of this community!

All those voting I would also love to hear why you love the OS and how it differs itself from others.

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • genebren
    genebren over 7 years ago +5
    I continue to use my Windows 7 Pro OS. I was never a fan of the later versions of Windows and I use too many programs that I could not find availables for Linux.
  • Fred27
    Fred27 over 7 years ago +4
    If you're a professional then you should be capable and comfortable with both Windows and Linux. By all means have a preference for one or the other, but don't make the mistake of thinking anyone else…
  • Jan Cumps
    Jan Cumps over 7 years ago +4
    others: windows and linux for boards that can run an OS. latest versions if I can. RTOSes for microcontrollers. FreeRTOS or TI-RTOS.
Parents
  • Gough Lui
    Gough Lui over 7 years ago

    I prefer Windows purely because I still have many devices that work better on Windows, so this remains my primary. However, the number of Linux boxen outnumber Windows boxes in the house, so it's a win for both really. Develop on one, deploy on/with the other.

     

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • xeonaj
    xeonaj over 7 years ago in reply to Gough Lui

    I have a got a single PC which works super fine!

    Running WSL which integrates with VS Code nicely. Yeah am waiting for WSL2!

    And I use my VMWare inside which is my main testing environment!

    image

    But sometimes I do get bottle necked due the amount of RAM needed for some OS's!

    I had MacOS Catalina running in the VMWare -> https://www.geekrar.com/install-macos-catalina-on-vmware-on-windows-pc/  (Not my Blog!)

    But then did some experiments and it crashed!

    My total amount of RAM is just 8GB! So allocating 5GB to MacOS doesn't even fulfill its basic needs!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 7 years ago in reply to xeonaj

    I do have a few Linux VMs myself as well. Don't run WSL - real Linux is better, but prior to WSL, I used Cygwin quite a bit.

     

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • xeonaj
    xeonaj over 7 years ago in reply to Gough Lui

    Yeah Real Linux is Better! Things like Snapd, Systemmd and many other core ubuntu linux stuff wont run on WSL!

    But when you just want to run some small shell scripts for some testing purpose WSL is super fast and integrates with Windows well!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • xeonaj
    xeonaj over 7 years ago in reply to Gough Lui

    Yeah Real Linux is Better! Things like Snapd, Systemmd and many other core ubuntu linux stuff wont run on WSL!

    But when you just want to run some small shell scripts for some testing purpose WSL is super fast and integrates with Windows well!