Arduino Projects
  • Products
  • Arduino
  • Arduino Projects
  • More
  • Cancel
Arduino Projects
Blog A simple DIY Oscilloscope with Arduino Uno and Mega
  • Blog
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Former Member
  • Date Created: 26 Dec 2014 11:05 AM Date Created
  • Views 34707 views
  • Likes 20 likes
  • Comments 79 comments
  • mega
  • ardbeginner
  • tft
  • oscilloscope
  • uno
  • arduino
Related
Recommended

A simple DIY Oscilloscope with Arduino Uno and Mega

Former Member
Former Member
26 Dec 2014

My DIY Oscilloscope, how i got my signal image

 

Content :

- Description

- Screenshots

- Video

- Credits and links

 

Descriptions

 

I am experimenting with RF and IR signals in various frequencies and had some trouble with the receivers and needed to see what kind of signal i was receiving.

I cannot afford a real oscilloscope but i knew about the older Arduino oscilloscopes.

 

After trying many different versions of code and tutorials, I was unable to get a single one to work, and all the tutorials and guides around was 2-3 years old.
Not sure if it is the IDE or the actual hardware that has changed in such a way that it didn't work anymore.

 

I finally found a working oscilloscope from a Japanese website, (linked below) and a working TFT screen library,

meaning i could read the various signals received.

 

Clearly the limitations are 0-5v but that is fine, what i needed to know is either wave type and frequency, and this is sufficient.
It also gives me an indication of the amplitude which is just a nice bonus.

 

But what I'm most happy with, is the two channel feature, i often use the second channel as a reference point to be able to

differentiate the main channel on the screen.

 

 

Some screenshots..

This is the .96" OLD test, single wave test imageimage

 

 

 

imageimageimage

2.4" TFT screen on the Uno,    two right images same screen on a Mega.

 

 

A youTube vidoe i made on the experience.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

 

Credits and Links :

 

My compilation of the Oscilloscope and TFT library  ( what you see on the video and images ) :

https://dl.dropboxusercontent.com/u/19761809/arduino/Vaupell-Oscilloscope.zip

 

 

Original Oscilloscope link (code by : Noriaki Mitsunaga ) :

http://n.mtng.org/ele/arduino/oscillo-j.html

 

 

Original TFT display link ( TFT shield library source ) :

http://www.smokeandwires.co.nz/blog/a-2-4-tft-touchscreen-shield-for-arduino/

 

TFT library :

Library : https://github.com/Smoke-And-Wires/TFT-Shield-Example-Code

Attachments:
Vaupell-Oscilloscope.zip
  • Sign in to reply

Top Comments

  • Former Member
    Former Member over 10 years ago in reply to 4ringfan +2
    True, I highly recomened if using ribbon cable, buy a roll, and add the ends yourself, much much cheaper. I usually buy them home in 10 meters at a time. But, I try to use cable as little as possible,…
  • 4ringfan
    4ringfan over 10 years ago +1
    I just received a LCD TFT shield that I had ordered for no particular reason. Now I'm going to have to play with it. Thanks for the incentive!
  • Former Member
    Former Member over 10 years ago in reply to Former Member +1
    Nope just one of them. The problem was the Screen it took up all my pins on the arduino uno. You could do a messy workaround, either by soldering something onto the SD pins (since were not using them anyway…
Parents
  • Former Member
    Former Member over 10 years ago

    So, we need both Mega AND Uno?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to Former Member

    Nope just one of them.

     

    The problem was the Screen it took up all my pins on the arduino uno.

    You could do a messy workaround, either by soldering something onto the SD pins (since were not using them anyway)

    or some mechanical workaround, like bending one of the SD card legs, to fit a jumper wire instead. image  (not recommended, they might break)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • lokkytron
    lokkytron over 10 years ago in reply to Former Member

    Hello Martin Vaupell , please, correct me if I am worng...

    Is not possible to use an Arduino proto shield between the LCD and the UNO board?

     

    ArduinoProtoShield_Front_450px.jpgArduinoProtoShield_Back_450px.jpg

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to lokkytron

    I don't see why not. 
    All the shield offers, is an extension to your arduino platform.  I use these shields myself all the time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • lokkytron
    lokkytron over 10 years ago in reply to Former Member

    I am sorry.. I meant instead of using the longer UNO board.

     

    If you put that shield between the UNO (same size than LCD) and the LCD, I think you could work on the pins you need in the proto shield.

     

    I don't really know... it is only an idea

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to lokkytron

    Yes that is correct, you can hook over some of the SD pins to some of the empty ones.
    That would also work, that's just extending the connection.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 4ringfan
    4ringfan over 10 years ago in reply to Former Member

    Could always just put the display on a ribbon cable and separate it from the arduino freeing up all unused and available pins.

     

    Using something along these lines:

     

    http://www.electrodragon.com/product/prototype-cable-female-and-male-end-40p/

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • 4ringfan
    4ringfan over 10 years ago in reply to Former Member

    Could always just put the display on a ribbon cable and separate it from the arduino freeing up all unused and available pins.

     

    Using something along these lines:

     

    http://www.electrodragon.com/product/prototype-cable-female-and-male-end-40p/

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Former Member
    Former Member over 10 years ago in reply to 4ringfan

    True, I highly recomened if using ribbon cable, buy a roll, and add the ends yourself, much much cheaper. I usually buy them home in 10 meters at a time.

     

    But, I try to use cable as little as possible, to keep everything a small tight unit.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 4ringfan
    4ringfan over 10 years ago in reply to Former Member

    vaupell,  Your intention was to make it as compact, simple, and neat as possible, which I totally get.  I like things neat and compact as well.

     

    The ribbon cable was just an idea to free up the available inputs and outputs on the controller.  The ribbon cable would also give you the possibility of mounting the display into the front panel of a project box away from the controller.

     

    I laughed a bit, not at you, but at the idea of myself making 36 cables with connectors all the same exact length.  It would be a project... that is for sure. Hehe.