Arduino Projects
  • Products
  • Arduino
  • Arduino Projects
  • More
  • Cancel
Arduino Projects
Blog A simple DIY Oscilloscope with Arduino Uno and Mega
  • Blog
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Arduino Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 26 Dec 2014 11:05 AM Date Created
  • Views 39366 views
  • Likes 20 likes
  • Comments 79 comments
  • mega
  • ardbeginner
  • tft
  • oscilloscope
  • uno
  • arduino
Related
Recommended

A simple DIY Oscilloscope with Arduino Uno and Mega

e14 Contributor
e14 Contributor
26 Dec 2014

My DIY Oscilloscope, how i got my signal image

 

Content :

- Description

- Screenshots

- Video

- Credits and links

 

Descriptions

 

I am experimenting with RF and IR signals in various frequencies and had some trouble with the receivers and needed to see what kind of signal i was receiving.

I cannot afford a real oscilloscope but i knew about the older Arduino oscilloscopes.

 

After trying many different versions of code and tutorials, I was unable to get a single one to work, and all the tutorials and guides around was 2-3 years old.
Not sure if it is the IDE or the actual hardware that has changed in such a way that it didn't work anymore.

 

I finally found a working oscilloscope from a Japanese website, (linked below) and a working TFT screen library,

meaning i could read the various signals received.

 

Clearly the limitations are 0-5v but that is fine, what i needed to know is either wave type and frequency, and this is sufficient.
It also gives me an indication of the amplitude which is just a nice bonus.

 

But what I'm most happy with, is the two channel feature, i often use the second channel as a reference point to be able to

differentiate the main channel on the screen.

 

 

Some screenshots..

This is the .96" OLD test, single wave test imageimage

 

 

 

imageimageimage

2.4" TFT screen on the Uno,    two right images same screen on a Mega.

 

 

A youTube vidoe i made on the experience.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

 

Credits and Links :

 

My compilation of the Oscilloscope and TFT library  ( what you see on the video and images ) :

https://dl.dropboxusercontent.com/u/19761809/arduino/Vaupell-Oscilloscope.zip

 

 

Original Oscilloscope link (code by : Noriaki Mitsunaga ) :

http://n.mtng.org/ele/arduino/oscillo-j.html

 

 

Original TFT display link ( TFT shield library source ) :

http://www.smokeandwires.co.nz/blog/a-2-4-tft-touchscreen-shield-for-arduino/

 

TFT library :

Library : https://github.com/Smoke-And-Wires/TFT-Shield-Example-Code

Attachments:
Vaupell-Oscilloscope.zip
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to 4ringfan +2
    True, I highly recomened if using ribbon cable, buy a roll, and add the ends yourself, much much cheaper. I usually buy them home in 10 meters at a time. But, I try to use cable as little as possible,…
  • 4ringfan
    4ringfan over 11 years ago +1
    I just received a LCD TFT shield that I had ordered for no particular reason. Now I'm going to have to play with it. Thanks for the incentive!
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor +1
    Nope just one of them. The problem was the Screen it took up all my pins on the arduino uno. You could do a messy workaround, either by soldering something onto the SD pins (since were not using them anyway…
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hi Enrico,

     

    thank you - this will bring progress in the prooject!

     

    See you

     

    Michael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to e14 Contributor

    Hi Michael,

     

    well, so if the original source code is the one you mentioned in the Instructables link and the library should replace the original code realted to the display, I will take a look as I have a minute.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hello Enrico,

     

    thanks for support. I could get the new library SPFD5408 in the arduino-libary folder and add it in the bibliotheque (when I tested the display). I use Win 10.  My problem is to modify the vaupell-sketch in this way, that it would work with my display - including the SPFD5408 library instead of the other one. But I'm not a progrmming genie. For a fit member, I think it is easy, but not for me (repair pinball machines, soldering etc. I have experience, but not in programming).

     

    Looking foreward for help.

     

    Michael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to e14 Contributor

    Hello Michael,

     

    it is a good info to know the platform you are working on; I assume that you are using Windows (but with some small changes the same proof of concept will work on Linux and OSX too). If your problem is how to include the library, what you need is to unpack the library folder and put it in your Arduino IDE libraries. There are some small differences in this approach depending on the platform you are on, but this is well documented on the arduino.cc site (the link is here) To be sure that your library has been correctly installed you should find it in the list of the available libraries from the Tools menu of the Arduino IDE. As this has been done, the library itself needs to be notified in some way to the application, including the library .h file. Also this operation can be done easily from the Tools menu of the IDE (add library) while you are editing your application.

     

    After these few preparation steps (longer to say than to do) you can use the library settings and API calls in your program as well. Instead, if you have already reached this point and need some helpful hint on how to use the library you mention with your LCD inside the sources, let me know and we will investigate in depth in the application. IMHO this should not be a too complex part.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hi,

     

    I could get my 2.4 LCD-Shield working on uno and mega with this library: How to use 2.4 inch TFT LCD SPFD5408 with Arduino Uno and Mega - All

     

    BUT because I´m a programming ***, I'm not fit to add the vaupell-oszi-sketch in the way to include the SDFD5408 libary instead of the other one (I tried but without success).

     

    Would be nice, if somebody could give me a hand (others will like it to, because with this cheap LCD-toughscreen (5.--)  and an mega, you have an oszi for about uder 20 bucks.

     

    Thanks and have a nice weekend.

     

    Michael

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>