Arduino Projects
  • Products
  • Arduino
  • Arduino Projects
  • More
  • Cancel
Arduino Projects
Blog A simple DIY Oscilloscope with Arduino Uno and Mega
  • Blog
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Arduino Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 26 Dec 2014 11:05 AM Date Created
  • Views 39366 views
  • Likes 20 likes
  • Comments 79 comments
  • mega
  • ardbeginner
  • tft
  • oscilloscope
  • uno
  • arduino
Related
Recommended

A simple DIY Oscilloscope with Arduino Uno and Mega

e14 Contributor
e14 Contributor
26 Dec 2014

My DIY Oscilloscope, how i got my signal image

 

Content :

- Description

- Screenshots

- Video

- Credits and links

 

Descriptions

 

I am experimenting with RF and IR signals in various frequencies and had some trouble with the receivers and needed to see what kind of signal i was receiving.

I cannot afford a real oscilloscope but i knew about the older Arduino oscilloscopes.

 

After trying many different versions of code and tutorials, I was unable to get a single one to work, and all the tutorials and guides around was 2-3 years old.
Not sure if it is the IDE or the actual hardware that has changed in such a way that it didn't work anymore.

 

I finally found a working oscilloscope from a Japanese website, (linked below) and a working TFT screen library,

meaning i could read the various signals received.

 

Clearly the limitations are 0-5v but that is fine, what i needed to know is either wave type and frequency, and this is sufficient.
It also gives me an indication of the amplitude which is just a nice bonus.

 

But what I'm most happy with, is the two channel feature, i often use the second channel as a reference point to be able to

differentiate the main channel on the screen.

 

 

Some screenshots..

This is the .96" OLD test, single wave test imageimage

 

 

 

imageimageimage

2.4" TFT screen on the Uno,    two right images same screen on a Mega.

 

 

A youTube vidoe i made on the experience.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

 

Credits and Links :

 

My compilation of the Oscilloscope and TFT library  ( what you see on the video and images ) :

https://dl.dropboxusercontent.com/u/19761809/arduino/Vaupell-Oscilloscope.zip

 

 

Original Oscilloscope link (code by : Noriaki Mitsunaga ) :

http://n.mtng.org/ele/arduino/oscillo-j.html

 

 

Original TFT display link ( TFT shield library source ) :

http://www.smokeandwires.co.nz/blog/a-2-4-tft-touchscreen-shield-for-arduino/

 

TFT library :

Library : https://github.com/Smoke-And-Wires/TFT-Shield-Example-Code

Attachments:
Vaupell-Oscilloscope.zip
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to 4ringfan +2
    True, I highly recomened if using ribbon cable, buy a roll, and add the ends yourself, much much cheaper. I usually buy them home in 10 meters at a time. But, I try to use cable as little as possible,…
  • 4ringfan
    4ringfan over 11 years ago +1
    I just received a LCD TFT shield that I had ordered for no particular reason. Now I'm going to have to play with it. Thanks for the incentive!
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor +1
    Nope just one of them. The problem was the Screen it took up all my pins on the arduino uno. You could do a messy workaround, either by soldering something onto the SD pins (since were not using them anyway…
  • Nate1616
    Nate1616 over 10 years ago in reply to e14 Contributor

    Michael,

    Can you give us a screen shot of the error(s) your getting.  It would help greatly getting you up and running.

     

    Nate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Is here anybody who get the sketch on an arduino mega? I downloaded it, unzipped with peazip, set the SWTFT-Library to mega-mode, but while compiling I get always errors in the sketch. We tried it with 3 different PCs and 2 different megas and one uno (then setup for uno).

     

    It looks very nice, but works it really, or is it just a fake?

     

    Would be nice, if somebody could help me, if this oscilloscope really works.

     

    Thank you and best regards.

     

    Michael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    hi I am work on your osc but evry think invers  in tft 2.4 lcd and I us uno r3 with this tft pleas if any help  .thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hello, https://dl.dropboxusercontent.com/u/19761809/arduino/Vaupell-Oscilloscope.zip, seems to be corrupted.   Can you send it to my e-mail?  leonardoxms@yahoo.com.br

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • niq_ro
    niq_ro over 11 years ago

    finally, I download the sketch image... but is not for shield display who works with SWTFT library... I change the sketch for work with SWTFT library and you can download from https://github.com/tehniq3/SWTFT-oscilloscope/blob/master/TFT_Oscillo2 image

    I made a small movie with TFT display with touch put on a shield: https://youtu.be/oylFMWnAePA but must made a intermediate shield for isolate A3, A4 (A5 is free)...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>