Arduino Projects
  • Products
  • Arduino
  • Arduino Projects
  • More
  • Cancel
Arduino Projects
Blog Arduino mini arcade cabinet
  • Blog
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Arduino Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: hwhardsoft
  • Date Created: 16 Sep 2014 4:49 PM Date Created
  • Views 3579 views
  • Likes 6 likes
  • Comments 18 comments
  • gamebuino
  • arcade
  • game
  • duinocade
  • arduino
Related
Recommended

Arduino mini arcade cabinet

hwhardsoft
hwhardsoft
16 Sep 2014

I want to introduce a tiny arcade cabinet (14cm heigth) based on the Arduino. The arcade is also full compatible to the Gamebuino - an Arduino based game console. The Arcade game is equipped with a ATMEGA328 and the screen of the game has been provided by a Nokia 5110 LCD. A couple of Open Source games for the Gamebuino and so also for this Arcade cabinet are available - programmed under the Arduino IDE... Check my website for more information.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

imageimage

imageimage

  • Sign in to reply

Top Comments

  • hwhardsoft
    hwhardsoft over 10 years ago in reply to Workshopshed +4
    Yep - back from the Maker Faire Berlin. It was awesome:
  • Workshopshed
    Workshopshed over 10 years ago +3
    I saw some big and small arcade machines at the Maker Faire And for those going to the Berlin Faire, I see that Hartmut will be there.
  • Workshopshed
    Workshopshed over 11 years ago +1
    Great result Hartmut , love the case design
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to hwhardsoft

    Almost yes. To make an arcade container in a scale (based on experience only it will be 1:1.5 or 1:2 max respect the Arduino version) and not doing a bad one I need to find the right measures for the proportion. I think.

     

    Finally today by the end of day I had time for a decent search ...

     

    First of all I see that in JSMame format there is an incredible quantity of original arcade games in the Internet Archive https://archive.org/details/internetarcade

    Then it is almost easy to find a good detailed reference to create a scaled design of an original arcade, with some interesting customisations:

    ArcadeX

    Cabinet Design Plans

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hwhardsoft
    hwhardsoft over 9 years ago

    Do you mean with 'arcade container' a finished arcade enclosure from any other source?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to hwhardsoft

    I agree, I have used only CNC to make almost all, not only cases but also PCB first prototype for testing (thin copper), vacuum chambers (PVC and Nylon), mechanical components and support (Aluminium), test cases (compact plastic), SMD components testing (Acrylic) and more. For the mass production - or also for small production series - I try to find the cheapest and less time consuming way. It was a revelation the laser cutting for most of the applications related to cases and 3D printing for some mechanical components. With all the three options I always try to see what is the best solution also considering how easily is finding material and the process time. With CNC the problems in this specific situation I think it is the process time and the amount of material that should be removed starting from a full material block instead of laser cutting just the pieces. As a matter of fact a miniature case is a replica of the biggest one IMHO it is helpful to see the construction building of the originals: 3 cm thick plywood of MDF plastic plated; the most similar approach in a reduced scale is acrylic and laser cutting. I think that the dramatic reduction of the machining time and the optimisation of the used material will definitely pay the choice.

     

    What do you think ? BTW, to you have idea if somewhere it is possible to find the sizes of an arcade container ?

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hwhardsoft
    hwhardsoft over 9 years ago in reply to balearicdynamics

    yes cnc milling is a little bit more expensive but you can mill much more different materials for example PVC....

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to hwhardsoft

    Hi,

     

    Why a CNC ? Is not too complex? I have and use by years a CNC machine, but  It is more expensive in my opinion. Please consider that I have never had in my hands one of these enclosures.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>