Arduino Projects
  • Products & Partners
  • Arduino
  • Arduino Projects
  • More
  • Cancel
Arduino Projects
Blog Arduino MKR DIN rail housing
  • Blog
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Arduino Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: hwhardsoft
  • Date Created: 14 Aug 2018 9:57 AM Date Created
  • Views 2924 views
  • Likes 5 likes
  • Comments 5 comments
  • arduino mkr1000
  • portenta h7
  • mkr
  • din rail
  • control cabinet
  • arduino mkr
  • cap rail
  • enclosures
  • useful arduino projects
  • arduino
Related
Recommended

Arduino MKR DIN rail housing

hwhardsoft
hwhardsoft
14 Aug 2018

The new Arduino MKR series sets up a standard about form factor, function and performance for Arduino boards in the future. These new boards comes in a compact shape, with a powerful 32 bit Cortex M0 micocontroller Atmel SAM D21 and a charger function for LiPo accumulators. Furthermore Arduino offers in this series different types of MKR modules for different IoT wireless technologies. Besides the base model Arduino MKR Zero some further types with WiFi, WAN or GSM support are available:

 

image

 

ArduiBox MKR is an enclosure set for the Arduino MKR series. The heart is an additional pcb with integrated voltage regulator and breadboard. It fits together with the Arduino MKR of your choice in a 3 module DIN rail enclosure.

Overview:

  • milled 3 module DIN rail enclosure
  • transparent lid in the top for displays, leds ....
  • pcb with socket to plug a Arduino MKR Zero / 1000 /1200 / 1400 / 1500 module
  • optional integrated voltage regulator (input voltage 9..35V via 2 way terminal block)
  • breadboard / proto board for own circuits
  • 2x 14 pole female pin header
  • all GPIO pins are marked and placed beside the breadboard area
  • 2x 3 way terminal blocks to connect external components to the breadboard

 

image

  • Sign in to reply

Top Comments

  • hwhardsoft
    hwhardsoft over 5 years ago +1
    We've reworked this enclosure set meanwhile. Now it supports MKR shields and the Arduino Portenta H7 also: Features of current version: milled 6 module DIN rail enclosure transparent or grey lid in the…
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to hwhardsoft +1
    I ordered one (I lurked when you first posted the original design, now pulled the trigger). Basic version with transparent lid. Including shipping and tax, to Brussels, just under 39 €. I have one request…
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to hwhardsoft +1
    Customer action photo:
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to Jan Cumps

    Lead-free (and LED-free):

    image

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to hwhardsoft

    Customer action photo:

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hwhardsoft
    hwhardsoft over 5 years ago in reply to Jan Cumps

    good idea!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to hwhardsoft

    I ordered one (I lurked when you first posted the original design, now pulled the trigger).

    Basic version with transparent lid. Including shipping and tax, to Brussels, just under 39 €.

     

    I have one request for the product photos on the shop: A photo of the underside with DIN mounting mechanism would have been useful.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hwhardsoft
    hwhardsoft over 5 years ago

    We've reworked this enclosure set meanwhile. Now it supports MKR shields and the Arduino Portenta H7 also:

     

    imageimage

     

    Features of current version:

     

    • milled 6 module DIN rail enclosure
    • transparent or grey lid in the top for displays, leds ....
    • pcb with slots to plug a Arduino MKR Zero / 1000 / 1200 / 1300 / 1400 / 1500 module or Portenta H7
    • slot for additional MKR Shield (e.g. MKR RS485, MKR CAN, MKR THERM...)
    • exclusive slot for the MKR ETH Ethernet shield
    • optional integrated voltage regulator (input voltage 9..35V via 2 way terminal block)
    • breadboard / proto board for own circuits
    • all GPIO pins are marked and placed beside the breadboard area
    • 2x 3 way terminal blocks to connect external components to the breadboard