• Products and Partners
    Products and Partners
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
Arduino Projects
  • Products and Partners
  • Arduino
  • Arduino Projects
  • More
  • Cancel
Arduino Projects
Blog HC-SR04 ultra sonic sensor working with Arduino Uno PLC server
  • Blog
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Arduino Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: SensoredHacker0
  • Date Created: 21 May 2026 3:41 AM Date Created
  • Views 246 views
  • Likes 3 likes
  • Comments 2 comments
  • oncod
  • On The Line
  • uno
  • arduino
  • industrial automation.
Related
Recommended

HC-SR04 ultra sonic sensor working with Arduino Uno PLC server

SensoredHacker0
SensoredHacker0
21 May 2026

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


My project is so cool, but i have nothing to say about it. 
it was a pain to get this thing working. I figured it out. 
No one wants to hear I wired it wrong,  I put the HC-SR04 on pins 9,10, only to figure out that those are network coms on the arduino UNO 
https://docs.arduino.cc/libraries/ethernet/

or that, even after figuring that out, that it was still whack. I got the serial print, for debug going. but the HMI wouldn't update properly. 
at best for a while this eveing, it was updating every other time.  then I figured to not call the function for range, but to stream it, and let the HMI read it whenever, Then you don't get timing issues so bad. 

I tried getting the Uno Q to work. I would love for that thing to work. but its slow AF in every aspect. Man I cant get that thing to update in real time fast enough to track multiple IO to my HMI. 

Ah to then youre out here trying to run an arduino as a PLC server, and you connect a PLC, which is a server. COOL, the PLC, doesnt want to be a client device. 
but I can send it client requests, so there is no problem. ... except when youre using Arduino ethernet shields those things don't do concurrent connections particularly well. 
So then youre slick, and multiplex the connection. TDM, but its just not fast enough to keep the HMI happy. So then I tried putting 2 Ethernet shields on the UNO, but that did not work either. 

Why is all this much more fun when Im not at work?

Lets see. Applications. ... ugh. Ic an read or write any sensor, or IO interface on the arduino, or PLC, and uses native ecosystem devices. 
are we going to use this in plant production? eh, probably not. I mean my boss seems pretty interested, but this was a fantasy until a few months ago. Even with PC integrations on the PLC, 
the PLC is just enough of a pain in the butt so that we're trying to drop them fast. Theres not going to be a long transition period, where some sort of platform extension would be relevant, with interoperability. back in 2020, during the chip shortage, then this project would have been amazing. 

So im just busting out proofs, getting the ideas for what needs to happen. ah got to write 16bit bi directional register translations. that'll be fun. 
then theres the hope that this might be useful to any other human. 

I wrote a library, well a couple the first one binds the register maps to the device function calls. turns out thats kinda confussing, and limiting. 
Then I wrote another library, where I focused more on protocol implementation. its better, but theres projects where the old code is in use. 
This is a team project. but therese just one of me, and I do random stuff.

I want to figure out how to run DOOM on the PLC/HMI. 


 //HC-SR04 example sketch
#include <SPI.h>
#include <Ethernet.h>
#include <Wire.h>
#include "Adafruit_seesaw.h"

const int trigPin = 6;
const int echoPin = 7;

float d682_float = 0;
float distance = 0.0;
unsigned long duration = 0;
unsigned long lastDistanceUpdate = 0;

byte mac[] = { 0x00, 0x03, 0x7B, 0x20, 0xFE, 0xED };
byte ip[]  = { 192, 168, 1, 50 };

EthernetServer server(2101);

#define SS_SWITCH        24
#define SEESAW_BASE_ADDR 0x36

const uint8_t Nencoders = 5;
Adafruit_seesaw encoders[Nencoders];

bool found_encoders[Nencoders] = { false };
int32_t encoder_positions[Nencoders] = { 0 };

int16_t w = 0;
int16_t x = 0;
int16_t y = 0;
int16_t z = 0;

bool blink_active = false;
unsigned long blink_timer = 0;
int blink_count = 0;
bool led_state = false;

float readDistanceCM() {
  digitalWrite(trigPin, LOW);
  delayMicroseconds(2);

  digitalWrite(trigPin, HIGH);
  delayMicroseconds(10);

  digitalWrite(trigPin, LOW);

  duration = pulseIn(echoPin, HIGH, 30000);

  if (duration == 0) {
    return -1.0;
  }

  return (duration * 0.0343) / 2.0;
}

void updateD682() {
  if (millis() - lastDistanceUpdate < 100) {
    return;
  }

  lastDistanceUpdate = millis();

  float v = readDistanceCM();

if (v > 0.0) {
  d682_float = v;
}
 // this was writen for a word, 
 // need to write a bitshift for 16b float conversion to arduino float
 // Serial.print("duration=");
 // Serial.print(duration);
//  Serial.print(" distance=");
//  Serial.println(distance);
 // Serial.print(" d682=");
 // Serial.println(d682);
}

void blinky(int count) {
  pinMode(LED_BUILTIN, OUTPUT);
  blink_count = count * 2;
  blink_active = true;
  blink_timer = millis();
}

void updateBlink() {
  if (!blink_active) {
    return;
  }

  if (millis() - blink_timer >= 500) {
    blink_timer = millis();
    led_state = !led_state;
    digitalWrite(LED_BUILTIN, led_state);
    blink_count--;

    if (blink_count <= 0) {
      blink_active = false;
      digitalWrite(LED_BUILTIN, LOW);
    }
  }
}

void oncod() {
  for (uint8_t enc = 0; enc < Nencoders; enc++) {
    if (!found_encoders[enc]) {
      continue;
    }

    int32_t new_position = encoders[enc].getEncoderPosition();

    if (encoder_positions[enc] != new_position) {
      encoder_positions[enc] = new_position;
    }
  }

  w = (int16_t)encoder_positions[0];
  x = (int16_t)encoder_positions[1];
  y = (int16_t)encoder_positions[2];
  z = (int16_t)encoder_positions[3];
}

uint16_t readDWord(int addr) {
  union {
    float f;
    uint32_t i;
  } u;

  switch (addr) {
    case 5:
      blinky(5);
      return 0;

    case 157:
      u.f = analogRead(A0);
      return (u.i >> 16) & 0xFFFF;

    case 156:
      u.f = analogRead(A0);
      return u.i & 0xFFFF;

    case 161:
      u.f = analogRead(A1);
      return (u.i >> 16) & 0xFFFF;

    case 160:
      u.f = analogRead(A1);
      return u.i & 0xFFFF;

    case 165:
      u.f = analogRead(A2);
      return (u.i >> 16) & 0xFFFF;

    case 164:
      u.f = analogRead(A2);
      return u.i & 0xFFFF;

    case 666:
      return digitalRead(21);

    case 669:
      return (uint16_t)w;

    case 670:
      return (uint16_t)x;

    case 671:
      return (uint16_t)y;

    case 672:
      return (uint16_t)z;

case 682: {
  union {
    float f;
    uint32_t i;
  } u;

  u.f = d682_float;

  return u.i & 0xFFFF;          // low word
}

case 683: {
  union {
    float f;
    uint32_t i;
  } u;

  u.f = d682_float;

  return (u.i >> 16) & 0xFFFF;  // high word
}

    case 570:
      return 26;

    case 3498:
    case 3499:
    case 3500:
      return 0;

    case 158:
      return random(50, 101);

    default:
      return 0;
  }
}

byte xorBcc(byte *data, int len) {
  byte bcc = 0;

  for (int i = 0; i < len; i++) {
    bcc ^= data[i];
  }

  return bcc;
}

void replyReadD(EthernetClient &c, int addr, int nbytes) {
  byte tx[96];
  int p = 0;

  tx[p++] = 0x06;
  tx[p++] = '0';
  tx[p++] = '0';
  tx[p++] = '0';

  int words = nbytes / 2;

  for (int i = 0; i < words; i++) {
    uint16_t v = readDWord(addr + i);

    const char *h = "0123456789ABCDEF";

    tx[p++] = h[(v >> 12) & 0xF];
    tx[p++] = h[(v >> 8)  & 0xF];
    tx[p++] = h[(v >> 4)  & 0xF];
    tx[p++] = h[v & 0xF];
  }

  byte bcc = xorBcc(tx, p);

  const char *h = "0123456789ABCDEF";

  tx[p++] = h[(bcc >> 4) & 0xF];
  tx[p++] = h[bcc & 0xF];
  tx[p++] = '\r';

  c.write(tx, p);
}

void handle(EthernetClient c) {
  byte buf[64];
  int len = 0;
  unsigned long lastRx = millis();

  while (c.connected() && (millis() - lastRx < 3000)) {
    oncod();
    updateBlink();
    updateD682();

    while (c.available()) {
      lastRx = millis();

      byte b = c.read();

      if (len < 64) {
        buf[len++] = b;
      }

      if (b == 0x0D) {
        if (len >= 14 && buf[0] == 0x05 && buf[4] == 'R' && buf[5] == 'D') {
          char a[5] = {
            (char)buf[6],
            (char)buf[7],
            (char)buf[8],
            (char)buf[9],
            0
          };

          char l[3] = {
            (char)buf[10],
            (char)buf[11],
            0
          };

          int addr = atoi(a);
          int nbytes = strtol(l, NULL, 16);

          replyReadD(c, addr, nbytes);
        }

        len = 0;
      }
    }

    delay(1);
  }

  c.stop();
}

void setup() {
  Serial.begin(9600);

  pinMode(trigPin, OUTPUT);
  pinMode(echoPin, INPUT);
  digitalWrite(trigPin, LOW);

  pinMode(LED_BUILTIN, OUTPUT);
  digitalWrite(LED_BUILTIN, LOW);

  pinMode(4, OUTPUT);
  digitalWrite(4, HIGH);

  Ethernet.begin(mac, ip);
  delay(1000);
  server.begin();

  randomSeed(analogRead(0));

  Wire.begin();

  for (uint8_t enc = 0; enc < Nencoders; enc++) {
    uint8_t addr = SEESAW_BASE_ADDR + enc;

    if (!encoders[enc].begin(addr)) {
      found_encoders[enc] = false;
    } else {
      encoders[enc].pinMode(SS_SWITCH, INPUT_PULLUP);
      encoders[enc].setEncoderPosition(0);
      encoder_positions[enc] = 0;
      encoders[enc].enableEncoderInterrupt();
      found_encoders[enc] = true;
    }
  }

  Serial.println("ready");
}

void loop() {
  oncod();
  updateBlink();
  updateD682();

  EthernetClient client = server.available();

  if (client) {
    handle(client);
  }
}
  • Sign in to reply

Top Comments

  • DAB
    DAB 4 months ago +1
    Every project is a learning experience.
  • kmikemoo
    kmikemoo 4 months ago

    So close... you're onto something.  Maybe you are just too early in the cycle.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB 4 months ago

    Every project is a learning experience.